DS2155移植到DS21458
Abstract
DS21458是一款四端口T1/E1/J1单片收发器(SCT),具有和DS2155单端口T1/E1/J1 SCT相同的寄存器组。DS2155和DS21458具有相同的软件架构,因而从单端口的DS2155向四端口的DS21458移植比较容易。本文详细说明了DS2155和DS21458之间的细微差异。
简介
DS21458是一款四端口T1/E1/J1单片收发器(SCT),具有和DS2155单端口T1/E1/J1 SCT相同的寄存器组。DS2155和DS21458具有相同的软件架构,因而从单端口的DS2155向四端口的DS21458移植比较容易。本文详细说明了DS2155和DS21458之间的细微差异。
寄存器映象
DS21458包含了DS2155寄存器映象的四份拷贝,每个端口一份。通过两条高位地址线A8和A9进行端口选择。尽管存储器映象基本上相同,DS2155和DS21458之间还是存在着一些小的差异。下面的表1总结了这些差异。
Register Name.Bit | Address | Bit Name | DS2155 | DS21458 | Comments |
CCR1.3 | 70h | DICAI | X | -- | Disable Idle Code Auto Increment - Selects/deselects the auto-increment feature for the transmit and receive idle code array address register, this function is not available in the DS21458 |
CCR1.7 | 70h | MCLKS | X | -- | MCLK Select, allows the user to select either TSYSCLK or MCLK as the master clock, this function is not available in the DS21458 |
CCR3.6 | 72h | INTDIS | X | -- | Interrupt Disable, allows the user to disable all interrupts regardless of the Interrupt Mask Register settings, this function is not available in the DS21458. |
CCR3.7 | 72h | TMSS | X | -- | Transmit Multi-frame Sync Source, allows the users to select the framer or TSYNC pin as the source of the multi-frame sync, this feature is not available on the DS21458. |
LBCR.7 | 4Ah | LTS | -- | X | LIUC/TPD Pin Function Select, this pin selects the function of the LIUC/TPD pin and should always be set to a 1 in the DS21458. This bit does not exist in the DS2155 memory map. |
PSA1 | F1h | -- | -- | X | Pulse Shape Adjustment Register 1 - Allows the user to adjust the transmit pulse waveform, this register is not available on the DS2155. |
PSA2 | F2h | -- | -- | X | Pulse Shape Adjustment Register 2 - Allows the user to adjust the transmit pulse waveform, this register is not available on the DS2155. |
IDR | 0Fh | -- | X | X | Device Identification Register - This read only register displays the Device ID and Chip Revision of the given device and the contents will depend on which part or revision is used. |
引脚变化
DS21458的引脚名与DS2155的对应引脚几乎相同,一个显著的区别是DS21458的有些引脚为了区分不同的端口而有所变化。例如,DS2155上的单个RSIG引脚在DS21458上变成了RSIG1, RSIG2, RSIG3和RSIG4,分别对应于四个端口。
DS2155有一个MCLK引脚,而DS21458有两个MCLK引脚,分别称为MCLK1和MCLK2。这两个引脚可以由DS21458上的一个公共源驱动。
DS2155有一个XTALD引脚,允许选择使用一个石英晶体连接在MCLK和XTALD引脚上。DS21458不支持这项功能,因而没有XTALD引脚。
8xCLK引脚也是DS21458所没有的。该引脚是DS2155的8倍频时钟输出,在DS21458上被取消了。
DS21458多了两个地址引脚, A8和A9,在DS2155上没有。这些地址引脚用于选择四个端口中的一个。
DS2155有四个普通用户输出引脚,不再出现在DS21458上。这些引脚是UOP0, UOP1, UOP2和UOP3。
LIUC引脚在DS2155上用于分离线路接口单元(LIU)和成帧器,在DS21458上被称为发送掉电(TPD)引脚。在DS21458上用户能够有限地访问成帧器和LIU之间的时钟和数据信号,不再需要LIUC引脚。在DS2155上只能通过LIC1寄存器中的TPD位使用TPD功能。由于能够有限地访问LIU和成帧器之间的信号,以下引脚在DS21458上不再出现:TPOSI, TNEGI, TCLKI, RPOSI, RNEGI和RCLKI。
ESIB功能
DS2155的扩展系统信息总线(ESIB)功能允许多达8个独立的DS2155作为一组,共用同一个8位CPU总线来报告告警和中断状态。为此,在DS2155架构中,多个器件的这些信号被外部连接在一起。在DS21458中,ESIB信号在内部汇流,只引出单组信号,以便连接另外的DS21458到ESIB总线上,构成8端口总线。有关ESIB总线功能的详细信息,请参照DS21458数据资料。
JTAG功能
DS21458的所有四个端口只用单个JTAG链。在DS2155中,JTAG链上只有一个端口。有关JTAG链的详细信息请参照DS21458数据资料中的JTAG部分。
结论
虽然DS2155和DS21458之间存在着细微的存储器映象差异,从单端口的DS2155到四端口的DS21458进行设计移植还是相当简单明了的。寄存器位的变化极少,并且除了DS21458中增加了一些支持多端口设计的引脚外,两款器件的引脚功能也基本上相同。要了解更多信息,请参阅DS2155和DS21458数据资料,请访问网站:analog.com。