Miniature, Precision Negative Reference Requires No Precision Resistors

2001-10-15

摘要

This application note discusses how to build a negative voltage reference without using external resistors or a negative supply by simply combining a simple charge-pump inverter and a positive output voltage reference.

Switched-capacitor charge-pumps, which occupy less space than do their inductor-based counterparts, are popular for providing inverted voltages in small hand-held equipment. Combining a switched-capacitor charge-pump with a precision reference, for example, yields an inverted reference from a positive power supply (Figure 1). Unlike the more typical combination of a positive 3-terminal reference and an op-amp inverter, this one delivers accurate inversions without the need for precision resistors and a negative supply.

Figure 1. A precision negative reference.

Figure 1. A precision negative reference.

The charge-pump inverter (U2) delivers -5V by inverting the output of a 5V precision reference (U1). U1 accepts inputs between 5.2V and 12.5V. Replacing it with a 2.5V reference that accepts 2.7V to 12.5V, as in the MAX6125, produces a -2.5V output. This circuit is very compact. It needs only three surface-mount capacitors, and the ICs occupy tiny SOT23 packages.

Output-voltage accuracy depends partly on the initial accuracy of U1. The MAX6150/MAX6125 devices, for example, offer 1% accuracy. To this you must add the error due to the circuit's output voltage drop, which is less than 2mV for 90µA of load current (Figure 2).

Figure 2. The load-regulation error of the circuit's output.

Figure 2. The load-regulation error of the circuit's output.

For a -2.5V output, the circuit draws low quiescent currents that range from 86µA for a 2.7V input to 105µA for a 12.5V input. For -5V outputs, the circuit draws 127µA for 5.2V inputs and 140µA for 12.5V inputs (Figure 3).

Figure 3. The circuit's supply current as a function of load current.

Figure 3. The circuit's supply current as a function of load current.

A similar version of this article appeared in the June 10, 1999 issue of EDN magazine.



添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目

关联至此文章

产品分类

最新视频 21

Subtitle
了解更多
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目