Murphy Rules!

QUESTION:

Why don’t my amplifiers and converters work correctly in the published circuit?

RAQ:  Issue 117

Answer:

When giving basic training on “Analog ICs, Their Care and Feeding,”1 I am often asked questions of this type. My questioner seems amazed when I ask for more detail before attempting to reply; seemingly “the published circuit” should provide all the information I need.

Experience shows that when the circuit in the data sheet or application note misbehaves, it is rarely the IC that is at fault. The problem is almost always due to some failure to create the circuit as given in the documentation, and that that failure is often due to Murphy’s Law. The simple form of Murphy’s Law states, “What can go wrong, will go wrong,”2 but I prefer to restate it as, “The Laws of Physics always work, even when you’re not paying attention.”

The published circuit makes a number of assumptions: the supplies will be noise-free, well-decoupled at HF and LF, low impedance, and the correct voltage; the source and load impedances will be reasonable for the intended application; the passive components will meet their specifications; the environment will not introduce noise into the circuit; and the test gear will work correctly.

Even though the engineers presumably want to solve the problem, it is sometimes difficult to persuade them to provide the details needed for diagnosis. It is necessary to know the source and load impedances likely to be encountered; if the power supply is less than ideal; if the working environment has magnetic, electrostatic, electromagnetic, or even acoustic noise; if the components used have parasitic reactances, large thermoelectric, piezoelectric, or photoelectric sensitivities, or are dissipating more power than they can handle; and what test gear is being used and if it has been checked for correct operation. In fact, in many cases when I ask for these details, I either hear no more of the problem, or am told “Oh, we solved it!” Often this means that looking for the details had revealed the cause of the problem.

I have discussed supply decoupling, environmental noise, and the unexpected properties of simple components in a number of previous RAQ columns3 and would advise anyone with unexpected circuit performance issues to review their system in the light of the advice given in those columns.

If a system is not working correctly and you have checked that the circuit is exactly the same as the one in the circuit diagram, it is well to perform simple function tests on as many of its components as you can. Often this can be done in situ with a digital multimeter (DMM) and an oscilloscope. Check that the voltages on every node are as expected and that the system is not oscillating (unless it is supposed to be oscillating, in which case check the frequency, amplitude, and waveform). Touch all of the components to ensure that nothing has become too hot. Also check for dry-soldered (high impedance) joints.

When there’s a problem, check everything. As former U.S. president Ronald Reagan said in good Russian (he was also an actor, and knew how to learn his lines): “Доверяй, но проверяй.”4 This includes test gear; it’s easy to assume that it’s working, but it might not be. I wasted a couple of hours trying to discover why my alternator was only generating 500 mA instead of >20 A. Then I discovered that one of the leads of my current meter had a resistance of over 25 Ω due to a dry joint and the entire problem was due to the test gear, not the alternator itself.

Only when you’ve proved that Murphy is not responsible should you actually start analyzing the circuit.


1Details of my courses on analog basics can be found at http://www.jbryant.eu/courses.htm

2Never forget Mrs. Murphy’s Law: “Murphy is an optimist!”

3RAQs:

4“Doveryai, no proveryai.” An old Russian proverb. In English, “Trust, but verify.”

Author

james-m-bryant

James Bryant

James Bryant was a European applications manager at Analog Devices from 1982 to his retirement in 2009, and he still writes and consults for the company. He holds a degree in physics and philosophy from the University of Leeds and is also C.Eng., EurEng., MIET, and an FBIS. In addition to his passion for engineering, James is a radio ham and holds the call sign G4CLF.