High Voltage LTC3892 Family of Controllers Reduces DC-to-DC Converter Cost and Size
High Voltage LTC3892 Family of Controllers Reduces DC-to-DC Converter Cost and Size
Introduction
LTC3892 is a versatile controller, widely used in automotive and industrial applications. The main advantages of this controller are the ability to reduce power losses by adjusting the gate voltage of switching MOSFETs and extremely low quiescent current—3.6 μA at shutdown. This is a high voltage family of controllers with an input/output voltage range of 4.5 V to 60 V. It’s very attractive for industrial customers because it can replace costly, bulky transformers in 48 V input rail applications with less expensive, compact step-down converters. High voltage controllers significantly reduce the cost of automotive electronics in 12 V and 24 V input rail applications by eliminating external transient and overvoltage protection circuitry, which simplifies the entire design.
Circuit Description and Functionality
Figure 1 illustrates a dual out, step-down converter with VOUT1 5 V at 8 A and VOUT2 12 V at 5 A. It features the LTC3892, a controller that comes in a 32-lead QFN package and that provides the following functions: selection options by the ILIM pin current sense voltage, pin VPRG1 that can set the output voltage to 3.3 V or 5.0 V without the external resistor divider, and power good pins for both outputs. LTC3892 also provides output overvoltage protection for both channels by turning on the bottom MOSFET in case of overvoltage. This chip provides protection from short-circuit conditions by implementing foldback current limiting.

Figure 1. Electrical schematic of LTC3892 in a dual output dc-to-dc converter where VOUT1 is 5 V at 8 A and VOUT2 is 12 V at 5 A.
The power train of the first channel includes MOSFETs Q1, Q4, inductor L1, and an output filter based on CO1. The power train of the second channel includes MOSFETs Q2, Q3, inductor L2, and an output filter based on CO2. The MOSFETs are not logic level and pins DRVUV and DRVSET are tied to INTVCC to provide a 10 V gate drive. Pin VPRG1 is tied to INTVCC to select a 5 V output voltage on the first channel. Figure 2 shows the converter’s efficiency. DC1998A was used for testing.

Figure 2. Efficiency curves of the dual output dc-to-dc converter.
Figure 3 illustrates a single output, dual phase step-down converter. It features LTC3892-2, a controller that comes in a 32-lead QFN package and provides features similar to those of LTC3892. However, two protection circuits are disabled: there is no overvoltage protection, nor is there protection from the short-circuit disable circuit. This chip can be used in high power battery charger applications where these protection features are not used and not desirable. Another advantage of the LTC3892-2 is its ability to support the pulse-skipping mode of operation while synchronizing to the external clock. This increases efficiency during light load operation.

Figure 3. Electrical schematic of LTC3892-2 in a single output dc-to-dc converter where VOUT is 12 V at 30 A.
To convert the dual output controller to a single output, the ITH, FB, and RUN pins of one channel are connected to the corresponding pins of the second channel. To minimize gate losses, the gate voltage of DRVCC is selected as 9 V by setting resistor RG off the DRVSET pin. Figure 4 presents the efficiency of the single output converter. DC2493A was used for evaluation..

Figure 4. Efficiency curves of the single output dc-to-dc converter.
The last IC in the family is LTC3892-1. This chip has a smaller pin count, comes in a 28-lead TSSOP package, has no PGOOD function, and it has no selectable current limit, but it provides overcurrent and overvoltage protection.
Conclusion
The LTC3892 family of controllers can be successfully used in high input/output voltage, high power applications. LTC3892 and LTC3892-1 provide a full range of protection features needed for design fully functional dc-to-dc converters. LTC3892-2 is a good choice for employment in high power charger applications.