Blood Pressure Monitor Design Considerations

May 10 2010

Abstract

This application note presents the two main types of blood pressure monitors, various measurement techniques, the functions of electrical components, and some crucial aspects that designers must consider when selecting products.

Overview

A blood pressure monitor, or sphygmomanometer, uses an inflatable air-bladder cuff and a listening device or pressure sensor to measure blood pressure in an artery. This monitoring can be performed by using either of two methods: a manually inflated cuff with a stethoscope for listening to arterial wall sounds (the auscultatory method), or a blood pressure monitor that contains a pressure sensor for sensing arterial wall vibrations (the oscillometric method).

Figure 1. Upper-arm blood pressure monitor.

Upper-arm blood pressure monitor.

Figure 2. Wrist blood pressure monitor.

Wrist blood pressure monitor.

Automatic Monitor Types

The two main types of automatic blood pressure monitors are upper-arm and wrist models. The upper-arm model has a cuff that is placed on the upper arm; the cuff is connected by a tube to the monitor that rests on a surface near the arm. The wrist model is smaller and the entire unit wraps around the wrist—this is a much more space-critical design. Some upper-arm models require manual inflation of the cuff, but most upper-arm and all wrist models are fully automatic.

Measurement Techniques

An automatic blood pressure monitor inflates a cuff surrounding an arm with sufficient pressure to prevent blood flow in the local main artery. This pressure is gradually released until the moment that the blood begins to flow through the artery, the measurement of which determines the systolic pressure. Pulse rate is also sensed at this time. The measurement taken when the blood flow is no longer restricted determines the diastolic pressure. This complete measurement cycle is performed automatically with a pump, cuff, valve, and pressure sensor.

The signal from the pressure sensor is conditioned with an op-amp circuit or by an instrumentation amplifier before data conversion by an analog-to-digital converter (ADC). The systolic pressure, diastolic pressure, and pulse rate are then calculated in the digital domain using a method appropriate for the type of monitor and sensor utilized. The resulting systolic, diastolic, and pulse-rate measurements are displayed on a liquid-crystal display (LCD), time/date-stamped, and stored in nonvolatile memory.

Figure 3. Functional block diagram of a blood pressure monitor that includes an advanced voice indicator.

Functional block diagram of a blood pressure monitor that includes an advanced voice indicator.

Data Interface

Some blood pressure monitors have the ability to upload data to a computer for further analysis and tracking of measurements over time. This data transfer is usually done through a USB interface. A discrete USB transceiver can provide this functionality, or it can be integrated within the microcontroller.

Audio Indicators

Audible indicators in blood pressure monitors range from simple beepers to more advanced audio output. A simple beeper can be driven by one or two microcontroller port pins that have pulse-width modulation (PWM) capability. More advanced voice indicators can be achieved by adding an audio digital-to-analog converter (DAC) and speaker amplifier.

Power Management

Upper-arm monitors typically use four AAA (1.5V) alkaline batteries and wrist monitors typically use two AAA alkaline batteries. The monitor's pump and analog circuitry require a 5V or 3.3V supply and the digital circuitry needs a 3.3V or 1.8V supply, depending on the technology used. Consequently, a typical upper-arm monitor would need a buck-boost switching regulator to regulate the pump/analog supply voltage to 5V and a low-dropout linear regulator (LDO) for the 3.3V digital requirement. The typical wrist monitor would use a boost switching regulator to step up the pump/analog supply voltage to 3.3V and an LDO for the 1.8V digital supply.

To extend battery life, powering down the switching regulators may be possible while the monitor is off, as long as the real-time clock (RTC) keeps running and the monitor can easily be turned back on.

Display and Backlighting

Blood pressure monitors use a simple LCD with 100 segments or less that can be driven by a driver integrated within the microcontroller. Backlighting can be added by using 1 or 2 white LEDs (WLEDs) or an electroluminescent (EL) source. A discrete WLED driver can easily be added to a monitor design by using a switching topology for wrist monitors and a linear topology for upper-arm monitors.

Electrostatic Discharge

All monitors must pass IEC 61000-4-2 electrostatic discharge (ESD) requirements. Using circuitry with built-in ESD protection or adding ESD line protectors to exposed traces can help meet these requirements.



Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

MAX1986

Ultra-Efficiency White LED Drivers

MAX1916
PRODUCTION

Low-Dropout, Constant-Current Triple White LED Bias Supply

MAX1984

Ultra-Efficiency White LED Drivers

MAX11600 PRODUCTION
2.7V to 3.6V and 4.5V to 5.5V, Low-Power, 4-/8-/12-Channel, 2-Wire Ser...
MAX1231 PRODUCTION

12-Bit 300ksps ADCs with FIFO, Temp Sensor, Internal Reference

MAX1393
1.5V to 3.6V, 312.5ksps, 1-Channel True-Differential/2-Channel Single-...
MAX1396
1.5V to 3.6V, 312.5ksps, 1-Channel True-Differential/2-Channel Single-...
MAX1227 PRODUCTION

12-Bit 300ksps ADCs with FIFO, Temp Sensor, Internal Reference

MAX1415 PRODUCTION

16-Bit, Low-Power, 2-Channel, Sigma-Delta ADCs

MAX1162 PRODUCTION

16-Bit, +5V, 200ksps ADC with 10µA Shutdown

MAX11605 PRODUCTION
2.7V to 3.6V and 4.5V to 5.5V, Low-Power, 4-/8-/12-Channel, 2-Wire Ser...
MAX1229 PRODUCTION

12-Bit 300ksps ADCs with FIFO, Temp Sensor, Internal Reference

MAX1416 PRODUCTION

16-Bit, Low-Power, 2-Channel, Sigma-Delta ADCs

DS1371 PRODUCTION

I²C, 32-Bit Binary Counter Watchdog Clock

MAXQ612

16-Bit Microcontrollers with Infrared Module and Optional USB

MAXQ622 PRODUCTION

16-Bit Microcontrollers with Infrared Module and Optional USB

MAXQ2010

16-Bit Mixed-Signal Microcontroller with LCD Interface

MAXQ2000 RECOMMENDED FOR NEW DESIGNS

Low-Power LCD Microcontroller

MAXQ8913
16-Bit, Mixed-Signal Microcontroller with Op Amps, ADC, and DACs for A...
MAXQ610 PRODUCTION

16-Bit Microcontroller with Infrared Module

MAX8892 PRODUCTION

High PSRR, Low-Dropout, 150mA Linear Regulators

MAX8891 PRODUCTION

High PSRR, Low-Dropout, 150mA Linear Regulators

MAX1574 PRODUCTION

180mA, 1x/2x, White LED Charge Pump in 3mm x 3mm TDFN

MAX1848 PRODUCTION

White LED Step-Up Converter in SOT23

Product Categories

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project