Gesture System Design

May 10 2023

Abstract

This document will provide design guidance to successfully implement a gesture detection system utilizing either the MAX25205 or MAX25405 gesture sensor. The gesture detection system will be broken down into its major system level blocks and describe each of those blocks in further detail. Two typical design examples will be shown. One for a dome light control and the other for an automotive infotainment system. Key design elements based on these two examples will relate basic design elements to many other gesture detection systems.

Request document

Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project