HFAN-06.0.1: Equalizing Gigabit-per-Second Signals on Copper Media

Mar 18 2002

Abstract

Several equalizer techniques are available for achieving signal integrity in Gigabit-per-second NRZ links on low-cost copper transmission line media, including FR-4 PCBs and coaxial cable. The most commonmethods are passive networks, adaptive receive equalization, and pre-emphasis. Use of these techniques normally involves a number of important tradeoffs, including performance, flexibility, EMI/EMC, media cost, and compatibility with standard signal formats such as SONET, Fiber Channel and Ethernet. This note provides an overview and comparison of practical methods to equalize Gigabit-per-second NRZsignals in applications, including OC-48/OC-192, XGbE and 10G FC systems, or anywhere dielectric lossand skin effect create unacceptable amounts of intersymbol interference. The results are applicable to a variety of interconnects, including backplanes, cable interconnects and 10G pluggable serial modules. Read full article.

Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project