HFTA-13.0: Designing External Cabling for Low EMI Radiation

May 22 2006

Abstract

The use of integrated circuits for equalization of cable loss has enabled a major reduction in the cost of interconnects for communication systems. For optimum performance such systems must minimize radiated emissions from the cables and connectors. Cables and connectors that interconnect various pieces of equipment should be specified to prevent interference, and to prevent the reciprocal effect of susceptibility to radiated energy. This article, which includes cable equalization to extend transmission distance and lower system costs, presents simple methods for reducing radiation to low levels. Read full article.



Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project