How Signal Chains and PLCs Impact Our Lives

Mar 29 2012

Figure 1

   

Abstract

It is incredible how many programmable logic controls (PLCs) around us make our modern life possible and pleasant. Machines in our homes heat and cool our air and water, as well as preserve and cook our food. This tutorial explains the importance of PLCs, and describes how to choose component parts using the parametric tools on the Maxim's website.

A similar version of this article was published February 29, 2012 in John Day's Automotive Electronic News.

Introduction

Automation by closed-loop signal-chain control is everywhere. It makes our homes more pleasant. It gives automobiles the ever-widening range of functions that goes beyond the freedom to travel. It is, in fact, quite astounding to look around and realize that so many of the today's products are manufactured with the help a closed-loop signal chain. It is also important to note that in industrial plants and factories, a more complex form of a signal chain is called a programmable logic controller (PLC). In this tutorial, we will see that signal-chain and PLC applications are limited only by our imaginations.

Signal Chains All Around You

Signal chains surround us. They make our modern life possible and pleasant. In fact, an application with a signal chain appears anytime one needs a control loop to monitor, manage, handle, regulate, limit, or organize something.

Machines using signal chains heat and cool air and water in our homes. They chill and cook our food. In industry almost everything that we buy is manufactured utilizing signal chains. Think of your automobile. (Yes, most of us jump into our cars without thinking. We drive our automobiles to work and some people drive using the "bang-bang" approach. This is not the bang-bang servo that we discuss in the Appendix, but actually hitting things.) Automotive antilock brakes, cruise controls, automatic transmissions, and traction controls are examples of signal-chain uses.

A Basic Signal Chain Controls with Feedback

How simple can a signal chain or process control be? Consider a common household oven and an electronic control unit (ECU) in an automobile.

The oven's components are enclosed inside one container, so no long-distance communication is necessary. When the user sets the thermostat to the desired temperature, the oven maintains the internal temperature at the set point (Figure 1).

The smell of cookies in the oven brings back pleasant memories.

The smell of cookies in the oven brings back pleasant memories.

Figure 1. A household oven is a simple example of a signal chain or process feedback control.

Figure 1. A household oven is a simple example of a signal chain or process feedback control.

When the thermostat setting senses that the oven temperature is low, the switch is closed, thus completing the circuit to open the gas valve to the main burner. Once the thermostat detects that the oven has reached the set point, the switch opens, the gas valve closes, and the main burner shuts off. The cycle repeats as needed. The pilot light provides a fail-safe function, while also providing an ignition source for the main burner. If the pilot light were to go out, no voltage would be created by the thermocouple so the main valve would not open.

Modern high-end cars can have up to 80 ECUs. They control engines, antilock brakes, cruise controls, automatic transmissions, and traction. Most ECUs are examples of signal chains because they sense one or more physical parameters, apply a logic or intelligence, and produce an action to benefit the consumer. (See the block diagram of signal-chain feedback in Figure 2). Table 1 outlines the signal-chain functions for various automotive applications.

Table 1. Signal-Chain Applications in an Automobile
Application Parameters Sensed Logic or Intelligence Actions Benefits
Engine control Temperature, air mass; fuel volume; engine speed and rotation angle; throttle position; engine load Optimizes multiple sensor inputs for conditions and maximum benefits Controls air/fuel ratio, ignition timing, idle speed, variable-valve timing Better fuel economy; reduced engine emissions; longer engine life; best power when needed
Antilock brakes Vehicle speed; wheel speed; brake pressure Compares wheel speeds during breaking to identify skidding Controls valves and pumps Increases driver control; decreases stopping distance under most adverse conditions
Cruise control Vehicle speed; engine speed; brake switch Sets and maintains vehicle speed through changing conditions Adjusts throttle position Better fuel economy; driver comfort
Automatic transmissions Throttle position; engine load; kick-down switch; vehicle speed, wheel speed; torque convertor slip Optimizes multiple sensor inputs for conditions Controls shifting; fast under power to minimize band and clutch wear; slow for passenger comfort under lower power loading Better fuel economy; increased transmission life; better vehicle handling; faster shift speed
Traction control Throttle position; engine load; vehicle speed; wheel speed Compares throttle vehicle and wheel for varying road-surface conditions Reduces engine power by removing fuel or spark from cylinder(s) or changing throttle position; applies brakes on one or more wheels Reduces traction loss on acceleration, enhancing driver control

Signal chains are also used for other automotive safety and convenience systems: infotainment; parking assist; airbags; seat belts; door locks; electric windows; running, courtesy, head, and tail lights; power steering; heating; air conditioning; seat control; and telephone...to name a few.

The Difference Between a Signal Chain and a PLC

A signal chain system that goes beyond what is needed for such a small, simple system like a household oven is called a PLC. Recalling that "signal chains are all around you," think next of an industrial factory. What controls and configurations are necessary in a factory? In a fully automated bakery, for example, many subsystems are needed such as weigh scales, valves, flow gauges, mixers, yeast-rising warming chambers, ovens, conveyer belts, fans, and packaging equipment. To be fully automated, the bakery needs a process-control system to manage and coordinate all of the time-critical events among these subsystems. To ensure successful coordination and operation for all these operations, each of these subsystems would include one or more PLCs. Even more complex communications are required when the controllers and the controlled elements are separated by a significant distance. In a complex control environment like a factory with operations spread among several buildings or sites, a PLC spends significant time communicating signals and process events to components throughout the system.

This leads us to the most important difference between a PLC and a signal chain: a PLC makes process change easy. We can illustrate this with a short digression into the history of automation in an automotive factory. An automotive company's strategy to manage change resulted in a PLC.

The Invention of a PLC

Factory automation took hold in the automotive industry when Henry Ford¹ expanded mass-production techniques early in the Twentieth Century. He used fixed assembly stations with the cars moving between positions. The employees learned just a few assembly tasks and performed those tasks for days on end. After many years the changeover for a new car model became very costly and time consuming. The production process was controlled by thousands of hard-wired relays, switches, cam and drum timers, and dedicated closed-loop controllers. To retool for the next model required electricians to mechanically rewire all of the thousands of relays. And then the troubleshooting began to ensure that the safety interlocks, control, and sequencing were all correct.

It was this need to manage the seemingly constant change that resulted in the invention of the PLC. In 1968 Dick Morely and his company were designing a new invention, a programmable controller. Meanwhile General Motors®, (GM®) the automobile company, "wanted a solid-state controller as an electronic replacement for hard-wired relay systems."² GM asked Morley for a quotation to solve their issue. Mr. Morely responded. He is now regarded as the father of the PLC and holds a patent on it.³

GM first used a PLC to assemble automobile automatic transmissions. An assembly plant is made of hundreds of machines that need to be coordinated to function smoothly. The PLC allowed the production line to be repurposed easily. Now a reprogrammed basic machine could be reused to produce a new part.

We can illustrate the pivotal importance of this evolution by focusing on one machine, a numerically controlled (NC) milling machine, and by comparing the old control system with a PLC. First, a human loaded a bare piece of metal on the cutting table and locked it down. Several switches verified that the metal was in the proper position. The operator then indicated that his body was out of danger by pushing two widely spaced buttons, one with each hand. A mechanical guard extended to protect the operator from flying metal shavings. Finally, multiple cutters sculpted the metal in a precise sequence. When the part was complete the mill retracted the tools, stopped all movements, and opened the guard so the human could remove the part and replace it with a new metal blank. Before the PLC, each of these small steps in the operation was hard wired with relays, timers, limit and position switches. It worked reliably...until one needed to make even a small change. The worst possible situation was when a new step needed to be added in the middle of the sequence. Someone might need to unwire all the steps after the new step, add the new step (a hardware relay or timer), and rewire everything that followed.

Enter the PLC. With a PLC that same milling machine becomes a general tool that is controlled and quickly changed a software or logic change. Changing a tool and giving it new instructions now allowed the basic mill to make many different parts. By extending this to the many machines in a factory, an automotive assembly line or other factory quickly adapted to change.

Today you find PLCs used in a modern factories, including an automotive assembly line. Similarly, a chemical, food, or cosmetic company may have to mix many different formulas to make their products. Without the PLC and its easy-to-reconfigure logic, manufacturing changes would still be cumbersome and costly. Many of the items that are common in our lives would be unaffordable.

We use PLCs in our daily lives more than each of us realizes. For other family-oriented examples, see the Appendix.

Factory Automation, Control, and Monitoring

There are areas in a factory that are too dangerous for humans. Fortunately, we have the brains and ability to use machines, and we let a PLC (Figure 2) control those machines.

Figure 2. Diagram of a simple, common signal-chain and PLC loop used in many product disciplines.

Figure 2. Diagram of a simple, common signal-chain and PLC loop used in many product disciplines.

Table 2 summarizes how PLC and signal-chain basics begin once we sense something, usually a physical parameter. Then PLC and signal-chain applications become so numerous and commonplace that we take many of their functions for granted.

Table 2. Measured Parameters that Provide PLC Inputs
Dimensions Pitch Position
Intensity Energy Pressure
Impedance Temperature Humidity
Density Speed Frequency
Viscosity Time of flight Phase
Velocity Distance Time
Acceleration Pressure Salinity
Water purity Torque Volume
Weight State of charge Gasses
Mass Conductivity Ph
Resistance Dissolved oxygen Voltage
Capacitance Ion concentration Current
Inductance Chemicals Level
Rotation Charge (electrons) Color

On the output side of a signal chain or PLC, we monitor a system or we operate or move something. Table 3 shows things monitored or controlled by a PLC.

Table 3. Things Monitored/Controlled by a PLC Output
Valve Pressure Switch
Motor Humidity Solenoid
Pressure Force feedback Lights
Velocity Room entry Weight
Flow Sequence Speed
Volume Authorization Meters
Torque Attenuation Display
Frequency Equalization Calibration
Voltage Communication Time
Current Gain offset Tool
Distance Flux density Pitch
Position Temperature Filter
Power Galvanometers Acceleration
Brightness Air-fuel ration Contrast

Maxim's portfolio is second to none, especially for portable and green energy devices where low-power consumption is critical. Small size is also necessary in such battery-operated devices. Find more information and recommended parts using Maxim's PLC solutions. With new parts appearing on the website daily, the parametric search tool helps engineers select exactly the right part based on electrical criteria.

For example, on the Data Converters Product Page you see a selection of resolutions. Choosing a 12-bit DAC causes the parameter table to be displayed for over 250 parts with 20 parameters (10 less-used parameters are hidden on the left). To use the tables, first click on the "Hidden Columns;" select ICC (mA); click "Hidden Columns;" select ICC (mA); click "Smallest Available Package (mm²)." Now move the slider under ICC (mA) to < 1mA and move the slider under Smallest Available Package (mm²). This shortens the list to over 70 parts. Continue selecting the number of channels, power-on reset (POR) state, output type, and interface to reduce the selection to a manageable numbers of parts and data sheets.

There is another example of the easy-to-use web functions for parts selection. Return to the home page (click the Maxim logo at the upper left of most pages). Mouse over "Power Management" in the left column and select "Voltage References." Now you can select a voltage, or "low power" or "small package" to see featured products.

Need more help? We have field support with Maxim and distribution sales and field application engineers worldwide.

Conclusion

Control-loop signal chains or PLCs, in relatively simple or complex applications, are found all around us. They heat and cool, and keep a temperature constant in any structure, regardless of size. Signal chains monitor and control antilock brakes, cruise controls, automatic transmissions, and traction controls in automobiles. Many household appliances today contain a signal chain. We spoke about an oven, but the list is seemingly endless: the microwave; washers and dryers; and even the lawn sprinkler that can sense ground moisture and regulate water use. Finally, it is important to remember that all these goods are produced in a factory where a PLC monitors and controls most every electronic system that operates or moves.

References

  1. For more information on Henry Ford and factory automation of automobiles, you can start here (http://en.wikipedia.org/wiki/Assembly_line).
  2. Dunn, Allison, "The father of invention: Dick Morley looks back on the 40th anniversary of the PLC," Manufacturing Automation Magazine, September 12, 2008, www.automationmag.com/features/the-father-of-invention-dick-morley-looks-back-on-the-40th-anniversary-of-the-plc.html.
  3. Dick Morley is known as the "father" of the PLC. His US Patent 3,761,893 is the basis of many PLCs today. http://patft.uspto.gov/netahtml/PTO/srchnum.htm.

Appendix: More PLCs in the Home

In a home, my home, we use a PLC in the crudest possible way. We have a "bang-bang servo," which is basically an old-fashioned human intervention for our heating, ventilating, and air-conditioning (HVAC) system. Bang-bang servos work because the system has a bandwidth so incredibly low that things change over minutes and hours. The thermal inertia of the walls, floor, and ceiling in our homes is very high, so a simple on/off thermostat controls heating and the air conditioning. Meanwhile, ventilation uses the most expensive and complex servo loop possible: a whole house fan pulls in air through open doors and windows and then exhausts it through the attic. The servo is very complex because it operates on human intervention. During the day we choose to use the fan instead of air conditioning to save energy. A timer turns the fan off at which time we have to shut the doors and windows.

Operation of the heating and air-conditioning control system is, theoretically, simpler than the bang-bang method above, but humans can complicate anything. The system is controlled by a bimetallic thermostat; the heater runs until the set point is exceeded. The heater turns off until the bimetallic strip cools and then the heater goes back on and repeats the cycle. The opposite happens for cooling. Depending on the weather, the heat loss or gain in the house changes the duty cycle of the on- and off-times. It is simple and reliable.

So much for theory of operation...humans have a propensity to complicate even the simplest systems with unexpected and often comical consequences. We replaced the old natural gas-fired forced-air heater with a modern high-efficiency furnace. This did two great things: it got me a lot of points with my wife because the new furnace fits entirely in the attic crawl space; and we have the prospect of saving money over time. The old furnace used a metal pipe to exhaust the very hot combustion products. The new one is a condensing furnace with the exhaust through a plastic pipe, and the air is just warm to the touch. At the same time we installed a more efficient air conditioner and a new thermostat. The new thermostat works well, but it is our human sensibilities that are skewed. First, it is digital, has a microprocessor and a real-time clock (RTC). It has many modes, more than we ever use. Now I have to learn how to program it. (My wife does not program it because she put it on my task list.) Second, placebos have powerful effects on humans. The old thermostat had hysteresis. It might have been as large as three or four degrees but we did not know and did not care. Now we both peek at the display as we walk past and get a silly, knowing smile.



Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

MAX6126
PRODUCTION

Ultra-High-Precision, Ultra-Low-Noise, Series Voltage Reference

MAX6033
PRODUCTION

High-Precision, Low-Dropout SOT23 Series Voltage Reference

MAX5420
PRODUCTION

Digitally Programmable Precision Voltage Divider for PGAs

MAX9914 PRODUCTION

1MHz, 20µA, Rail-to-Rail I/O Op Amps with Shutdown

MAX9913 PRODUCTION

200kHz, 4µA, Rail-to-Rail I/O Op Amps with Shutdown

MAX9910 PRODUCTION

200kHz, 4µA, Rail-to-Rail I/O Op Amps with Shutdown

MAX9917 PRODUCTION

1MHz, 20µA, Rail-to-Rail I/O Op Amps with Shutdown

MAX5154 PRODUCTION

Low-Power, Dual, 12-Bit Voltage-Output DACs with Serial Interface

MAX5235 PRODUCTION

Single-Supply 3V/5V, Voltage-Output, Dual, Precision 12-Bit DACs

MAX5130 PRODUCTION

+3V/+5V, 13-Bit, Serial, Voltage-Output DACs with Internal Reference

MAX5177 PRODUCTION

Low-Power, Serial, 12-Bit DACs with Force-Sense Voltage-Output

MAX5270B

Octal, 13-Bit Voltage-Output DAC with Parallel Interface

MAX5764

32-Channel, 16-Bit, Voltage-Output DACs with Serial Interface

MAX5443 PRODUCTION

+3V/+5V, Serial-Input, Voltage-Output, 16-Bit DACs

MX7548 PRODUCTION

CMOS, 8-Bit-Compatible, 12-Bit DAC

MAX5170 PRODUCTION

Low-Power, Serial, 14-Bit DACs with Voltage-Output

MAX551 PRODUCTION

+3V/+5V, 12-Bit, Serial, Multiplying DACs in 10-Pin µMAX Package

MAX5722 PRODUCTION

12-Bit, Low-Power, Dual, Voltage-Output DAC with Serial Interface

MAX5306 PRODUCTION

Low-Power, Low-Glitch, Octal 12-Bit Voltage-Output DACs with Serial Interface

MAX5712 PRODUCTION

Low-Power, 12-Bit, Rail-to-Rail Voltage-Output Serial DAC in SOT23

MAX5200 NOT RECOMMENDED FOR NEW DESIGNS

Low-Cost, Voltage-Output, 16-Bit DACs with Internal Reference in µMAX

MAX532 PRODUCTION

Dual, Serial Input, Voltage-Output, Multiplying, 12-Bit DAC

MAX5531 PRODUCTION

Ultra-Low-Power, 12-Bit, Voltage-Output DACs

MAX5631 Obsolete

16-Bit DACs with 32-Channel Sample-and-Hold Outputs

MAX5153 Obsolete

Low-Power, Dual, 13-Bit Voltage-Output DACs with Configurable Outputs

MAX5143 PRODUCTION

+3V/+5V, Serial-Input, Voltage-Output, 14-Bit DACs

MAX5234

Single-Supply 3V/5V, Voltage-Output, Dual, Precision 12-Bit DACs

MAX5735 PRODUCTION

32-Channel, 16-Bit, Voltage-Output DACs with Serial Interface

MAX5156 PRODUCTION

Low-Power, Dual, 12-Bit Voltage-Output DACs with Configurable Outputs

MAX5322 PRODUCTION

±10V, Dual, 12-Bit, Serial, Voltage-Output DAC

MAX5312 Obsolete

±10V, 12-Bit, Serial, Voltage-Output DAC

MAX5207 NOT RECOMMENDED FOR NEW DESIGNS

Low-Cost, Voltage-Output, 16-Bit DACs in µMAX

MAX5544 PRODUCTION

Low-Cost, +5V, Serial-Input, Voltage-Output, 14-Bit DAC

MAX5291 PRODUCTION

Buffered, Fast-Settling, Dual, 12-/10-/8-Bit, Voltage-Output DACs

MAX5534 PRODUCTION

Dual, Ultra-Low-Power, 12-Bit, Voltage-Output DACs

MAX5839B

Octal, 13-Bit Voltage-Output DAC with Parallel Interface

MX7547 PRODUCTION

CMOS, Parallel Loading, Dual, 12-Bit Multiplying DAC

MX7535 PRODUCTION

Microprocessor-Compatible, 14-Bit DACs

MX7837 PRODUCTION

Complete, Dual, 12-Bit Multiplying DAC with 8-Bit Bus Interface

MX7521 PRODUCTION

CMOS, 14- and 12-Bit Multiplying DACs

MAX545 PRODUCTION

+5V, Serial Input, Voltage-Output 14-Bit DACs

MAX535 PRODUCTION

Low-Power, 13-Bit Voltage-Output DACs with Serial Interface

MAX5139 PRODUCTION

Low-Power, Single, 16-/12-Bit, Buffered Voltage-Output DACs

MAX508 PRODUCTION

Voltage-Output, 12-Bit DAC with Internal Reference and 12-Bit Interface

MAX5264

Octal, 14-Bit, Voltage-Output DAC with Parallel Interface for ATE

MAX5142 PRODUCTION

+3V/+5V, Serial-Input, Voltage-Output, 14-Bit DACs

MAX5132 PRODUCTION

+5V/+3V, 13-Bit, Serial, Force/Sense DACs with 10ppm/°C Internal Reference

MAX5352 PRODUCTION

Low-Power, 12-Bit Voltage-Output DACs with Serial Interface

MAX5155 PRODUCTION

Low-Power, Dual, 12-Bit Voltage-Output DACs with Serial Interface

MAX5104 PRODUCTION

Low-Power, Dual, Voltage-Output, 12-Bit DAC with Serial Interface

MAX5290 PRODUCTION

Buffered, Fast-Settling, Dual, 12-/10-/8-Bit, Voltage-Output DACs

MX7845 PRODUCTION

Complete, 12-Bit Multiplying DAC

MAX5533 PRODUCTION

Dual, Ultra-Low-Power, 12-Bit, Voltage-Output DACs

MAX5839A

Octal, 13-Bit Voltage-Output DAC with Parallel Interface

MX7248 PRODUCTION

Complete, 12-Bit, Voltage-Output Multiplying DAC

MAX5812 PRODUCTION

12-Bit Low-Power, 2-Wire, Serial Voltage-Output DAC

MAX5172 Obsolete

Low-Power, Serial, 14-Bit DACs with Voltage-Output

MX7534 PRODUCTION

Microprocessor-Compatible, 14-Bit DACs

MAX5202 NOT RECOMMENDED FOR NEW DESIGNS

Low-Cost, Voltage-Output, 16-Bit DACs with Internal Reference in µMAX

MAX5633 PRODUCTION

16-Bit DACs with 32-Channel Sample-and-Hold Outputs

MX7542 RECOMMENDED FOR NEW DESIGNS

CMOS, 12-Bit, µP-Compatible DAC

MAX5144 PRODUCTION

+3V/+5V, Serial-Input, Voltage-Output, 14-Bit DACs

MAX5134 PRODUCTION

Pin-/Software-Compatible, 16-/12-Bit, Voltage-Output DACs

MAX507 PRODUCTION

Voltage-Output, 12-Bit DAC with Internal Reference and 12-Bit Interface

MAX5842 PRODUCTION

Quad, 12-Bit, Low-Power, 2-Wire, Serial Voltage-Output DAC

MAX5253 PRODUCTION

+3V, Quad, 12-Bit Voltage-Output DAC with Serial Interface

MAX5131

+3V/+5V, 13-Bit, Serial, Voltage-Output DACs with Internal Reference

MAX5590 PRODUCTION

Buffered, Fast-Settling, Octal, 12/10/8-Bit, Voltage-Output DACs

MAX5121 PRODUCTION

+3V/+5V, 12-Bit, Serial, Voltage-Output DACs with Internal Reference

MAX5351 PRODUCTION

Low-Power, 13-Bit Voltage-Output DACs with Serial Interface

MX7537 PRODUCTION

CMOS, Parallel Loading, Dual, 12-Bit Multiplying DAC

MAX547 PRODUCTION

Octal, 13-Bit Voltage-Output DAC with Parallel Interface

MAX537 PRODUCTION

Calibrated, Quad, 12-Bit Voltage-Output DACs with Serial Interface

MAX5171 PRODUCTION

Low-Power, Serial, 14-Bit DACs with Force-Sense Voltage-Output

MAX552 PRODUCTION

+3V/+5V, 12-Bit, Serial, Multiplying DACs in 10-Pin µMAX Package

MX7839

Octal, 13-Bit Voltage-Output DAC with Parallel Interface

MAX542 PRODUCTION

+5V, Serial-Input, Voltage-Output 16-Bit DACs

MAX5201 NOT RECOMMENDED FOR NEW DESIGNS

Low-Cost, Voltage-Output, 16-Bit DACs with Internal Reference in µMAX

MAX5134A

Pin-/Software-Compatible, 16-/12-Bit, Voltage-Output DACs

MAX5632

16-Bit DACs with 32-Channel Sample-and-Hold Outputs

MX7541 PRODUCTION

CMOS, 12-Bit Multiplying DAC

MAX5133

+5V/+3V, 13-Bit, Serial, Force/Sense DACs with 10ppm/°C Internal Reference

MAX5123 PRODUCTION

+5V/+3V, 12-Bit, Serial, Force/Sense DACs with 10ppm/°C Internal Reference

MAX526 PRODUCTION

Calibrated, Quad, Voltage-Output, 12-Bit DAC

MAX5150 PRODUCTION

Low-Power, Dual, 13-Bit Voltage-Output DACs with Serial Interface

MAX5120 PRODUCTION

+3V/+5V, 12-Bit, Serial, Voltage-Output DACs with Internal Reference

MAX502 PRODUCTION

Voltage-Output, 12-Bit Multiplying DACs

MAX5742 PRODUCTION

12-Bit, Low-Power, Quad, Voltage-Output DAC with Serial Interface

MAX5732 PRODUCTION

32-Channel, 16-Bit, Voltage-Output DACs with Serial Interface

MAX5174 Obsolete

Low-Power, Serial, 12-Bit DACs with Voltage-Output

MX7536 PRODUCTION

µP-Compatible, 14-Bit DAC

MAX5157 PRODUCTION

Low-Power, Dual, 12-Bit Voltage-Output DACs with Configurable Outputs

MAX5774 PRODUCTION

32-Channel, 14-Bit, Voltage-Output DACs with Serial Interface

MAX5204 NOT RECOMMENDED FOR NEW DESIGNS

Low-Cost, Voltage-Output, 16-Bit DACs in µMAX

MAX536 PRODUCTION

Calibrated, Quad, 12-Bit Voltage-Output DACs with Serial Interface

MAX5541 PRODUCTION

Low-Cost, +5V, Serial-Input, Voltage-Output, 16-Bit DAC

MX7847 PRODUCTION

Complete, Dual, 12-Bit Multiplying DAC with 8-Bit Bus Interface

MAX5535 PRODUCTION

Dual, Ultra-Low-Power, 12-Bit, Voltage-Output DACs

MAX5353 PRODUCTION

Low-Power, 12-Bit Voltage-Output DACs with Serial Interface

MAX5231 PRODUCTION

3V/5V, 12-Bit, Serial Voltage-Output Dual DACs with Internal Reference

MAX5302 PRODUCTION

Low-Power, 12-Bit Voltage-Output DAC with Serial Interface

MAX541 PRODUCTION

+5V, Serial-Input, Voltage-Output 16-Bit DACs

MAX531 PRODUCTION

+5V, Low-Power, Voltage-Output, Serial 12-Bit DACs

MAX5661 PRODUCTION

Single 16-Bit DAC with Current and Voltage Outputs for Industrial Analog Output Modules

MAX5136 PRODUCTION

Pin-/Software-Compatible, 16-/12-Bit, Voltage-Output DACs

MAX5122 PRODUCTION

+5V/+3V, 12-Bit, Serial, Force/Sense DACs with 10ppm/°C Internal Reference

MAX525 PRODUCTION

Low-Power, Quad, 12-Bit Voltage-Output DAC with Serial Interface

MAX5621

16-Bit DACs with 16-Channel Sample-and-Hold Outputs

MAX501 PRODUCTION

Voltage-Output, 12-Bit Multiplying DACs

MAX5442 PRODUCTION

+3V/+5V, Serial-Input, Voltage-Output, 16-Bit DACs

MAX5173 PRODUCTION

Low-Power, Serial, 14-Bit DACs with Force-Sense Voltage-Output

MAX5773

32-Channel, 14-Bit, Voltage-Output DACs with Serial Interface

MAX5203 PRODUCTION

Low-Cost, Voltage-Output, 16-Bit DACs with Internal Reference in µMAX

MAX539 PRODUCTION

+5V, Low-Power, Voltage-Output, Serial 12-Bit DACs

MAX5270A

Octal, 13-Bit Voltage-Output DAC with Parallel Interface

MAX5530 PRODUCTION

Ultra-Low-Power, 12-Bit, Voltage-Output DACs

MX7245 PRODUCTION

Complete, 12-Bit, Voltage-Output Multiplying DAC

MX7543 PRODUCTION

CMOS, 12-Bit, Serial-Input DAC

MX7531 Obsolete

CMOS, 10-Bit Multiplying DAC

MAX5230 PRODUCTION

3V/5V, 12-Bit, Serial Voltage-Output Dual DACs with Internal Reference

MAX530 PRODUCTION

+5V, Low-Power, Parallel-Input, Voltage-Output, 12-Bit DAC

MAX5152 PRODUCTION

Low-Power, Dual, 13-Bit Voltage-Output DACs with Configurable Outputs

MAX5135 PRODUCTION

Pin-/Software-Compatible, 16-/12-Bit, Voltage-Output DACs

MAX5591 PRODUCTION

Buffered, Fast-Settling, Octal, 12/10/8-Bit, Voltage-Output DACs

MAX514

CMOS Quad, 12-Bit, Serial-Input Multiplying DAC

MAX5581 Obsolete

Buffered, Fast-Settling, Quad, 12-/10-/8-Bit, Voltage-Output DACs

MAX5441 PRODUCTION

+3V/+5V, Serial-Input, Voltage-Output, 16-Bit DACs

MAX5734 PRODUCTION

32-Channel, 16-Bit, Voltage-Output DACs with Serial Interface

MAX5176

Low-Power, Serial, 12-Bit DACs with Voltage-Output

MX7538 PRODUCTION

CMOS, µP-Compatible, 14-Bit DAC

MAX544 PRODUCTION

+5V, Serial Input, Voltage-Output 14-Bit DACs

MAX5206 PRODUCTION

Low-Cost, Voltage-Output, 16-Bit DACs in µMAX

MAX538 PRODUCTION

+5V, Low-Power, Voltage-Output, Serial 12-Bit DACs

MAX5762

32-Channel, 16-Bit, Voltage-Output DACs with Serial Interface

MX7841

Octal, 14-Bit Voltage-Output DAC with Parallel Interface

MAX5822 PRODUCTION

Dual, 12-Bit, Low-Power, 2-Wire, Serial Voltage-Output DAC

MAX5138 PRODUCTION

Low-Power, Single, 16-/12-Bit, Buffered Voltage-Output DACs

MAX5151 PRODUCTION

Low-Power, Dual, 13-Bit Voltage-Output DACs with Serial Interface

MAX5141 PRODUCTION

+3V/+5V, Serial-Input, Voltage-Output, 14-Bit DACs

MAX527 PRODUCTION

Calibrated, Quad, Voltage-Output, 12-Bit DAC

MAX5580 PRODUCTION

Buffered, Fast-Settling, Quad, 12-/10-/8-Bit, Voltage-Output DACs

MX7541A PRODUCTION

CMOS, 12 Bit Multiplying D/A Converter

MAX5775

32-Channel, 14-Bit, Voltage-Output DACs with Serial Interface

MAX5444 PRODUCTION

+3V/+5V, Serial-Input, Voltage-Output, 16-Bit DACs

MAX5733 PRODUCTION

32-Channel, 16-Bit, Voltage-Output DACs with Serial Interface

MAX5175

Low-Power, Serial, 12-Bit DACs with Force-Sense Voltage-Output

MAX5307 PRODUCTION

Low-Power, Low-Glitch, Octal 12-Bit Voltage-Output DACs with Serial Interface

MAX5500 PRODUCTION

Low-Power, Quad, 12-Bit Voltage-Output DACs with Serial Interface

MAX543 PRODUCTION

Serial, CMOS, Multiplying, 12-Bit DAC in 8-Pin Package

MAX5205 PRODUCTION

Low-Cost, Voltage-Output, 16-Bit DACs in µMAX

MX7545A PRODUCTION

CMOS 12-Bit Buffered Multiplying DACs

MAX5532 PRODUCTION

Dual, Ultra-Low-Power, 12-Bit, Voltage-Output DACs

MX7545 PRODUCTION

CMOS, Buffered, 12-Bit Multiplying DAC

MAX5137 PRODUCTION

Pin-/Software-Compatible, 16-/12-Bit, Voltage-Output DACs

MAX1393

1.5V to 3.6V, 312.5ksps, 1-Channel True-Differential/2-Channel Single-Ended, 12-Bit, SAR ADCs

MAX1391

1.5V to 3.6V, 416ksps, 1-Channel True-Differential/2-Channel Single-Ended, 8-Bit, SAR ADCs

MAX5403 PRODUCTION

Dual, 256-Tap, Low-Drift, Digital Potentiometers in 10-µMAX

MAX5405 PRODUCTION

Dual, 256-Tap, Low-Drift, Digital Potentiometers in 10-µMAX

MAX5421 PRODUCTION

Digitally Programmable Precision Voltage Divider for PGAs

Product Categories

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project