How to Modify an Existing Design from a TDA5200 or TDA5201 to a MAX1470 Superheterodyne Receiver

Jun 29 2002

Abstract

This application note covers the step-by-step procedure required to replace the TDA5200 or TDA5201 in a design with the MAX1470 supeheterodyne receiver.

If you have been looking into modifying your existing Infineon receiver board with a MAX1470 to take advantage of its unique features, this app note is for you. Figure 1 shows a typical TDA5200/TDA5201 based circuit tuned to receive 433.92MHz signals, and the four simple steps needed to upgrade this TDA5200/TDA5201 receiver board to the MAX1470.

Equipment/components needed:

  • Your assembled receiver board
  • A soldering iron
  • A MAX1470 IC
  • A 6.6128MHZ (433.92MHz operation) or a 4.7547MHz (315MHz operation) crystal
  • 2x100pF and 1x3.0pF capacitors for 433.92MHz or 2x100pF and 1x4.7pF capacitors for 315MHz operation
  • 1x68nH, and 2x15nH inductors for 433.92MHz or 1x15nH, 1x27nH, and 1x120nH inductors for 315MHz operation

Or call +1 (408) 601-1000x6503 and request a conversion kit. Please specify frequency of operation.

Figure 1. Typical TDA5200 based circuit (433.92MHz) and the four conversion steps.

Figure 1. Typical TDA5200 based circuit (433.92MHz) and the four conversion steps.

The four simple steps for this conversion are described here:

  1. Supply voltage: The MAX1470 requires a 3.3V supply. Care must then be taken not to connect the TDA's 5V supply to the MAX1470 based circuit.
  2. IC and XTAL oscillator: Replace the TDA5200 with the MAX1470. The MAX1470 PLL uses a 64x clock divider which forces the XTAL to be 6.6128MHz for a 433.92MHz receive frequency. Depending on the crystal used, capacitors C15 and C16 may have to be different, to compensate for the crystal being pulled away from its stated operating frequency due to the difference in load capacitance. This is referred to as crystal pulling. Refer to application note 1017, "How to Choose a Quartz Crystal Oscillator for the MAX1470 Superheterodyne Receiver" for more details.
  3. Input matching and degeneration inductor: The MAX1470 based design replaces C1, C2, C3, and L1 with a series 100pF cap and a series 68nH inductor. In addition, replace C5 with a 15nH inductor. The two new inductors will need to be positioned in place of the C3 and C5 capacitors. The values given in Table 1 are nominal but may need to be slightly tuned since they can be affected by the PC board traces.
  4. LC tank and mixer input. L2, C6, and C8 will have to be changed to the values listed in Table 1. Once again, the values given are nominal but may need to be slightly tuned since they are affected by the PC board traces.

Table 1 lists all the component changes. Although not required above, resistors R2 and R3 can be removed for a lower component count.

Table 1. Component differences between the TDA5200 and MAX1470 based designs
  Infineon Circuit Maxim Circuit
Supply 5V 3.3V
IC TDA5200/1 MAX1470
XTAL 13.2256MHz 6.6128MHz (433.92MHz), 4.7547MHz (315MHz)
R1 100K Unchanged
R2 120K None
R3 180K None
L1 15nH None
L2 10nH 15nH (433.92MHz) 27nH (315MHz)
C1 1pF 100pF
C2 4.7pF None
C3 6.8pF L=68nf (433.92MHz) 120nH (315MHz)
C4 100pF Unchanged or 10nF
C5 47nF L=15nH
C6 8.2pF 3.0pf (433.92MHz) 4.7pF (315MHz)
C7 100pF Unchanged
C8 100pF 100pF
C9 100pF Unchanged
C10 10nF Unchanged
C11 10nF Unchanged
C12 220pF Unchanged
C13 47nF Unchanged
C14 470pF Unchanged
C15 15pF Unchanged
C16 8.2pF 15pF

The resulting circuit is shown in Figure 2.

Figure 2. Typical MAX1470 based circuit (433.92MHz).

Figure 2. Typical MAX1470 based circuit (433.92MHz).

If the tank tuning and antenna matching are done correctly, you should expect the sensitivity to exceed -112dBm (315MHz), or -108dBm (433.92MHz). Image rejection is typically 53dB at 315MHz and 35dB at 433.92MHz.



Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

Product Categories

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project