Interfacing a DS1868 3-Wire Device to a SPI Bus

Dec 26 2001

Abstract

The DS1868 uses a dual digital potentiometer with a 3-wire (shift register) interface. This application note describes the logic and firmware required to interface the DS1868, as well as any other Dallas Semiconductor 3-wire devices to the Motorola SPI bus.

Introduction to DS1868

The DS1868 is a dual digital potentiometer with a 3-wire interface. This application note will describe how to interface a Dallas Semiconductor 3-wire device to a microcontroller with a SPITM interface.

Comparing SPI And 3-Wire Interfaces

The SPI and 3-wire are different serial interfaces but they are compatible. The following section describes the differences.

Serial Peripheral Interface (SPI)

The SPI has 4 signals: SDO, SDI, SCK, and active-low SS. The SDO signal is data out, SDI is data in, SCK is the clock, and active-low SS is the slave select.

3-Wire Serial Interface

The 3-wire serial interface has 4 signals: DQ, Cout, active-low RST and CLK. The data in is on the DQ signal, data out is on the Cout signal, active-low RST signal enables the 3-wire interface, and CLK is the clock.

Table 1. 3-Wire vs. SPI Interface.
Serial Interface Signal names Signal Descriptions BUS Speed (Typical) Data Format
3-WIRE DQ Data In 500kHz to 5 MHz LSB first, MSB last
Cout Data Out
active-low RST active-low Reset
CLK Clock
SPI SDI Data In 10MHz MSB first, LSB last
SDO Data Out
active-low SS active-low Slave Select
SCK Clock
Note: In this application note, active-low SS is not used (only used when in slave mode).

Writing/Reading Bytes

Writing Data to DS1868


The microcontroller, which contains an SPI interface, transmits and receives data in multiples of 8 bits. Therefore, 7 additional bits need to be sent along with the 17 bits of data for a total of 3 bytes. The microcontroller sends the MSB first. When the microcontroller writes data to the DS1868, the first 7 bits of the first byte are pushed out of the shift register and b0 contains the LSB of the first byte (see Figure 1).

Figure 1. Shift register with 7 additional bits during a write.

Figure 1. Shift register with 7 additional bits during a write.

Reading Data from the DS1868

When the microcontroller reads the data from the DS1868, the stack select bit (b0) gets transmitted first, then the MSB of Pot 1 (b1) and so on (see Figure 2). When reading, the extra 7 bits are located in the third byte.

Figure 2. 17-Bit Shift register.

Figure 2. 17-Bit Shift register.

The following is an example of how bytes are written and read. In this example the stack select bit selects Pot 1. Pot 1 is programmed to 0Fh and Pot 0 is programmed to 55h. The value of the selected pot's wiper will be on the SOUT pin. The three bytes that are written to the DS1868 are 01h, 0Fh, and 55h. The leading zeros of 01h are the 7 additional bits. The microcontroller sends the MSB first so the leading 7 zeros are first transmitted. These leading zeros fall off the end and the '1' ends up in b0. Pot 1 will have the first 4 bits filled with 0s and the last 4 bits filled with 1s. The MSB in Pot 0 will be a '0' with the remaining bits alternating between 1 and 0.

Byte 0: 00000001b (01h) The additional bits are underlined.
Byte 1: 00001111b (0Fh)
Byte 2: 01010101b (55h)

When the data is read, b0 is the first bit out. The 3 bytes that are output will now read as follows:

Byte 0: 10000111 (87h)
Byte 1: 10101010 (AAh)
Byte 2: 10000000 (80h) The additional bits are underlined.
The 7 additional bits are now at the end of Byte 2.

More examples of converting written to read data are in Table 2.

The software compares the bytes written to the bytes read from the DS1868 (see the Appendix).

Table 2. Converting Data Bytes Between Writing and Reading
3 Bytes Written (hex) 3 Bytes Written (binary) Pot Settings
SS Pot1 Pot0
3 Bytes Read (hex) 3 Bytes Read (binary)
01h FFh 80h 00000001
11111111
10000000
1 FFh 80h FFh C0h 00h 11111111
11000000
00000000
01h 80h 80h 00000001
10000000
10000000
1 FFh 80h C0h 40h 00h 11000000
01000000
00000000
00h 80h 0Fh 00000000
10000000
00001111
0 80h 0Fh 40h 07h 80h 01000000
00000111
10000000

Hardware Configuration

A schematic of the board is shown in Figure 3.

Figure 3. Board Schematic.

Figure 3. Board Schematic.

Software Configuration

The software configuration is for a PIC16F872.

Port Settings

The TRISx register sets the pins to an input (1) or an output (0). The PORTA register will drive active-low RST and LED to 5V or 0V.

TRISA = --1xxx00—RA5active-low SS is set to an input. This is used to enable the serial port. RA0 and RA1 are set to outputs for the active-low RST and LED
TRISB = Not used
TRISC = xx010xxx—Clears SCK and SDO, sets SDI

The active-low RST pin needs to be set before data is transmitted/received and then needs to be cleared after the transaction is complete.

SPI Settings

SSPSTAT = 01000000 (40h)—bit SMP = 0, bit CKE = 1
When SMP = 0, the input data is sampled at the end of data output time.
When CKE = 1, transmit happens on transition from active clock state to idle clock state when CKP = 0.

The SSPSTAT register sets up the clock and data to have the correct timing to interface with the DS1868.

SSPCON = 00100001 (21h)—bit SSPEN = 1, bit SSPM3-0 = 0001
SSPEN = 1 enables the serial port.
SSPM3-0 selected the clock frequency. SSPM3-0 = 0001 = Fosc/16 = 20MHz/16 = 1.25MHz

The DS1868 has a maximum clock rate of 10MHz.

Code

The Appendix contains the assembly code to write, read, and compare potentiometer data.

Each port that is used needs to be initialized in addition to the SPI port. The potentiometers also need to be initialized to zero. Then data can be written to the potentiometers.

SPI Timing

Using the register settings described above, the microcontroller produces the following timing signals.

Figure 4. SPI timing diagram.

Figure 4. SPI timing diagram.

Transmission of the data on SDO is completed on the falling edge of the clock. Data is received on SDI during the clock cycle. The following are diagrams of the potentiometer data being received and transmitted. Figure 5 shows 01h, FFh, and 80h being sent to the DS1868 on the SDO line. SDI contains the data the DS1868 sends back to the microcontroller. The data on SDI is FFh, C0h, and 00h. See Table 2 for more information on converting data.

Figure 5. Data transmitted/received.

Figure 5. Data transmitted/received.

Transmission of the data on SDO is completed on the falling edge of the clock. Data is received on SDI during the clock cycle. The following are diagrams of the potentiometer data being received and transmitted. Figure 5 shows 01h, FFh, and 80h being sent to the DS1868 on the SDO line. SDI contains the data the DS1868 sends back to the microcontroller. The data on SDI is FFh, C0h, and 00h. See Table 2 for more information on converting data.

Figure 6 shows 01h, 80h, and 80h being sent to the DS1868. The data is then compared to C0h, 40h, and 00h. See Table 2 for more information on converting data.

Figure 6. Data transmitted/received (detail).

Figure 6. Data transmitted/received (detail).

Appendix

Assembly Code using the PIC16F872


; *****************
; App Note Code
; The following code was developed on the PIC16F872.
; *****************
LIST p=16F872
#INCLUDE <p16f872.inc>
GOTO MAIN
; ***Subroutines***
; Delay for LED
WAIT MOVWF 0x23
MOVLW 0x20
MOVWF 0x20
DEC1 DECFSZ 0x20
GOTO LOOP1
RETURN
LOOP1 MOVLW 0xFF
MOVWF 0X21
DEC2 DECFSZ 0X21
GOTO LOOP2
GOTO DEC1
LOOP2 MOVLW 0xFF
MOVWF 0x22
DEC3 DECFSZ 0X22
GOTO DEC3
GOTO DEC2
; *************************************
; Test to Determine is TX is Complete
DONE BSF STATUS, RP0 ; Select Bank 1
BTFSS SSPSTAT,0 ; Test SSPBUF to determine if TX is complete
GOTO DONE
RETURN

; **************************************
; Initialize PORTA
INITA BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
CLRF PORTA ; Clear output data latches
BSF STATUS, RP0 ; Select Bank 1
MOVLW 0x06 ; All outputs set digital
MOVWF ADCON1
MOVLW 0x20 ; Value used to initialize data direction
MOVWF TRISA ; LED and active-low RST outputs
BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
BSF PORTA, 1 ; LED off
BCF PORTA, 0 ; active-low RST = 0V
RETURN
; **************************************
; Initialize PORTC
INITC BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
CLRF PORTC ; Clear output data latches
BSF STATUS, RP0 ; Select Bank 1
MOVLW 0x10 ; Value used to initialize data direction
MOVWF TRISC ; Clears SCK and SDO, sets SDI
RETURN
; **************************************
; Initialize SPI
SPI BSF STATUS, RP0 ; Select Bank 1
MOVLW 0x40
MOVWF SSPSTAT ; SMP=0, CKE=1: These bits set up the data & clock.
BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
MOVLW 0x21
MOVWF SSPCON ; SSPEN=1, CKP=SSPMx=0001 (Fosc/16)
RETURN

; ***************************************
; Initialize POT1
WRITE0 BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
BSF PORTA, 0 ; active-low RST = 5V
MOVLW 0x00 ; Clear Byte 0
MOVWF SSPBUF
CALL DONE ; Test SSPBUF to determine if TX is complete
BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
MOVLW 0x00 ; Clear Byte 1
MOVWF SSPBUF
CALL DONE ; Test SSPBUF to determine if TX is complete
BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
MOVLW 0x00 ; Clear Byte 2
MOVWF SSPBUF
CALL DONE ; Test SSPBUF to determine if TX is complete
BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
BCF PORTA, 0 ; active-low RST = 0V
RETURN

; ***************************************
; Write to Pot1
WRITE BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
BSF PORTA, 0 ; active-low RST = 5V
MOVLW 0x01 ; Stack Select bit = 1 (Byte 0)
MOVWF SSPBUF
CALL DONE
BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
MOVLW 0xFF ; Pot1 = FF (Byte 1)
MOVWF SSPBUF
CALL DONE
BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
MOVLW 0x80 ; Pot0 = 80 (Byte 2)
MOVWF SSPBUF
CALL DONE
BCF STATUS, RP0 ; Bank0
BCF STATUS, RP1
BCF PORTA, 0 ; active-low RST = 0V
RETURN
; ***************************************
; Compare Data Transmitted and Received
CMPR BCF STATUS, RP ; Select Bank 0
BCF STATUS, RP1
BSF PORTA, 0 ; active-low RST = 5V
MOVLW 0x01 ; Write Byte 0
MOVWF SSPBUF
BCF PORTA, 1 ; LED on
CALL DONE
BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
MOVF SSPBUF, 0 ; Read Byte 0
XORLW 0xFF
BTFSS STATUS, 2
GOTO FAIL

MOVLW 0xFF ; Write Byte 1
MOVWF SSPBUF
CALL DONE
BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
MOVF SSPBUF, 0 ; Read Byte 1
XORLW 0xC0
BTFSS STATUS, 2
GOTO FAIL
MOVLW 0x80 ; Write Byte 2
MOVWF SSPBUF
CALL DONE
BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
MOVF SSPBUF, 0 ; Read Byte 2
ANDLW 0x80
BTFSS STATUS, 2
GOTO FAIL
BCF PORTA, 0 ; active-low RST = 0V
GOTO PASS
RETURN
; ***************************************
; If Compare Fails
FAIL BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
CLRF PORTA ; Initialize PORTA by clearing output data latches
BSF STATUS, RP0 ; Select Bank 1
MOVLW 0x06 ; All outputs set digital
MOVWF ADCON1
MOVLW 0x20 ; Value used to initialize data direction
MOVWF TRISA ; LED on and active-low RST high
BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
BCF PORTA, 1 ; LED on
CALL WAIT
BSF PORTA, 1 ; LED off
CALL WAIT
GOTO FAIL ; Repeat blinking LED

; ***********************************
; If Compare Passes
PASS BCF STATUS, RP0 ; Select Bank 0
BCF STATUS, RP1
BCF PORTA, 1 ; LED on
GOTO PASS ; LED remains on
; ******THE MAIN PROGRAM********
MAIN CALL INITA ; Initialize PORTA
CALL INITC ; Initialize PORTC
CALL SPI ; Initialize SPI
CALL WRITE0 ; Initialize Pots
CALL WRITE ; Write data to pots
CALL CMPR Compare data written to pots w/ data received from pots
END</p16f872.inc>


Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Product Categories

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project