LTspice: Computing the Average or RMS Value of a Trace

Nov 6 2013

The LTspice waveform viewer can integrate a trace to produce the average or RMS value over a given region.

To integrate a trace in the waveform viewer:

  1. Zoom in to the region of interest.
  2. Hold down the control key and click the label of the trace you want to integrate.

Based on the physical units of the data trace, LTspice IV displays a meaningful average for that type of data. For example, if the units are a voltage or current, LTspice IV displays the average and the RMS values. Otherwise, LTspice IV displays the average and integral of the data displayed in the waveform viewer. If you are plotting noise densities from a .noise simulation, LTspice IV shows total RMS noise.

About The Authors

Gabino Alonso
Gabino Alonso is currently the director of strategic marketing for the Power by Linear™ Group. Prior to joining ADI, Gabino held various positions in marketing, engineering, operations, and education at Linear Technology, ...
Add to myAnalog

Author's Contact Information

Gabino Alonso

Director, Power Strategic Marketing

Related to this Article

Resources

Latest Media 20

Subtitle
Learn More
Add to myAnalog