Optimizing the Load-Switch Function of the DS2715 Battery-Charger IC

Feb 14 2023

The DS2715 is unique compared to other charging ICs in that it provides a charging and discharging path to battery cells through a single transistor. This functionality, combined with its 10-cell charging capacity, makes it a very popular charging solution for many types of battery-powered devices. Explaining exactly how the DS2715 controls the regulation transistor, this application note describes circuit adjustments that designers can make to optimize their DS2715 application. First, it details a typical application circuit for a 3-cell battery pack. Then, it presents two alternate circuits: an improved circuit for applications in which the DS2715 is connected to loads that operate noncontinuously, and a circuit for powering the load directly from batteries.

 

Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project