PCBs Layout Guidelines for RF & Mixed-Signal

Sep 14 2011

Figure 1

   

Abstract

This application note provides guidelines and suggestions for RF printed-circuit board (PCB) design and layout, including some discussion of mixed-signal applications. The material provides "best practices" guidance, and should be used in conjunction with all other design and manufacturing guidelines that may apply to particular components, PCB manufacturers, and material sets as applicable.

This application note applies to all Analog Device wireless products.

Introduction

This application note provides guidelines and suggestions for RF printed-circuit board (PCB) design and layout, including some discussion of mixed-signal applications, such as digital, analog, and RF components on the same PCB. The material is arranged by topic areas and provides "best practices" guidance. It should be used in conjunction with all other design and manufacturing guidelines that may apply to particular components, PCB manufacturers, and material sets as applicable.

RF Transmission Lines

Many of Analog Devices' RF components require controlled impedance transmission lines that will transport RF power to (or from) IC pins on the PCB. These transmission lines can be implemented on a exterior layer (top or bottom), or buried in an internal layer. Guidelines for these transmission lines include discussions relating to the microstrip, suspended stripline, coplanar waveguide (grounded), and characteristic impedance. It also describes transmission line bends and corner compensation, and layer changes for transmission lines.


Microstrip


This type of transmission line consists of fixed-width metal routing (the conductor), along with a solid unbroken ground plane located directly underneath (on the adjacent layer). For example, a microstrip on Layer 1 (top metal) requires a solid ground plane on Layer 2 (Figure 1). The width of the routing, the thickness of the dielectric layer, and the type of dielectric determine the characteristic impedance (typically 50Ω or 75Ω).

Isometric view Microstrip example.

Figure 1. Microstrip example (isometric view).

Suspended Stripline


This line consists of a fixed-width routing on an inner layer, with solid ground planes above and below the center conductor. The conductor can be located midway between the ground planes (Figure 2), or it can be offset (Figure 3). This is the appropriate method for RF routing on inner layers.

Suspended stripline (end view).

Figure 2. Suspended stripline (end view).

Offset suspended stripline. A variant of the stripline, for PCBs with unequal layer thicknesses (end view).

Figure 3. Offset suspended stripline. A variant of the stripline, for PCBs with unequal layer thicknesses (end view).

Coplanar Waveguide (Grounded)


A coplanar waveguide provides for better isolation between nearby RF lines, as well as other signal lines (end view). This medium consists of a center conductor with ground planes on either side and below (Figure 4).

Coplanar waveguide provides for better isolation between nearby RF lines and other signal lines.

Figure 4. A coplanar waveguide provides for better isolation between nearby RF lines and other signal lines.

Via "fences" are recommended on both sides of a coplanar waveguide, as shown in Figure 5. This top view provides an example of a row of ground vias on each top metal gound plane on either side of the center conductor. Return currents induced on the top layer are shorted to the underlying ground layer.

Via fences are recommended on both sides of a coplanar waveguide.

Figure 5. Via fences are recommended on both sides of a coplanar waveguide.

Characteristic Impedance


There are several calculators available to properly set the signal conductor line width to achieve the target impedance. However, caution should be used when entering the dielectric constant of the layers. The outer laminated layers of typical PCBs often contain less glass content than the core of the board, and consequently the dielectric constant is lower. For example, FR4 core is generally given as εR = 4.2, whereas the outer laminate (prepreg) layers are typically εR = 3.8. Examples given below for reference only, metal thickness assumed for 1oz copper (1.4 mils, 0.036mm).

Table 1. Examples of Characteristic Impedance
Media Dielectric Layer Thickness in mils (mm) Center Conductor in mils (mm) Gap Characteristic Impedance
Microstrip Prepreg (3.8) 6 (0.152) 11.5 (0.292) N/A 50.3
10 (0.254) 20 (0.508) 50.0
Diff. Pair Prepreg (3.8) 6 (0.152) 25 (0.635) 6 (0.152) 50.6
Stripline FR4 (4.5) 12 (0.305) 3.7 (0.094) N/A 50.0
Offset Stripline Prepreg (3.9)
6 (0.152) upper, 4.8 (0.122)

N/A

50.1
10 (0.254) lower
Coplanar WG Prepreg (3.8)
6 (0.152) 14 (0.35) 20 (0.50) 49.7

Transmission Line Bends and Corner Compensation


When transmission lines are required to bend (change direction) due to routing constraints, use a bend radius that is at least 3 times the center conductor width. In other words:

Bend Radius ≥ 3 × (Line Width).

This will minimize any characteristics impedance changes moving through the bend.

In cases where a gradually curved bend is not possible, the transmission line can undergo a right-angle bend (noncurved). See Figure 6. However, this must be compensated to reduce the impedance discontinuity caused by the local increase in effective line width going through the bend. A standard compensation method is the angled miter, as illustrated below. The optimum microstrip right-angle miter is given by the formula of Douville and James:

Equation 1.

Where M is the fraction (%) of the miter compared to the unmitered bend. This formula is independent of the dielectric constant, and is subject to the constraint that w/h ≥ 0.25.

Similar methods can be employed for other transmission lines. If there is any uncertainty as to the correct compensation, the bend should be modeled using an electromagnetic simulator if the design requires high-performance transmission lines.

When a curved bend is not possible, the transmission line can undergo a right-angle bend.

Figure 6. When a curved bend is not possible, the transmission line can undergo a right-angle bend.

Layer Changes for Transmission Lines


When layout constraints required that a transmission line move to a different layer, it is recommended that at least two via holes be used for each transition to minimize the via inductance loading. A pair of vias will effectively cut the transition inductance by 50%, and the largest diameter via should be utilized that is compatible with the transmission line width. For example, on a 15-mil microstrip line, a via diameter (finished plated diameter) of 15 mils to 18 mils would be used. If space does not permit the use of larger vias, then three transition vias of smaller diameter should be used.

Signal Line Isolation

Care must be taken to prevent unintended coupling between signal lines. Some examples of potential coupling and preventative measures:

  • RF Transmission Lines: Lines should be kept as far apart as possible, and should not be routed in close proximity for extended distances. Coupling between parallel microstrip lines will increase with decreasing separation and increasing parallel routing distance. Lines that cross on separate layers should have a ground plane keeping them apart. Signal lines that will carry high power levels should be kept away from all other lines whenever possible. The grounded coplanar waveguide provides for excellent isolation between lines. It is impractical to achieve isolation better than approximately -45dB between RF lines on small PCBs.
  • High-Speed Digital Signal Lines: These lines should be routed separately on a different layer than the RF signal lines, to prevent coupling. Digital noise (from clocks, PLLs, etc.) can couple onto RF signal lines, and these can be modulated onto RF carriers. Alternatively, in some cases digital noise can be up/down-converted.
  • VCC/Power Lines: These should be routed on a dedicated layer. Adequate decoupling/bypass capacitors should be provided at the main VCC distribution node, as well as at VCC branches. The choice of the bypass capacitances must be made based on the overall frequency response of the RF IC, and the expected frequency distribution nature of any digital noise from clocks and PLLs. These lines should also be separated from any RF lines that will transmit large amounts of RF power.

Ground Planes

The recommended practice is to use a solid (continuous) ground plane on Layer 2, assuming Layer 1 is used for the RF components and transmission lines. For striplines and offset striplines, ground planes above and below the center conductor are required. These planes must not be shared or assigned to signal or power nets, but must be uniquely allocated to ground. Partial ground planes on a layer, sometimes required by design constraints, must underlie all RF components and transmission lines. Ground planes must not be broken under transmission line routing.

Ground vias between layers should be added liberally throughout the RF portion of the PCB. This helps prevent accrual of parasitic ground inductance due to ground-current return paths. The vias also help to prevent cross-coupling from RF and other signal lines across the PCB.

Special Consideration on Bias and Ground Layers

The layers assigned to system bias (DC supply) and ground must be considered in terms of the return current for the components. The general guidance is to not have signals routed on layers between the bias layer and the ground layer.

Incorrect layer assignment: there are signal layers between the bias layer and ground-current return path on ground layer. Bias line noise can be coupled to the signal layers.

Figure 7. Incorrect layer assignment: there are signal layers between the bias layer and ground-current return path on ground layer. Bias line noise can be coupled to the signal layers.

Better layer assignment: there are no signal layers between the bias and ground return layers.

Figure 8. Better layer assignment: there are no signal layers between the bias and ground return layers.

Power (Bias) Routing and Supply Decoupling

A common practice is to use a "star" configuration for the power-supply routes, if a component has several supply connections (Figure 9). A larger decoupling capacitor (tens of µFds) is mounted at the "root" of the star, and smaller capacitors at each of the star branches. The value of these latter capacitors depends on the operating frequency range of the RF IC, and their specific functionality (i.e., interstage vs. main supply decoupling). An example is shown below.

Component has several supply connections, the power-supply routes can be arranged in a star configuration

Figure 9. If a component has several supply connections, the power-supply routes can be arranged in a star configuration.

The "star" configuration avoids long ground return paths that would result if all the pins connected to the same bias net were connected in series. A long ground return path would cause a parasitic inductance that could lead to unintended feedback loops. The key consideration with supply decoupling is that the DC supply connections must be electrically defined as AC ground.

Selection of Decoupling or Bypass Capacitors

Real capacitors have limited effective frequency ranges due to their self-resonant frequency (SRF). The SRF is available from the manufacturer, but sometimes must be characterized by direct measurement. Above the SRF, the capacitor is inductive, and therefore will not perform the decoupling or bypass function. When broadband decoupling is required, standard practice is to use several capacitors of increasing size (capacitance), all connected in parallel. The smaller value capacitors normally have higher SRFs (for example, a 0.2pF value in a 0402 SMT package with an SRF = 14GHz), while the larger values have lower SRFs (for example, a 2pF value in the same package with an SRF = 4GHz). A typical arrangement is depicted in Table 2.

Table 2. Useful Frequency Ranges of Capacitors
Component Capacitance Package SRF Useful Frequency Range*
Ultra-High Range 20pF 0402 2.5GHz 800MHz to 2.5GHz
Very High Range 100pF 0402 800MHz 250MHz to 800MHz
High Range 1000pF 0402 250MHz 50MHz to 250MHz
Midrange 1µF 0402 60MHz 100kHz to 60MHz
Low Range 10µF 0603 600kHz 10kHz to 600kHz
*Low end of useful frequency range defined as less than 5Ω of capacitive reactance.

Bypass Capacitor Layout Considerations

Since the supply lines must be AC ground, it is important to minimize the parasitic inductance added to the AC ground return path. These parasitic inductances can be caused by layout or component orientation choices, such as the orientation of a decoupling capacitor's ground. There are two basic methods, shown in Figure 10 and Figure 11.

Figure 10. This configuration presents the smallest total footprint for the bypass capcitor and related vias.

Figure 10. This configuration presents the smallest total footprint for the bypass capacitor and related vias.

In this configuration, the vias connecting the VCC pad on the top layer to the inner power plane (layer) potentially impede the AC ground current return, forcing a longer return path with resulting higher parasitic inductance. Any AC current flowing into the VCC pin passes through the bypass capacitor to its ground side before returning on the inner ground layer. This configuration presents the smallest total footprint for the bypass capacitor and related vias.

Figure 11. This configuration requires more PCB area.

Figure 11. This configuration requires more PCB area.

In this alternate configuration, the AC ground return paths are not blocked by the power-plane vias. Generally this configuration requires somewhat more PCB area.

Grounding of Shunt-Connected Components

For shunt-connected (grounded) components (such as power-supply decoupling capacitors), the recommended practice is to use at least two grounding vias for each component (Figure 12). This reduces the effect of via parasitic inductance. Via ground "islands" can be used for groups of shunt-connected components.

Figure 12. Using at least two grounding vias for each components reduces the effect of via parasitic inductance.

Figure 12. Using at least two grounding vias for each components reduces the effect of via parasitic inductance.

IC Ground Plane ("Paddle")

Most ICs require a solid ground plane on the component layer (top or bottom of PCB) directly underneath the component. This ground plane will carry DC and RF return currents through the PCB to the assigned ground plane. The secondary function of this component "ground paddle" is to provide a thermal heatsink, so the paddle should include the maximum number of thru vias that are allowed by the PCB design rules. The example below shows a 5 × 5 array of via holes embedded in the central ground plane (on the component layer) directly under the RF IC (Figure 13). The maximum number of vias that can be accommodated by other layout considerations should be used. These vias are ideally thru-vias (i.e., penetrate all the way through the PCB), and must be plated. If possible, the vias should be filled with thermally conductive paste to enhance the heatsink (the paste is applied after via plating and prior to final board plating).

Figure 13. A 5 × 5 array of via holes embedded in the central ground plane directly under the RF IC.

Figure 13. A 5 × 5 array of via holes embedded in the central ground plane directly under the RF IC.



Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

MAX3654EVKIT

MAX3654 Evaluation Kit

MAX3654

47MHz to 870MHz Analog CATV Transimpedance Amplifier

MAX2990

10kHz to 490kHz OFDM-Based Power Line Communications Modem

MAX9957

Fast Dual Driver for ATE with Waveform Shaping

MAX19692

12-Bit, 2.3Gsps Multi-Nyquist DAC

MAX5879

14-Bit, 2.3Gsps Direct RF Synthesis DAC with Selectable Frequency Response

MAX5879EVKIT

Evaluation Kit for the MAX5879

MAX5894

14-Bit, 500Msps, Interpolating and Modulating Dual DAC with CMOS Inputs

MAX66901-K00

High-Frequency Developers Kit for ISO 14443B and ISO 15693 RFID Keys

MAX4987AE

Overvoltage-Protection Controller with USB ESD Protection

MAX77179

High-Bandwidth LTE/WCDMA PA Power Management ICs in a 1.75mm x 1.4mm, 0.4mm Pitch WLP

MAX77178

High-Bandwidth LTE/WCDMA PA Power Management ICs in a 1.75mm x 1.4mm, 0.4mm Pitch WLP

MAX2135

ISDB-T/DVB-T Diversity Tuner

MAX3660

Analog CATV Transimpedance Amplifier

MAX2742

Single-Chip Global Positioning System Receiver Front-End

DS4026

10MHz to 51.84MHz TCXO

MAX3660EVKIT
MAX2041

High-Linearity, 1700MHz to 3000MHz Upconversion/Downconversion Mixer with LO Buffer/Switch

MAX3517EVKIT

Evaluation Kit for the MAX3514, MAX3516, MAX3517

MAX2900EVKIT

Evaluation Kit for the MAX2900, MAX2901, MAX2902, MAX2903, MAX2904

MAX2507

Complete Cellular Baseband-to-RF Transmitters with PA

MAX2325

Triple/Dual-Mode CDMA LNA/Mixers

MAX3543

Multiband Analog and Digital Television Tuner

MAX2504AEVKIT

Evaluation Kits for the MAX2500/03/04/04A/06/07/07A/09

MAX2401

W-CDMA/W-TDD/TD-SCDMA Zero-IF Receivers

MAX2684

3.5GHz Downconverter Mixers with Selectable LO Doubler

MAX19757

Dual, SiGe, High-Linearity, 1700MHz to 2700MHz Downconversion Mixer with Advanced Shutdown Features

MAX7044EVKIT

Evaluation Kit for the MAX7044

MAX2721EVKIT

Evaluation Kit for the MAX2720, MAX2721

MAX2842

3.3GHz to 3.9GHz MIMO Wireless Broadband RF Transceiver

MAX2633

VHF-to-Microwave, +3V, General-Purpose Amplifiers

MAX2064

50MHz to 1000MHz, High-Linearity, Serial/Analog-Controlled VGA

MAX2623

Monolithic Voltage Controlled Oscillators

MAX2902

200mW Single-Chip Transmitter ICs for 868MHz/915MHz ISM Bands

MAX7042EVKIT

Evaluation Kit for the MAX7042

MAX2821A

2.4GHz 802.11b Zero-IF Transceivers

MAX2607

45MHz to 650MHz, Integrated IF VCOs with Differential Output

MAX2460EVKIT

Evaluation Kit for the MAX2420, MAX2421, MAX2422, MAX2460, MAX2463

MAX9930

2MHz to 1.6GHz 45dB RF-Detecting Controllers and RF Detector

MAX2118

Complete DBS Direct-Conversion Tuner ICs with Monolithic VCOs

MAX2507AEVKIT

Evaluation Kits for the MAX2500/03/04/04A/06/07/07A/09

MAX2108

Direct-Conversion Tuner IC

MAX2471EVKIT

Evaluation Kit for the MAX2470, MAX2471

MAX2364EVKIT

Evaluation Kit for the MAX2360, MAX2362, MAX2364

MAX2680EVKIT

Evaluation Kit for the MAX2680/MAX2681/MAX2682

MAX2121EVKIT

Evaluation Kit for the MAX2121

MAX2268

+2.7V, Single-Supply, Cellular-Band Linear Power Amplifiers

MAX2608EVKIT

Evaluation Kit for the MAX2605, MAX2606, MAX2607, MAX2608, MAX2609

MAX2553

Band Class 0, 1, and 10 cdma2000 Femtocell Transceiver

MAX1470EVKIT

Evaluation Kit for the MAX1470

MAX9988

+14dBm to +20dBm LO Buffers/Splitters with ±1dB Variation

MAX2547

WCDMA/HSPA Band I RF-to-Bits Femto-Basestation Radio Receiver

MAX2173

RF to Bits Tuner for Digital Audio Broadcast

MAX2606EVKIT

Evaluation Kit for the MAX2605, MAX2606, MAX2607, MAX2608, MAX2609

MAX2244

2.5GHz, 22dBm/20dBm Power Amplifiers with Analog Closed-Loop Power Control

MAX2537

Quadruple-Mode PCS/Cellular/GPS LNA/Mixers

MAX2441

900MHz Image-Reject Receivers

MAX2232

900MHz ISM-Band, 250mW Power Amplifiers with Analog or Digital Gain Control

MAX2023EVKIT

MAX2023 Evaluation Kit

MAX2720EVKIT

Evaluation Kit for the MAX2720, MAX2721

MAX2314

CDMA IF VGAs and I/Q Demodulators with VCO and Synthesizer

MAX3518EVKIT

Evaluation Kit for the MAX3518

MAX2701EVKIT

Evaluation Kit for the MAX2700, MAX2701

MAX2051

SiGe, High-Linearity, 850MHz to 1550MHz Up/Downconversion Mixer with LO Buffer

MAX2507EVKIT

Evaluation Kits for the MAX2500/03/04/04A/06/07/07A/09

MAX2422EVKIT

Evaluation Kit for the MAX2420, MAX2421, MAX2422, MAX2460, MAX2463

MAX2673

400MHz to 2.5GHz Upconverters

MAX3516

Upstream CATV Amplifiers

MAX7058EVKIT

Evaluation Kit for the MAX7058

MAX2202

RMS Power Detector

MAX2663

400MHz to 2.5GHz Upconverters

MAX2831

2.4GHz to 2.5GHz, 802.11g RF Transceivers with Integrated PA

MAX2170EVKIT

MAX2170 Evaluation Kit

DS1870

LDMOS RF Power-Amplifier Bias Controller

MAX7036

300MHz to 450MHz ASK Receiver with Internal IF Filter

MAX2368

Complete Dual-Band Quadrature Transmitters

MAX2657

GPS/GNSS Low-Noise Amplifiers

MAX2821

2.4GHz 802.11b Zero-IF Transceivers

MAX9981

825MHz to 915MHz, Dual SiGe High-Linearity Active Mixer

MAX2424

900MHz Image-Reject Receivers with Transmit Mixer

MAX2027

IF Digitally Controlled Variable-Gain Amplifier

MAX2538EVKIT

Quadruple-Mode LNA/Mixer Evaluation Kits

MAX2839ASEVKIT

Evaluation Kit for the MAX2839AS

MAX2751

2.4GHz Monolithic Voltage-Controlled Oscillators

MAX2745EVKIT

Evaluation Kit for the MAX2745

MAX3580EVKIT

MAX3580 Evaluation Kit

MAX3505EVKIT

Evaluation Kit for the MAX3503, MAX3505

MAX2745

Single-Chip Global Positioning System Front-End Downconverter

MAX2371

LNAs with Step Attenuator and VGA

MAX2162

ISDB-T 1- and 3-Segment Low-IF Tuners

MAX2354

Quadruple-Mode PCS/Cellular/GPS LNA/Mixers

MAX2091
50MHz to 500MHz Analog VGA, 1735MHz to 1935MHz Upconverting Mixer with Image Filtering, Threshold Alarm Circui...
MAX2308EVKIT

Evaluation Kit for the MAX2306, MAX2308, MAX2309

MAX2822EVKIT

Evaluation Kit for the MAX2822

MAX2430

Low-Voltage Silicon RF Power-Amplifier Predriver

MAX2721

1.7GHz to 2.5GHz, Direct I/Q Modulator with VGA and PA Driver

MAX2205EVKIT

Evaluation Kit for the MAX2205, MAX2206, MAX2207, MAX2208

MAX2043EVKIT

Evaluation Kit for the MAX2043

MAX2209A

RF Power Detector with Shutdown Control

MAX2338

Triple/Dual-Mode CDMA LNA/Mixers

MAX2502

Complete Cellular Baseband-to-RF Transmitters with PA

MAX19993

Dual, SiGe, High-Linearity, 1200MHz to 1700MHz Downconversion Mixer with LO Buffer/Switch

MAX2121

Complete Direct-Conversion L-Band Tuner

MAX2871

23.5MHz to 6000MHz Fractional/Integer-N Synthesizer/VCO

MAX3542

Complete Single-Conversion Television Tuner

MAX2400

W-CDMA/W-TDD/TD-SCDMA Zero-IF Receivers

MAX2655EVKIT

Evaluation Kit for the MAX2654, MAX2655, MAX2656

MAX2741EVKIT

Evaluation Kit for the MAX2741

MAX3532

Upstream CATV Driver Amplifier

MAX2687

GPS/GNSS Low-Noise Amplifiers

MAX2769

Universal GPS Receiver

MAX2580

LTE Small-Cell MIMO Transceiver

MAX2047EVKIT

Evaluation Kit for the MAX2045, MAX2046, MAX2047

MAX9987EVKIT

Evaluation Kit for the MAX9987, MAX9988

MAX9990EVKIT

Evaluation Kit for the MAX9989, MAX9990

MAX2067

50MHz to 1000MHz High-Linearity, Serial/Analog-Controlled VGA

MAX2169

Multiband Tuner for Mobile Multimedia Applications

MAX2622

Monolithic Voltage Controlled Oscillators

MAX2421EVKIT

Evaluation Kit for the MAX2420, MAX2421, MAX2422, MAX2460, MAX2463

MAX9986A

SiGe High-Linearity, 815MHz to 1000MHz Downconversion Mixer with LO Buffer/Switch

MAX2612

40MHz to 4GHz Linear Broadband Amplifiers

MAX2901

200mW Single-Chip Transmitter ICs for 868MHz/915MHz ISM Bands

MAX2509EVKIT

Evaluation Kits for the MAX2500/03/04/04A/06/07/07A/09

MAX2504A

Complete Cellular Baseband-to-RF Transmitters with PA

MAX2043

1700MHz to 3000MHz High-Linearity, Low LO Leakage Base-Station Rx/Tx Mixer

MAX2606

45MHz to 650MHz, Integrated IF VCOs with Differential Output

MAX2320

Adjustable, High-Linearity, SiGe, Dual-Band, LNA/Mixer ICs

MAX2769EVKIT

Evaluation Kit for the MAX2769

MAX2205

RF Power Detectors in UCSP

MAX2690

Low-Noise, 2.5GHz Downconverter Mixer

MAX2839AS

2.3GHz to 2.7GHz MIMO Wireless Broadband RF Transceiver

MAX2552

Band III, IV, IX, and X WCDMA Femtocell Transceiver with GSM Monitoring

MAX2839

2.3GHz to 2.7GHz MIMO Wireless Broadband RF Transceiver

MAX2027EVKIT

Evaluation Kit for the MAX2027

MAX2829

Single-/Dual-Band 802.11a/b/g World-Band Transceiver ICs

MAX2511EVKIT

Evaluation Kit for the MAX2511

MAX2172

Direct-Conversion to Low-IF Tuner for Digital Audio Broadcast

MAX2247

2.4GHz SiGe Linear Power Amplifier

MAX2700

1.8GHz to 2.5GHz, Direct-Downconversion Receivers

MAX2387EVKIT

Evaluation Kit for the MAX2387, MAX2388, MAX2389

MAX2440

900MHz Image-Reject Receivers

MAX2644EVKIT

Evaluation Kit for the MAX2644

MAX2652EVKIT

Evaluation Kit for the MAX2651, MAX2652, MAX2653

MAX2383

WCDMA Upconverter and PA Driver with Power Control

MAX4001

2.5GHz 45dB RF-Detecting Controllers

MAX2676

GPS/GNSS LNAs with Antenna Switch and Bias

MAX9985EVKIT

MAX9985 Evaluation Kit

MAX7049

High-Performance, 288MHz to 945MHz ASK/FSK ISM Transmitter

MAX2656EVKIT

Evaluation Kit for the MAX2654, MAX2655, MAX2656

MAX2373

LNAs with Step Attenuator and VGA

MAX3505

Upstream CATV Amplifier

MAX2367

Complete Dual-Band Quadrature Transmitters

MAX2652

GSM900 and DCS1800/PCS1900 Dual-Band, Low-Noise Amplifiers

MAX2820

2.4GHz 802.11b Zero-IF Transceivers

MAX9994

SiGe High-Linearity, 1400MHz to 2200MHz Downconversion Mixer with LO Buffer/Switch

MAX2383EVKIT

Evaluation Kit for the MAX2383

MAX2648EVKIT

Evaluation Kit for the MAX2648

MAX2032

High-Linearity, 650MHz to 1000MHz Upconversion/Downconversion Mixer with LO Buffer/Switch

MAX2395EVKIT

Evaluation Kit for the MAX2395

MAX2045EVKIT

Evaluation Kit for the MAX2045, MAX2046, MAX2047

MAX2016

LF-to-2.5GHz Dual Logarithmic Detector/Controller for Power, Gain, and VSWR Measurements

MAX2839EVKIT

Evaluation Kit for the MAX2839

MAX2582

Complete RF-to-Baseband Receiver

MAX2750

2.4GHz Monolithic Voltage-Controlled Oscillators

MAX3503EVKIT

Evaluation Kit for the MAX3503, MAX3505

MAX2902EVKIT

Evaluation Kit for the MAX2900, MAX2901, MAX2902, MAX2903, MAX2904

MAX2740

Integrated GPS Receiver and Synthesizer

MAX7042

308MHz/315MHz/418MHz/433.92MHz Low-Power, FSK Superheterodyne Receiver

MAX2370

Complete 450MHz Quadrature Transmitter

MAX2161

ISDB-T 1- and 3-Segment Low-IF Tuners

MAX2829EVKIT

Evaluation Kits for the MAX2828 and MAX2829

MAX3516EVKIT

Evaluation Kit for the MAX3514, MAX3516, MAX3517

MAX3514EVKIT

Evaluation Kit for the MAX3514, MAX3516, MAX3517

MAX2246EVKIT

Evaluation Kit for the MAX2244, MAX2245, MAX2246

MAX8805X

600mA/650mA PWM Step-Down Converters in 2mm x 2mm WLP for WCDMA PA Power

MAX2172EVKIT

Evaluation Kit for the MAX2172

MAX2232EVKIT

Evaluation Kit for the MAX2232, MAX2233

MAX2327

Adjustable, High-Linearity, SiGe, Dual-Band, LNA/Mixer ICs

MAX2904EVKIT

Evaluation Kit for the MAX2900, MAX2901, MAX2902, MAX2903, MAX2904

MAX2692

WLAN/WiMAX Low-Noise Amplifiers

MAX2686

GPS/GNSS Low-Noise Amplifiers

MAX2850

5GHz, 4-Channel MIMO Transmitter

MAX2361EVKIT

Evaluation Kit for the MAX2361, MAX2363, MAX2365

MAX2673EVKIT

Evaluation Kit for the MAX2673

MAX2066

50MHz to 1000MHz High-Linearity, Serial/Parallel-Controlled Digital VGA

MAX2373EVKIT

Evaluation Kit for the MAX2371, MAX2373

MAX2360

Complete Dual-Band Quadrature Transmitters

MAX2135A

ISDB-T/DVB-T Diversity Tuner

MAX2411A

Low-Cost RF Up/Downconverter with LNA and PA Driver

MAX2164

ISDB-T 1-Segment Tuner

MAX2180A

AM/FM Car Antenna Low-Noise Amplifier

MAX2251EVKIT

Evaluation Kit for the MAX2251

MAX2539

Quadruple-Mode PCS/Cellular/GPS LNA/Mixers

MAX2654EVKIT

Evaluation Kit for the MAX2654, MAX2655, MAX2656

MAX2056

800MHz to 1000MHz Variable-Gain Amplifier with Analog Gain Control

MAX2366EVKIT

Evaluation Kit for the MAX2366, MAX2367, MAX2368

MAX2880EVKIT

Evaluation Kit for the MAX2880

MAX2611

DC-to-Microwave, Low-Noise Amplifier

MAX2904

200mW Single-Chip Transmitter ICs for 868MHz/915MHz ISM Bands

MAX2042

SiGe High-Linearity, 2000MHz to 3000MHz Upconversion/Downconversion Mixer with LO Buffer

MAX2424EVKIT

Evaluation Kit for the MAX2424, MAX2426

MAX2601

3.6V, 1W RF Power Transistors for 900MHz Applications

MAX9932

2MHz to 1.6GHz 45dB RF-Detecting Controllers and RF Detector

MAX2112

Complete, Direct-Conversion Tuner for DVB-S2 Applications

MAX3518

DOCSIS 3.0 Upstream Amplifier

MAX19995A

Dual, SiGe, High-Linearity, 1700MHz to 2200MHz Downconversion Mixer with LO Buffer/Switch

MAX2102

Direct-Conversion Tuner ICs for Digital DBS Applications

MAX2204

RF Power Detector

MAX19994A

Dual, SiGe, High-Linearity, 1200MHz to 2000MHz Downconversion Mixer with LO Buffer/Switch

MAX9996EVKIT

Evaluation Kit for the MAX9996

MAX2830EVKIT

Evaluation Kit for the MAX2830

MAX2116EVKIT

Evaluation Kit for the MAX2116, MAX2118

MAX2659

GPS/GNSS Low-Noise Amplifier

MAX2470

10MHz to 500MHz, VCO Buffer Amplifiers with Differential Outputs

MAX2649

5GHz Low-Noise Amplifier with Shutdown

MAX2828

Single-/Dual-Band 802.11a/b/g World-Band Transceiver ICs

MAX2750EVKIT

Evaluation Kit for the MAX2750, MAX2751, MAX2752

MAX2039

High-Linearity, 1700MHz to 2200MHz Upconversion/Downconversion Mixer with LO Buffer/Switch

MAX2246

2.5GHz, 22dBm/20dBm Power Amplifiers with Analog Closed-Loop Power Control

MAX2531

Quadruple-Mode PCS/Cellular/GPS LNA/Mixers

MAX2055EVKIT

Evaluation Kit for the MAX2055

MAX2264EVKIT

Evaluation Kit for the MAX2264, MAX2265, MAX2266

MAX2029

High-Linearity, 815MHz to 1000MHz Upconversion/Downconversion Mixer with LO Buffer/Switch

MAX2316

CDMA IF VGAs and I/Q Demodulators with VCO and Synthesizer

MAX2396

W-CDMA/W-TDD/TD-SCDMA Zero-IF Receivers

MAX2306

CDMA IF VGAs and I/Q Demodulators with VCO and Synthesizer

MAX2386

CDMA + GPS LNA/Mixers

MAX4000

2.5GHz 45dB RF-Detecting Controllers

MAX2327EVKIT

Evaluation Kit for the MAX2320, MAX2321, MAX2322, MAX2324, MAX2326, MAX2327

MAX2665

VHF/UHF Low-Noise Amplifiers

MAX2362

Complete Dual-Band Quadrature Transmitters

MAX2651

GSM900 and DCS1800/PCS1900 Dual-Band, Low-Noise Amplifiers

MAX9993

High-Linearity 1700MHz to 2200MHz Down-Conversion Mixer with LO Buffer/Switch

MAX2641

300MHz to 2500MHz SiGe Ultra-Low-Noise Amplifiers

MAX2510EVKIT

Evaluation Kit for the MAX2510

MAX2368EVKIT

Evaluation Kit for the MAX2366, MAX2367, MAX2368

MAX2582EVKIT

MAX2582 Evaluation Kit

MAX2031

High-Linearity, 650MHz to 1000MHz Upconversion/Downconversion Mixer with LO Buffer/Switch

MAX2310EVKIT

Evaluation Kit for the MAX2310, MAX2314

MAX2426

900MHz Image-Reject Receivers with Transmit Mixer

MAX2572EVKIT

Evaluation Kit for the MAX2560, MAX2566, MAX2572

MAX19995

Dual, SiGe, High-Linearity, 1700MHz to 2200MHz Downconversion Mixer with LO Buffer/Switch

MAX3558

Quad-Output LNA with AGC for Cable TV Applications

MAX19999A

Dual, SiGe, High-Linearity, High-Gain, 3200MHz to 3900MHz Downconversion Mixer with LO Buffer/Switch

MAX2021

High-Dynamic-Range, Direct Up-/Downconversion 650MHz to 1200MHz Quadrature Mod/Demod

MAX2411AEVKIT

Evaluation Kit for the MAX2411A

MAX19998A

SiGe, High-Linearity, High-Gain, 3200MHz to 3900MHz Downconversion Mixer with LO Buffer/Switch

MAX2015

0.1GHz to 3GHz, 75dB Logarithmic Detector/Controller

MAX19791

50MHz to 4000MHz Dual Analog Voltage Variable Attenuator with On-Chip 10-Bit SPI-Controlled DAC

MAX2406EVKIT

Evaluation Kit for the MAX2406

MAX2162EVKIT

Evaluation Kits for the MAX2161/MAX2162

MAX2753

2.4GHz, Monolithic Voltage-Controlled Oscillator with Differential Outputs

MAX2689

GPS/GNSS Low-Noise Amplifiers

MAX2557A

Multiband, Multimode RF-to-Bits CDMA Femto-Basestation Radio Receiver

MAX2901EVKIT

Evaluation Kit for the MAX2900, MAX2901, MAX2902, MAX2903, MAX2904

MAX8805W

600mA/650mA PWM Step-Down Converters in 2mm x 2mm WLP for WCDMA PA Power

MAX7031

Low-Cost, 308MHz, 315MHz, and 433.92MHz FSK Transceiver with Fractional-N PLL

MAX2150

Wideband I/Q Modulator with Sigma-Delta Fractional-N Synthesizer

MAX9996

SiGe High-Linearity, 1700MHz to 2200MHz Downconversion Mixer with LO Buffer/Switch

MAX2056EVKIT

Evaluation Kit for the MAX2056

MAX2140

Complete SDARS Receiver

MAX2504

Complete Cellular Baseband-to-RF Transmitters with PA

MAX2322

Adjustable, High-Linearity, SiGe, Dual-Band, LNA/Mixer ICs

MAX2420EVKIT

Evaluation Kit for the MAX2420, MAX2421, MAX2422, MAX2460, MAX2463

MAX2609

45MHz to 650MHz, Integrated IF VCOs with Differential Output

MAX3544

Multiband Digital Television Tuner

MAX2691

L2 Band GPS Low-Noise Amplifier

MAX2531EVKIT

Quadruple-Mode LNA/Mixer Evaluation Kits

MAX2681

400MHz to 2.5GHz, Low-Noise, SiGe Downconverter Mixers

MAX2472

500MHz to 2500MHz, VCO Buffer Amplifiers

MAX2233EVKIT

Evaluation Kit for the MAX2232, MAX2233

MAX2391EVKIT

Evaluation Kit for the MAX2390, MAX2391, MAX2392, MAX2393, MAX2396, MAX2400

MAX2630

VHF-to-Microwave, +3V, General-Purpose Amplifiers

MAX2687L

GPS/GNSS Low-Noise Amplifier with Integrated LDO

MAX2041EVKIT

Evaluation Kit for the MAX2041

MAX2624

Monolithic Voltage Controlled Oscillators

MAX7033EVKIT

Evaluation Kit for the MAX7033

MAX2538

Quadruple-Mode PCS/Cellular/GPS LNA/Mixers

MAX2055

Digitally Controlled, Variable-Gain, Differential ADC Driver/Amplifier

MAX7036EVKIT

Evaluation Kit for the MAX7036

MAX2442

900MHz Image-Reject Receivers

MAX2233

900MHz ISM-Band, 250mW Power Amplifiers with Analog or Digital Gain Control

MAX2614

40MHz to 4GHz Linear Broadband Amplifiers

MAX2903

200mW Single-Chip Transmitter ICs for 868MHz/915MHz ISM Bands

MAX1479

300MHz to 450MHz Low-Power, Crystal-Based +10dBm ASK/FSK Transmitter

MAX2045

High-Gain Vector Multipliers

MAX9931

2MHz to 1.6GHz 45dB RF-Detecting Controllers and RF Detector

MAX2903EVKIT

Evaluation Kit for the MAX2900, MAX2901, MAX2902, MAX2903, MAX2904

MAX2204EVKIT

MAX2204 Evaluation Kit

MAX3517

Upstream CATV Amplifiers

MAX2160EBG

ISDB-T Single-Segment Low-IF Tuners

MAX2207

RF Power Detectors in UCSP

MAX3507

Upstream CATV Amplifier

MAX2265

2.7V, Single-Supply, Cellular-Band Linear Power Amplifiers

MAX2369

Complete Dual-Band Quadrature Transmitter

MAX2371EVKIT

Evaluation Kit for the MAX2371, MAX2373

MAX2180

AM/FM Antenna Low-Noise Amplifier

MAX7049EVKIT-915

Evaluation Kits for the MAX7049

MAX9985

Dual, SiGe, High-Linearity, 700MHz to 1000MHz Downconversion Mixer with LO Buffer/Switch

MAX2251

+2.8V, Single-Supply, Cellular-Band Linear Power Amplifier

MAX2648

5GHz to 6GHz Low-Noise Amplifier in 6-Pin UCSP

MAX2661EVKIT

Evaluation Kit for the MAX2660, MAX2661, MAX2663, MAX2671

MAX2530

Quadruple-Mode PCS/Cellular/GPS LNA/Mixers

MAX2410EVKIT

Evaluation Kit for MAX2410

MAX2307EVKIT

Evaluation Kit for the MAX2307

MAX1471

315MHz/434MHz Low-Power, 3V/5V ASK/FSK Superheterodyne Receiver

MAX2660EVKIT

Evaluation Kit for the MAX2660, MAX2661, MAX2663, MAX2671

MAX2693L

GPS/GNSS Low-Noise Amplifiers with Integrated LDO

MAX2385

CDMA + GPS LNA/Mixers

MAX2670

GPS/GNSS Front-End Amplifier

MAX9989EVKIT

Evaluation Kit for the MAX9989, MAX9990

MAX2664

VHF/UHF Low-Noise Amplifiers

MAX2042A

SiGe, High-Linearity, 1600MHz to 3900MHz Upconversion/Downconversion Mixer with LO Buffer

MAX7044

300MHz to 450MHz High-Efficiency, Crystal-Based +13dBm ASK Transmitter

MAX19983A

Dual, SiGe, High-Linearity, High-Gain, 650MHz to 850MHz Downconversion Mixer with LO Buffer/Switch

MAX2361

Complete Dual-Band Quadrature Transmitters

MAX2654

1575MHz/1900MHz Variable-IP3 Low-Noise Amplifiers

MAX2822

2.4GHz 802.11b Zero-IF Transceiver with Integrated PA and Tx/Rx Switch

MAX2359

Quadruple-Mode PCS/Cellular/GPS LNA/Mixers

MAX77271

Multimode PA Step-Down Converter with Linear Bypass Mode

MAX2640

300MHz to 2500MHz SiGe Ultra-Low-Noise Amplifiers

MAX9982

825MHz to 915MHz, SiGe High-Linearity Active Mixer

MAX3509EVKIT

Evaluation Kit for the MAX3509

MAX2136

ISDB-T/DVB-T Low-IF Tuner

MAX2421

900MHz Image-Reject Transceivers

MAX9984EVKIT

Evaluation Kit for the MAX9984

MAX2753EVKIT

Evaluation Kit for the MAX2753

MAX2010

500MHz to 1100MHz Adjustable RF Predistorter

MAX2245EVKIT

Evaluation Kit for the MAX2244, MAX2245, MAX2246

MAX19790

250MHz to 4000MHz Dual, Analog Voltage Variable Attenuator

MAX2235EVKIT

MAX2235 Evaluation Kit

MAX2752

2.4GHz Monolithic Voltage-Controlled Oscillators

MAX2688

GPS/GNSS Low-Noise Amplifiers

MAX3541EVKIT

Evaluation Kits for the MAX3541 and MAX3542

MAX2351

Quadruple-Mode PCS/Cellular/GPS LNA/Mixers

MAX7030

Low-Cost, 315MHz and 433.92MHz ASK Transceiver with Fractional-N PLL

MAX9995

Dual, SiGe, High-Linearity, 1700MHz to 2700MHz Downconversion Mixer with LO Buffer/Switch

MAX2058

700MHz to 1200MHz High-Linearity, SPI-Controlled DVGA with Integrated Loopback Mixer

MAX2335EVKIT

Evaluation Kit for the MAX2335

MAX2335

450MHz CDMA/OFDM LNA/Mixer

MAX2503

Complete Cellular Baseband-to-RF Transmitters with PA

MAX2120EVKIT

Evaluation Kit for the MAX2120

MAX2362EVKIT

Evaluation Kit for the MAX2360, MAX2362, MAX2364

MAX9982EVKIT

Evaluation Kit for the MAX9982

MAX1473EVKIT

Evaluation Kit for the MAX1473

MAX2321

Adjustable, High-Linearity, SiGe, Dual-Band, LNA/Mixer ICs

MAX2608

45MHz to 650MHz, Integrated IF VCOs with Differential Output

MAX2694

GPS/GNSS Low-Noise Amplifiers

MAX2828EVKIT

Evaluation Kits for the MAX2828 and MAX2829

MAX2326EVKIT

Evaluation Kit for the MAX2320, MAX2321, MAX2322, MAX2324, MAX2326, MAX2327

MAX2680

400MHz to 2.5GHz, Low-Noise, SiGe Downconverter Mixers

MAX2471

10MHz to 500MHz, VCO Buffer Amplifiers with Differential Outputs

MAX2852

5GHz Receiver

MAX2557

Multiband, Multimode RF-to-Bits Femto-Basestation Radio Receiver

MAX2613

40MHz to 4GHz Linear Broadband Amplifiers

MAX2044

SiGe, High-Linearity, 2300MHz to 4000MHz Upconversion/Downconversion Mixer with LO Buffer

MAX7049EVKIT-868

Evaluation Kits for the MAX7049

MAX2308

CDMA IF VGAs and I/Q Demodulators with VCO and Synthesizer

MAX2114

DBS Direct Downconverter

MAX2388

W-CDMA LNA/Mixer ICs

MAX2663EVKIT

Evaluation Kit for the MAX2660, MAX2661, MAX2663, MAX2671

MAX2104

Direct-Conversion Tuner IC for Digital DBS Applications

MAX2206

RF Power Detectors in UCSP

MAX2667

GPS/GNSS Ultra-Low-Noise-Figure LNAs

MAX2264

2.7V, Single-Supply, Cellular-Band Linear Power Amplifiers

MAX2825

2.4GHz/5GHz, Single-Band and Dual-Band, 802.11g/a RF Transceiver ICs

MAX7060

280MHz to 450MHz Programmable ASK/FSK Transmitter

MAX2504EVKIT

Evaluation Kits for the MAX2500/03/04/04A/06/07/07A/09

MAX2140EVKIT

Evaluation Kit for the MAX2140

MAX9984

SiGe High-Linearity, 400MHz to 1000MHz Downconversion Mixer with LO Buffer/Switch

MAX3543EVKIT

Evaluation Kit for the MAX3543

MAX2370EVKIT

Evaluation Kit for the MAX2370

MAX9993EVKIT

Evaluation Kit for the MAX9993

MAX2470EVKIT

Evaluation Kit for the MAX2470, MAX2471

MAX2240

2.5GHz, +20dBm Power Amplifier IC in UCSP Package

MAX2701

1.8GHz to 2.5GHz, Direct-Downconversion Receivers

MAX9986AEVKIT

Evaluation Kit for the MAX9986A

MAX2310

CDMA IF VGAs and I/Q Demodulators with VCO and Synthesizer

MAX1470

315MHz Low-Power, +3V Superheterodyne Receiver

MAX2597

Femto-Basestation Bits-to-RF Radio Transmitter

MAX19793

1500MHz to 6000MHz Dual Analog Voltage Variable Attenuator with On-Chip 10-Bit SPI-Controlled DAC

MAX2391

W-CDMA/W-TDD/TD-SCDMA Zero-IF Receivers

MAX4002

2.5GHz 45dB RF-Detecting Controllers

MAX7057

300MHz to 450MHz Frequency-Programmable ASK/FSK Transmitter

MAX2374

SiGe, Variable IIP3, Low-Noise Amplifier in UCSP Package

MAX2769B

Universal GPS Receiver

MAX2364

Complete Dual-Band Quadrature Transmitters

MAX2653

GSM900 and DCS1800/PCS1900 Dual-Band, Low-Noise Amplifiers

MAX2358

Quadruple-Mode PCS/Cellular/GPS LNA/Mixers

MAX2393EVKIT

Evaluation Kit for the MAX2390, MAX2391, MAX2392, MAX2393, MAX2396, MAX2400

MAX7033

315MHz/433MHz ASK Superheterodyne Receiver with AGC Lock

MAX2312EVKIT

Evaluation Kit for the MAX2312, MAX2316

MAX2141

Low-Power XM Satellite Radio Receiver

MAX2643

900MHz SiGe, High-Variable IP3, Low-Noise Amplifier

MAX2500EVKIT

Evaluation Kits for the MAX2500/03/04/04A/06/07/07A/09

MAX1385

Dual RF LDMOS Bias Controllers with I²C/SPI Interface

MAX8805Z

600mA/650mA PWM Step-Down Converters in 2mm x 2mm WLP for WCDMA PA Power

MAX7057EVKIT

Evaluation Kit for the MAX7057

MAX2831EVKIT

Evaluation Kit for the MAX2831

MAX2503EVKIT

Evaluation Kits for the MAX2500/03/04/04A/06/07/07A/09

MAX2420

900MHz Image-Reject Transceivers

MAX2683EVKIT

Evaluation Kit for the MAX2683, MAX2684

MAX2506

Complete Cellular Baseband-to-RF Transmitters with PA

MAX9947EVKIT

Evaluation Kit for the MAX9947

MAX19997

Dual, SiGe, High-Linearity, High-Gain, 2300MHz to 2700MHz Downconversion Mixer with LO Buffer/Switch

MAX2566EVKIT

Evaluation Kit for the MAX2560, MAX2566, MAX2572

MAX8805

600mA/650mA PWM Step-Down Converters in 2mm x 2mm WLP for WCDMA PA Power

MAX2023

High-Dynamic-Range, Direct Up-/Downconversion 1500MHz to 2500MHz Quadrature Mod/Demod

MAX2410

Low-Cost RF Up/Downconverter with LNA and PA Driver

MAX2385EVKIT

Evaluation Kit for the MAX2385, MAX2386

MAX2741

Integrated L1-Band GPS Receiver

MAX5860

Scalable High-Density Downstream Cable QAM Modulator

MAX2506EVKIT

Evaluation Kits for the MAX2500/03/04/04A/06/07/07A/09

MAX2386EVKIT

Evaluation Kit for the MAX2385, MAX2386

MAX2057

1300MHz to 2700MHz Variable-Gain Amplifier with Analog Gain Control

MAX2616

40MHz to 4GHz Linear Broadband Amplifiers

MAX9947

AISG Integrated Transceiver

MAX2047

High-Gain Vector Multipliers

MAX9933

2MHz to 1.6GHz 45dB RF-Detecting Controllers and RF Detector

MAX2117

Complete, Direct-Conversion Tuner for MMDS Applications

MAX2324

Adjustable, High-Linearity, SiGe, Dual-Band, LNA/Mixer ICs

MAX2209

RF Power Detector

MAX3542EVKIT

Evaluation Kits for the MAX3541 and MAX3542

MAX2683

3.5GHz Downconverter Mixers with Selectable LO Doubler

MAX2851

5GHz, 5-Channel MIMO Receiver

MAX2267

+2.7V, Single-Supply, Cellular-Band Linear Power Amplifiers

MAX2112EVKIT

Evaluation Kit for the MAX2112

MAX2460

900MHz Image-Reject Transceivers

MAX2632

VHF-to-Microwave, +3V, General-Purpose Amplifiers

MAX3540EVKIT

Evaluation Kit for the MAX3540

MAX9994EVKIT

Evaluation Kit for the MAX9994

MAX2165

Single-Conversion DVB-H Tuner

MAX2039EVKIT

Evaluation Kit for the MAX2039

MAX2235

+3.6V, 1W Autoramping Power Amplifier for 900MHz Applications

MAX2367EVKIT

Evaluation Kit for the MAX2366, MAX2367, MAX2368

MAX2602

3.6V, 1W RF Power Transistors for 900MHz Applications

MAX2307

Low-Power, Cellular Upconverter-Driver

MAX2387

W-CDMA LNA/Mixer ICs

MAX2209EVKIT

Evaluation Kit for the MAX2209

MAX2666

Tiny Low-Noise Amplifiers for HSPA/LTE

MAX2426EVKIT

Evaluation Kit for the MAX2424, MAX2426

MAX2838

3.3GHz to 3.9GHz Wireless Broadband RF Transceiver

MAX2247EVKIT

Evaluation Kit for the MAX2247

MAX3509

Upstream CATV Amplifier

MAX2656

1575MHz/1900MHz Variable-IP3 Low-Noise Amplifiers

MAX2161EVKIT

Evaluation Kits for the MAX2161/MAX2162

MAX2837EVKIT

Evaluation Kit for the MAX2837

MAX9987

+14dBm to +20dBm LO Buffers/Splitters with ±1dB Variation

MAX2622EVKIT

Evaluation Kit for the MAX2622, MAX2623, MAX2624

MAX1473

315MHz/433MHz ASK Superheterodyne Receiver with Extended Dynamic Range

MAX19792

500MHz to 4000MHz Dual Analog Voltage Variable Attenuator with On-Chip 10-Bit SPI-Controlled DAC

MAX2390

W-CDMA/W-TDD/TD-SCDMA Zero-IF Receivers

MAX2653EVKIT

Evaluation Kit for the MAX2651, MAX2652, MAX2653

MAX2754

1.2GHz VCO with Linear Modulation Input

MAX2830

2.4GHz to 2.5GHz 802.11g/b RF Transceiver with PA and Rx/Tx/Diversity Switch

MAX2363

Complete Dual-Band Quadrature Transmitters

MAX9990

+14dBm to +20dBm LO Buffers with ±1dB Variation

MAX2090

50MHz to 1000MHz Analog VGA with Threshold Alarm Circuit and Error Amplifier for Level Control

MAX7032

Low-Cost, Crystal-Based, Programmable, ASK/FSK Transceiver with Fractional-N PLL

MAX2560EVKIT

Evaluation Kit for the MAX2560, MAX2566, MAX2572

MAX2642

900MHz SiGe, High-Variable IP3, Low-Noise Amplifier

MAX2374EVKIT

Evaluation Kit for the MAX2374

MAX8805Y

600mA/650mA PWM Step-Down Converters in 2mm x 2mm WLP for WCDMA PA Power

MAX2870EVKIT

Evaluation Kit for the MAX2870 and MAX2871

MAX19996

SiGe, High-Linearity, High-Gain, 2000MHz to 3000MHz Downconversion Mixer with LO Buffer

MAX2022

High-Dynamic-Range, Direct Up/Downconversion 1500MHz to 3000MHz Quadrature Modulator/Demodulator

MAX2120

Complete, Direct-Conversion Tuner for DVB-S and Free-to-Air Applications

MAX2244EVKIT

Evaluation Kit for the MAX2244, MAX2245, MAX2246

MAX2605EVKIT

Evaluation Kit for the MAX2605, MAX2606, MAX2607, MAX2608, MAX2609

MAX2180AEVKIT

Evaluation Kit for the MAX2180A

MAX2165EVKIT

MAX2165 Evaluation Kit

MAX2684EVKIT

Evaluation Kit for the MAX2683, MAX2684

MAX2839SEVKIT
MAX2720

1.7GHz to 2.5GHz, Direct I/Q Modulator with VGA and PA Driver

MAX2511

Low-Voltage IF Transceiver with Limiter and RSSI

MAX2615

40MHz to 4GHz Linear Broadband Amplifiers

MAX2740EVKIT

Evaluation Kit for the MAX2740

MAX2430EVKIT

Evaluation Kit for the MAX2430

MAX2046

High-Gain Vector Multipliers

MAX2316EVKIT

Evaluation Kit for the MAX2312, MAX2316

MAX2605

45MHz to 650MHz, Integrated IF VCOs with Differential Output

MAX2750AUA

2.4GHz Monolithic Voltage-Controlled Oscillator

MAX2242EVKIT

Evaluation Kit for the MAX2242

MAX2870

23.5MHz to 6000MHz Fractional/Integer-N Synthesizer/VCO

MAX2116

Complete DBS Direct-Conversion Tuner ICs with Monolithic VCOs

MAX2323

Triple/Dual-Mode CDMA LNA/Mixers

MAX3541

Complete Single-Conversion Television Tuner

MAX2106

DBS Direct Downconverter

MAX2208

RF Power Detectors in UCSP

MAX2602EVKIT

Evaluation Kit for the MAX2601, MAX2602

MAX2682

400MHz to 2.5GHz, Low-Noise, SiGe Downconverter Mixers

MAX2473

500MHz to 2500MHz, VCO Buffer Amplifiers

MAX2269EVKIT

Evaluation Kit for the MAX2267, MAX2268, MAX2269

MAX2392EVKIT

Evaluation Kit for the MAX2390, MAX2391, MAX2392, MAX2393, MAX2396, MAX2400

MAX2266

2.7V, Single-Supply, Cellular-Band Linear Power Amplifiers

MAX2754EVKIT

Evaluation Kit for the MAX2754

MAX1479EVKIT

Evaluation Kit for the MAX1479

MAX2645EVKIT

Evaluation Kit for the MAX2645

MAX2136A

Global Automotive TV Tuner

MAX2181

FM Automotive Low-Noise Amplifier

MAX2463

900MHz Image-Reject Transceivers

MAX2631

VHF-to-Microwave, +3V, General-Purpose Amplifiers

MAX2322EVKIT

Evaluation Kit for the MAX2320, MAX2321, MAX2322, MAX2324, MAX2326, MAX2327

MAX2685EVKIT

Evaluation Kit for the MAX2685

MAX2171

Direct-Conversion to Low-IF Tuners for Digital Audio Broadcast

MAX3580

Direct-Conversion TV Tuner

MAX2063

Dual 50MHz to 1000MHz High-Linearity, Serial/Parallel-Controlled Digital VGA

MAX7060EVKIT

Evaluation Kit for the MAX7060

MAX2900

200mW Single-Chip Transmitter ICs for 868MHz/915MHz ISM Bands

MAX2396EVKIT

Evaluation Kit for the MAX2396

MAX19997A

Dual, SiGe High-Linearity, High-Gain, 1800MHz to 2900MHz Downconversion Mixer with LO Buffer/Switch

MAX3524

Low-Noise, High-Linearity Broadband Amplifier

MAX19996A

SiGe, High-Linearity, 2000MHz to 3900MHz Downconversion Mixer with LO Buffer

MAX3514

Upstream CATV Amplifiers

MAX2669

GPS/GNSS Ultra-Low-Noise-Figure LNAs

MAX2837

2.3GHz to 2.7GHz Wireless Broadband RF Transceiver

MAX2551

Band II and V WCDMA Femtocell Transceiver with GSM Monitoring

MAX2366

Complete Dual-Band Quadrature Transmitters

MAX2655

1575MHz/1900MHz Variable-IP3 Low-Noise Amplifiers

MAX2827

2.4GHz/5GHz, Single-Band and Dual-Band, 802.11g/a RF Transceiver ICs

MAX9930EVKIT

Evaluation Kit for the MAX9930

MAX9986

SiGe High-Linearity, 815MHz to 995MHz Downconversion Mixer with LO Buffer/Switch

MAX2651EVKIT

Evaluation Kit for the MAX2651, MAX2652, MAX2653

MAX2645

3.4GHz to 3.8GHz SiGe Low-Noise Amplifier/PA Predriver

MAX2360EVKIT

Evaluation Kit for the MAX2360, MAX2362, MAX2364

MAX2320EVKIT

Evaluation Kit for the MAX2320, MAX2321, MAX2322, MAX2324, MAX2326, MAX2327

MAX2530EVKIT

Quadruple-Mode LNA/Mixer Evaluation Kits

MAX2242

2.4GHz to 2.5GHz Linear Power Amplifier

MAX2181A

FM Automotive Low-Noise Amplifier

MAX2324EVKIT

Evaluation Kit for the MAX2320, MAX2321, MAX2322, MAX2324, MAX2326, MAX2327

MAX2162S

ISDB-T 1- and 3-Segment Low-IF Tuners

MAX19999

Dual, SiGe High-Linearity, 3000MHz to 4000MHz Downconversion Mixer with LO Buffer

MAX2312

CDMA IF VGAs and I/Q Demodulators with VCO and Synthesizer

MAX2700EVKIT

Evaluation Kit for the MAX2700, MAX2701

MAX1472

300MHz-to-450MHz Low-Power, Crystal-Based ASK Transmitter

MAX2161S

ISDB-T 1- and 3-Segment Low-IF Tuners

MAX2599

Femto Basestation Bits-to-RF Radio Transmitter

MAX2406

Low-Cost Downconverter with Low-Noise Amplifier

MAX2207EVKIT

Evaluation Kit for the MAX2205, MAX2206, MAX2207, MAX2208

MAX2393

W-CDMA/W-TDD/TD-SCDMA Zero-IF Receivers

MAX2671

400MHz to 2.5GHz Upconverters

MAX2208EVKITS

Evaluation Kit for the MAX2205, MAX2206, MAX2207, MAX2208

MAX2009

1200MHz to 2500MHz Adjustable RF Predistorter

MAX2585

Advanced Multimode Complete RF-to-Baseband Receiver

MAX1472EVKIT

Evaluation Kit for the MAX1472

MAX2585EVKIT

MAX2585 Evaluation Kit

MAX2661

400MHz to 2.5GHz Upconverters

MAX2267EVKIT

Evaluation Kit for the MAX2267, MAX2268, MAX2269

MAX2160

ISDB-T Single-Segment Low-IF Tuners

MAX2649EVKIT

Evaluation Kit for the MAX2649

MAX2057EVKIT

Evaluation Kit for the MAX2057

MAX2338EVKIT

Evaluation Kit for the MAX2338

MAX2422

900MHz Image-Reject Transceivers

MAX3507EVKIT

Evaluation Kit for the MAX3507

MAX2326

Adjustable, High-Linearity, SiGe, Dual-Band, LNA/Mixer ICs

MAX2240EVKIT

Evaluation Kit for the MAX2240

MAX19985

Dual, SiGe, High-Linearity, High-Gain, 700MHz to 1000MHz Downconversion Mixer with LO Buffer/Switch

MAX2695

WLAN/WiMAX Low-Noise Amplifiers

MAX2685

Low-Cost, 900MHz, Low-Noise Amplifier and Downconverter Mixer

MAX7049EVKIT-433

Evaluation Kits for the MAX7049

MAX7058

315MHz/390MHz Dual-Frequency ASK Transmitter

MAX2584A

Complete RF-to-Baseband Receiver

MAX2634

315MHz/433MHz Low-Noise Amplifier for Automotive RKE

MAX8805WEVKIT

Evaluation Kit for the MAX8805W/X/Y/Z

MAX2065

50MHz to 1000MHz High-Linearity, Serial/Parallel-Controlled Analog/Digital VGA

MAX5862

High-Density Downstream Cable QAM Modulator

MAX2659EVKIT

MAX2659 Evaluation Kit

MAX2059

1700MHz to 2200MHz, High-Linearity, SPI-Controlled DVGA with Integrated Loopback Mixer

MAX2510

Low-Voltage IF Transceiver with Limiter RSSI and Quadrature Modulator

MAX2584AEVKIT

Evaluation Kit for the MAX2584A

MAX2309EVKIT

Evaluation Kit for the MAX2306, MAX2308, MAX2309

MAX2016EVKIT

Evaluation Kit for the MAX2016

MAX2500

Complete Cellular Baseband-to-RF Transmitters with PA

MAX3540

Complete Single-Conversion Television Tuner

MAX2169EVKIT

Evaluation Kit for the MAX2169

MAX2105

Direct-Conversion Tuner ICs for Digital DBS Applications

MAX2838EVKIT

Evaluation Kit for the MAX2838

MAX2160EVKIT

Evaluation Kit for the MAX2160

MAX2269

+2.7V, Single-Supply, Cellular-Band Linear Power Amplifiers

MAX9988EVKIT

Evaluation Kit for the MAX9987, MAX9988

MAX2363WEVKIT

Evaluation Kit for the MAX2361, MAX2363, MAX2365

MAX2117EVKIT

Evaluation Kit for the MAX2117

MAX9989

+14dBm to +20dBm LO Buffers with ±1dB Variation

MAX2548

Quad-Band TDD-WCDMA RF-to-Bits Radio Receiver

MAX12005

Satellite IF Switch

MAX2170

Direct-Conversion to Low-IF Tuners for Digital Audio Broadcast

MAX2620

10MHz to 1050MHz Integrated RF Oscillator with Buffered Outputs

MAX2245

2.5GHz, 22dBm/20dBm Power Amplifiers with Analog Closed-Loop Power Control

MAX2686L

GPS/GNSS Low-Noise Amplifiers with Integrated LDO

MAX2062

Dual 50MHz to 1000MHz High-Linearity, Serial/Parallel-Controlled Analog/Digital VGA

MAX2395

WCDMA Quasi-Direct Modulator with VGA and PA Driver

MAX2309

CDMA IF VGAs and I/Q Demodulators with VCO and Synthesizer

MAX2389

W-CDMA LNA/Mixer ICs

MAX2674

GPS/GNSS LNAs with Antenna Switch and Bias

MAX2203

RMS Power Detector

MAX2668

Tiny Low-Noise Amplifiers for HSPA/LTE

MAX2832

2.4GHz to 2.5GHz, 802.11g RF Transceivers with Integrated PA

MAX3503

Upstream CATV Amplifier

MAX2550

Band I, V, and VIII WCDMA Femtocell Transceiver with GSM Monitoring

MAX2365

Complete Dual-Band Quadrature Transmitters

MAX2658

GPS/GNSS Low-Noise Amplifiers

MAX2826

2.4GHz/5GHz, Single-Band and Dual-Band, 802.11g/a RF Transceiver ICs

MAX12000

1575MHz GPS Front-End Amplifier

MAX2321EVKIT

Evaluation Kit for the MAX2320, MAX2321, MAX2322, MAX2324, MAX2326, MAX2327

MAX2644

2.4GHz SiGe, High IP3 Low-Noise Amplifier

MAX2118EVKIT

Evaluation Kit for the MAX2116, MAX2118

MAX1386

Dual RF LDMOS Bias Controllers with I²C/SPI Interface

MAX2820A

2.4GHz 802.11b Zero-IF Transceivers

MAX19998

SiGe, High-Linearity, 2300MHz to 4000MHz Downconversion Mixer with LO Buffer

MAX9995EVKIT

Evaluation Kit for the MAX9995

MAX2314EVKIT

Evaluation Kit for the MAX2310, MAX2314

MAX2014

50MHz to 1000MHz, 75dB Logarithmic Detector/Controller

MAX2598

Quad-Band TDD-WCDMA Bits-to-RF Radio Transmitter

MAX19794

10MHz to 500MHz Dual Analog Voltage Variable Attenuator with On-Chip 10-Bit SPI-Controlled DAC

MAX2268EVKIT

Evaluation Kit for the MAX2267, MAX2268, MAX2269

MAX2500B

Complete Cellular Baseband-to-RF Transmitter with PA

MAX19985A

Dual, SiGe, High-Linearity, High-Gain, 700MHz to 1000MHz Downconversion Mixer with LO Buffer/Switch

MAX2392

W-CDMA/W-TDD/TD-SCDMA Zero-IF Receivers

MAX2206EVKIT

Evaluation Kit for the MAX2205, MAX2206, MAX2207, MAX2208

MAX2463EVKIT

Evaluation Kit for the MAX2420, MAX2421, MAX2422, MAX2460, MAX2463

MAX2660

400MHz to 2.5GHz Upconverters

MAX2150EVKIT

Evaluation Kit for MAX2150

MAX9981EVKIT

Evaluation Kit for the MAX9981

MAX3558EVKIT

Evaluation Kit for the MAX3558

MAX2650

DC-to-Microwave, +5V Low-Noise Amplifier

MAX2092

700MHz to 2700MHz Analog VGA with Threshold Alarm Circuit and Error Amplifier for Level Control

MAX7034

315MHz/434MHz ASK Superheterodyne Receiver

MAX3544EVKIT

Evaluation Kit for the MAX3544

Product Categories

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project