Power Supply Design Considerations for Primary Cell Powered Remote Patient Monitors

May 4 2022

Abstract

Remote patient monitors (RPMs) are continuously evolving to include more features that enable doctors to gain greater insights into their patients' health. These features create greater demands on the single-cell batteries that power the monitors. This article provides a power supply solution for an ECG remote patient monitoring patch that preserves battery life to take advantage of these features. The article also presents strategies to accurately estimate battery life for an RPM as well as ways to extend the battery life of the RPM before it is even powered on.

Introduction

The Internet of Things (IoT) revolution has allowed for a paradigm shift in the way healthcare providers leverage technology to provide their patients with real-time care. Today, remote patient monitoring is an area where new medical devices are changing the way doctors interact with their patients. Smaller ICs and wireless communication have enabled decades old devices to be updated to enhanced functional form factors that increase patient adherence and outcomes. Replacing clunky Holter devices of the past, current remote patient monitoring patches include a variety of sensors that gather heart rate, temperature, and accelerometer data. These patches transmit patient data to the cloud allowing patients and doctors to access the data in real time.

While these devices are increasing the ability for doctors to provide better care, they pose challenges for power supply designers who must balance system performance and battery life requirements. The challenges increase further as second-generation patches adopt multimodal sensing to improve accuracy and efficacy, which, in turn, increases the demands on the power supply.

In this article, we will refer to the ECG RPM patch example shown in Figure 1. This patch continuously monitors the ECG and accelerometer while checking the temperature every 15 minutes. The data are transmitted via Bluetooth® Low Energy (BLE) once every 2 hours for a total of 12 BLE transactions per day. This patch incorporates three different modes each with distinct load profiles: standard monitoring, temperature monitoring, and transmission modes. In standard monitoring mode, only the ECG and accelerometer are monitored. In temperature monitoring mode, an additional temperature sensor is monitored. In transmission mode, the BLE radio communicates the data while simultaneously monitoring the ECG and accelerometer data.

Figure 1. ECG patch power supply diagram. A 235 mAh CR2032 lithium coin cell battery provides power to the voltage regulators, microcontroller, ECG front end, temperature sensor, and accelerometer.

Power Supply Challenges

Designing an RPM, such as an ECG patch, poses multiple challenges for power supply designers. The design is typically space constrained and patches with several sensors may require multiple power rails. Because the RPM patch is usually intended to be a single-use item, a coin cell battery is typically the most cost-effective power source available to the designer. Using only a coin cell battery to supply power to the patch, a designer must also be cognizant of the efficiency of the power supply subsystem.

An often overlooked challenge for power supply designers is extending the shelf life of the product. Shutdown currents and battery self-discharge can shorten the life of any system. Therefore, it is important for a designer to determine if the RPM patch can meet operating time requirements after a typical shelf life period and, if it cannot, what steps can be taken to preserve battery life before the patch reaches the end user.

Determining Battery Run Time

To accurately determine if the power supply solution meets battery life requirements, a load profile must be determined. A load profile is a simple representation of the load duty cycle of the system. For the remote patient monitoring patch we’re using, we’ll consider the three different operating modes that were previously presented: standard monitoring, temperature monitoring, and transmission modes.

In standard monitoring mode, the current consumption of the patch shown in Figure 1 (including the 330 nA quiescent current of each buck converter and the current draw of the MCU) is 1.88 mA. In temperature monitoring mode, the current draw is 1.95 mA for 200 ms every 15 minutes. In transmission mode, the current draw is 7.90 mA for 30 seconds every 2 hours while the patch is transmitting data via BLE. These values can be found within the respective device data sheets by looking at active and quiescent current specifications.

To start the load profile analysis, a duty cycle calculation is determined using the time period for each operating mode during a day. Equation 1 is used:

Equation 01

Which gives us the duty cycles for our patch seen in Table 1.

Table 1. Duty Cycles for Patch Operating Modes
Operation Mode Duty Cycle
Temperature Measurement Percentage (%/Day) 0.02%
BLE Communication Percentage (%/Day) 0.42%
ECG Monitoring Duration (%/Day) 99.56%

Using the load profile in Figure 2, we can calculate the current consumption of the patch. Taking the active current consumption of each operating mode, the average current consumption per day can be approximated from Equation 2:

Figure 2. Load profile diagram.

Equation 02

Here is a sample calculation:

Standard Monitoring Mode Current per Day = Standard Monitoring Mode Current × Standard Monitoring Mode Duty Cycle × 24 Hours

Standard Monitoring Mode Current = 1.88 mA

Standard Monitoring Mode Duty Cycle = 0.9956

Standard Monitoring Mode Current per Day = 1.88 mA × 0.9956 × 24 Hours = 44.92 mAh/Day

Once each operating mode’s current consumption per day is found, the lifetime of the battery can be determined via Equation 3:

Equation 03

Here is a sample calculation:

Battery Capacity = 235 mAh

Standard Monitoring Mode Current per Day = 44.92 mAh/Day

Temperature Monitoring Mode Current per Day = 0.01 mAh/Day

Transmission Mode Current per Day = 0.79 mAh/Day

Battery Life (Days) = 235 mAh/(44.92 mAh/Day + 0.01 mAh/Day + 0.79 mA/Day) = 5.14 Days

The results of these calculations show that the device will meet the 5 day run-time requirements with a battery life of over 5.1 days. This is deceiving, however, as this does not consider the shelf life of the system. In the medical device industry, it is best practice to design for a 14-month shelf life (12 months on the shelf, two months in transit).

Shelf-Life Considerations

Summing the shutdown currents of the devices in the system while using the typical 1% to 2% per year self-discharge rate of a CR2032 battery, one can see that, after 14 months, the battery does not have enough capacity to support a 5-day run time and a battery seal is required.

Table 2. Battery Capacity After 14 Months
   
2% Battery Capacity Leakage (mAh) 230.30
Standby Current Consumption (mA) 0.0082
Shelf Life—Hours 28085.37
Shelf Life—Days 1170.22
Shelf Life—Years 3.21
Capacity After 14 Months (mAh) 146.66
Percent Capacity Left After 14 Months 63.68

The battery capacity after 14 months on the shelf will be severely diminished. Nearly 40% of the CR2032’s energy will be consumed by shutdown currents and battery self-leakage while sitting idle on the shelf. Inserting this battery capacity into Equation 3, a more accurate run time can be determined:

Battery Life (Days) = 146.66 mAh/(Standard Monitoring Mode + Temperature Monitoring Mode + Transmission Mode)

Battery Life (Days) = 146.66 mAh/(44.92 mAh/Day + 0.01 mAh/Day + 0.79 mA/Day) = 3.21 Days

While sitting on a shelf for over a year, the battery capacity is impacted by battery self-discharge and system shutdown currents. Battery self-discharge is a function of the battery chemistry and environment. A CR2032 battery has a lithium manganese chemistry and a self-discharge rate of 1% to 2% a year. At the end of a year, the coin cell battery can lose 2% of its capacity while sitting dormant. Meanwhile, a BR2032 battery has a lithium carbon monofluoride chemistry and a self-discharge rate of 0.3% per year. It is easy to assume that the best battery chemistry for the application is the one with the lowest discharge rate but that is not necessarily the case. While the BR2032 battery has a lower discharge rate, it also has a lower capacity than a CR2032 battery cell with 200 mAh. By recalculating using the previous formulas, one can determine if such a lower capacity battery is adequate.

In this ECG patch, the IC shutdown currents are the greatest contributors to reducing battery life while the system is powered off. Shutdown current is drawn when an IC is disabled and there is no active load. These currents are usually due to leakage in the IC and ESD protection devices within the IC that draw small amounts of current even when there is no load. These currents are usually small (under 1 μA) but can have a massive impact on battery life. In this RPM patch, shutdown currents can reduce battery capacity by as much as 40% in a year. A battery seal can be used to limit the system from drawing too much current from the battery while in shutdown.

Two common options for battery seals are mechanical battery seals in the form of a mylar pull tab and an electrical battery seal in the form of a load switch. Mylar/plastic pull tabs provide a mechanical battery seal where a plastic tab sits between the battery and the system. When the device is ready to be used, the user simply extracts the plastic tab and the battery begins powering the system. This is a simple, cheap, and proven mechanical battery seal that has been employed for many years. However, for medical devices, this solution is not always feasible. For an ECG patch where waterproofing is required, the slot that the mylar protrudes from can make the patch susceptible to water damage. In addition, the small plastic tab could potentially be difficult to use for an end user with low dexterity.

A simple load switch, like the Vishay SiP32341, would make an excellent choice for an electrical battery seal. This device is a FET that, when open, blocks the battery from the rest of the system leaving the SiP32341 shutdown current as the only draw on the battery. The load switch has a logic control line that can be turned on via push button when the device is ready to be used. The SiP32341 has a 14 pA typical shutdown current, which is a dramatic improvement over the current draw of the entire system if no battery seal were in place. When the SiP32341 is used as a battery seal, a CR2032 primary cell retains 99.97% of its capacity over the course of 14 months. When no battery seal is used to protect the battery from the ECG patch shutdown currents, a CR2032 primary cell only retains 62.39% of its original charge. This 37% difference in capacity is what allows for the ECG patch to meet the 5-day requirement after a 14-month shelf life.

Table 3. Battery Capacity After 14 Months with a Battery Seal
   
2% Battery Capacity Leakage (mAh) 230.30
Standby Current Consumption (mA) 0.000005
Shelf Life—Hours 46060000.00
Shelf Life—Days 1919166.67
Shelf Life—Years 5257.99
Capacity After 14 Months (mAh) 230.25
Percent Capacity Left After 14 Months 99.98

A battery seal preserves battery capacity by preventing all the devices in the system from drawing shutdown currents from the battery. Over 99.9% of the battery capacity is remaining after the RPM patch sits idle for 14 months.

Inserting this battery capacity into Equation 3, a more accurate run time can be determined:

Battery Life (Days) = 230.25 mAh/(Standard Monitoring Mode + Temperature Monitoring Mode + Transmission Mode)

Battery Life (Days) = 230.25 mAh/(44.92 mAh/Day + 0.01 mAh/Day + 0.79 mA/Day) = 5.04 Days

Conclusion

The battery analysis of a system when it is active and when it is in shutdown/low power mode is critical to designing a power supply that will meet all the requirements for a medical device. While this article exclusively discussed an ECG patch that gathers heart rate, temperature, and acceleration data with BLE communication, the analysis and principles within this article can be applied to any number of medical device systems powered by a primary cell battery.

About the Authors

Fahad Masood
Fahad Masood is a senior applications engineer for health and medical biosensing applications at Analog Devices. He has nearly a decade of experience in electronics development for healthcare, computing, and industrial app...
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Industry Solutions
Product Categories

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project