Pushbutton On/Off Controller Provides µProcessor Reset Monitor and Input Supply Monitoring
Pushbutton On/Off Controller Provides µProcessor Reset Monitor and Input Supply Monitoring
Oct 1 2007
Introduction
System designers often grapple with ways to debounce and control the on/off pushbutton of portable devices. Traditional debounce designs use discrete logic, flip-flops, resistors and capacitors. Some designs require an onboard microprocessor to monitor the pushbutton, but this puts a burden on the microprocessor—if it hangs up, all device on/off control is lost. Also, in high voltage, multicell battery applications the low voltage circuits require an LDO power supply. In the end, what should be a simple monitoring circuit consumes an oversized share of the space and complexity of the system. Plus, its draw on the power budget is high even when the system is off, since the microprocessor must keep awake, constantly watching the pushbutton.
The LTC2953 pushbutton on/off controller with voltage monitoring alleviates the headaches of discrete implementations and provides a self-contained alternative to microprocessor based pushbutton monitoring. The LTC2953 integrates all the flexible timing circuits needed to debounce the on/off pushbutton of portable systems and provides a simple yet powerful interface that allows for controlled power up and power down.
The part also includes input and output supply monitors. A power fail comparator issues an early warning when it detects a low battery condition, while a UVLO comparator prevents a user from applying system power from a dead battery (or low supply). Additionally, an adjustable single supply supervisor provides a 200ms reset output delay after the monitored supply rises above the programmed voltage.
The LTC2953’s wide input voltage range (2.7V to 27V) is designed to operate from single-cell to multicell battery stacks, thus eliminating the need for a high voltage LDO. The part’s features allow the system designer to turn off power to all circuits except the LTC2953, whose very low quiescent current (14µA typical) extends battery life. The device is available in a space saving 12 lead 3mm × 3mm DFN package.
Orderly Power On
The pushbutton input of the LTC2953 controls the logic state of the open drain enable output. Figure 1 shows the EN output of the LTC2953-1 driving a DC/DC converter. To turn on system power, the pushbutton input must be debounced (held low continuously for at least 32ms). See the timing diagram shown in Figure 2. Note that once power has been enabled, the system must set the KILL input high within 512ms.

Figure 1. A complete pushbutton and voltage monitoring system is easy to set up with the LTC2953-1.

Figure 2. Timing diagram shows a pushbutton-controlled system power on.
Orderly Power Off
The LTC2953 provides two ways to manually turn off system power: issuing an orderly power off request, and forcing an immediate power off. An orderly power off involves a simple push and release of the on/off button. For instance, for the circuit in Figure 1, if an end user is using an MP3 player, he presses and releases the on/off button, which subsequently drives the INT output low for a minimum of 32ms. The system logic that monitors the LTC2953’s INT output then initiates various pre-powerdown and housekeeping tasks, and asserts KILL low when all is well. The LTC2953 then shuts down the DC/DC converter—turning off system power. See the timing diagram shown in Figure 3.

Figure 3. Timing diagram for normal power off sequence.
The other type of shutdown is a manual reset. This allows the user to force power off if the system logic or µP fails to respond to the interrupt signal. To do so, the end user presses and holds the pushbutton down. The length of time required to force a power down is given by a fixed internal 64ms delay plus an adjustable power down timer delay. The adjustable delay is set by placing an optional external capacitor on the PDT pin. See Figure 4.

Figure 4. Timing diagram for forced power off, in the case where the user must bypass system logic control.
Power Fail Comparator Issues Low Supply Warning
The LTC2953 provides an uncommitted power fail comparator that can serve as the first warning of a decaying battery or a low supply. The PFO output is driven low when the PFI input voltage drops below 0.5V. This comparator provides real time supply information and does not affect the functionality of the enable and interrupt outputs. A system designer can use the power fail comparator to identify the source of a power down interrupt request: the pushbutton or the UVLO. If the PFO output is low when the interrupt output is asserted, then the UVLO input initiated the power down request (see Figure 5).

Figure 5. De-glitched UVLO comparator monitors battery stack.
UVLO Comparator Rejects Short Supply Glitches
The application shown in Figure 5 monitors a 2-cell Li-Ion battery stack. The UVLO comparator has glitch immunity to prevent short spikes on the supply line from issuing a power down request. All glitches shorter than 32ms are ignored. If the battery voltage drops below 5.4V for longer than 32ms, however, the LTC2953 asserts the interrupt output for a minimum of 32ms. When both INT and PFO are driven low, this alerts the system logic that a significant battery glitch has occurred. For cases where the battery voltage falls and stays below 5.4V for an indefinite length of time, the LTC2953 automatically shuts off system power. See the Figure 6 timing diagram.

Figure 6. Low supply initiates system power down and locks out enable.
UVLO Locks Out Pushbutton Input
The LTC2953 prevents a user from turning on system power with a dead battery or low supply. If system power is off and the voltage on the UVLO input is below 0.5V, the pushbutton input is ignored. This means that if a battery or supply drops below a predetermined adjustable level, the LTC2953 does not allow system power on (see Figure 6 timing diagram).
Pushbutton Controlled Supply Sequencing
The circuit in Figure 7 uses the LTC2953-2 to sequence three supply rails. Power on supply sequencing begins by pressing the pushbutton for 32ms. This asserts the EN output low, which turns on the V1 supply.

Figure 7. Pushbutton controlled supply sequencing.
Using the reset comparator and 200ms after V1 reaches 80% of its final value (2.66V), the V2 supply is enabled. When the V2 DC voltage reaches 80% of its final value (2V), the V3 supply in enabled.
A user initiates a power down supply sequence by again pressing the pushbutton for 32ms. When EN is released and pulls up to VIN, V1 disconnects first. When the V1 supply decays to 2.66V, V2 is immediately disabled (there is no delay from VM to RST during power down supply sequencing). When V2 decays to 2V, V3 is immediately disabled (see the timing diagram in Figure 8).

Figure 8. Timing diagrams for sequencing three supplies.
LTC2953-1 and LTC2953-2 Versions
The LTC2953-1(EN) and LTC2953-2(EN) differ only by the polarity of the EN/EN pin. The LTC2953-1 is intended to drive a DC/DC converter while the LTC2953-2 drives an external power PFET.
Pushbutton Product Family
Table 1 summarizes Linear Technology’s family of pushbutton products. The LTC2950, LTC2951 and LTC2954 provide a complete standalone solution for interfacing a manual on/off pushbutton to system power and system logic. The LTC2953 adds voltage monitoring functions to allow for failsafe operation. The LTC2952 offers selectable dual power path ideal diode controllers.
Part Number | Supply Voltage (V) | Supply Current (µA) | ON Timer | OFF Timer | Kill Timer | Comments | Package |
LTC2950 | 2.7 to 26 | 6 | Adj | Adj | 1024ms | Active high enable output (LTC2950-1) Active low enable output (LTC2950-2) |
TSOT-8 DFN-8 |
LTC2951 | 2.7 to 26 | 6 | 128ms | Adj | Adj | Active high enable output (LTC2951-1) Active low enable output (LTC2951-2) |
TSOT-8 DFN-8 |
LTC2952 | 2.7 to 28 | 25 | Adj | Adj | Extendable | Pushbutton PowerPath controller with system monitoring | TSSOP-20 QFN-20 |
LTC2953 | 2.7 to 27 | 14 | 32ms | Adj | Pushbutton controller with supply monitor, UVLO and power fail comparators | DFN-12 | |
LTC2954 | 2.7 to 26 | 6 | Adj | Adj | Interrupt logic for menu driven applications. Active high enable output (LTC2954-1) Active low enable output (LTC2954-2) |
TSOT-8 DFN-8 |
Conclusion
The LTC2953 is a low power, wide input voltage range (2.7V to 27V) pushbutton on/off controller with input and output voltage monitoring. The LTC2953 provides a simple and complete solution to manually toggling power to many types of systems. It includes a power fail comparator that issues an early warning of a decaying supply, along with a UVLO comparator that prevents a user from turning on a system with a low supply or dead battery. The LTC2953 furthers system reliability by integrating an adjustable single supply supervisor. The device is available in a space saving 3mm × 3mm DFN package.
About the Authors
Victor Fleury is a senior design engineer in the Mixed Signal Products Group at Analog Devices. He has specialized in high voltage and high speed products during his 18 years in the Industry. Victor holds a BSEE from MIT a...