Why Now is a Good Time to Secure Your Embedded Systems with SHA-3

Feb 26 2019

Abstract

Published by the National Institute of Standards and Technology (NIST), Secure Hash Algorithms continue to evolve to provide increasingly stronger levels of cryptography-based security. The latest iteration, SHA-3, has a new internal computational structure as compared to previous NIST-specified hash algorithms to address known vulnerabilities of its predecessors. As embedded systems become smarter and more connected, it’s more critical than ever to safeguard them from attack. SHA-3 can help; however, implementing cryptographic hash functions can be challenging without a background in cryptography. This white paper discusses the merits of SHA-3 and highlights how secure authenticators designed with SHA-3 algorithms and physically unclonable function (PUF) technology can provide strong embedded security without requiring cryptography expertise. Read full article.

Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Product Categories

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project