Design Note 11: Testing Linearity of the LTC2400 24-Bit No Latency Delta Sigma A/D Converter Help from the Nineteenth Century
Introduction
Verifying the linearity of the LTC2400 analog to digital converter requires special considerations. Typical nonlinearity is only 2ppm (0.0002%). Bench testing this necessitates some form of voltage source that produces equal amplitude output steps for incremental digital inputs. Additionally, for measurement confidence, it is desirable that the source be substantially more linear than the 2ppm requirement. This is, of course, a stringent demand and painfully close to the state of the art.
The most linear “D to A” converter is also one of the oldest: Lord Kelvin’s Kelvin-Varley divider (KVD), in its most developed form, is linear to 0.1ppm. This manually switched device features ten million individual dial settings arranged in seven decades. It may be thought of as a 3-terminal potentiometer with fixed “end-to-end” resistance and a 7-decade switched wiper position (Figure 1).
Figure 1. Conceptual Kelvin-Varley Divider.
Figure 2. A 4-Decade Kelvin-Varley Divider. Additional Decades Are Implemented By Opening Last Switch, Deleting Two Associated 80Ω Values and Continuing ÷ 5 Resistor Chains.
Figure 3. KVD with Buffer Gives Output Drive Capability.
Figure 4. Error Budget Analysis for the KVD Buffer. Selection Permits ≈0.4ppm Predicted Linearity Error.
Figure 5. Simplified High Linearity Voltage Source.
The voltmeters, specified for <1ppm nonlinearity on the 10V range, “vote” on the source’s output. Figure 6 is a more detailed schematic and Figure 7 highlights issues and concerns.
Figure 6. Complete High Linearity Voltage Source.
Figure 7. Voltage Source Notes and Special Attention Areas.
When studying the approach used, it is essential to differentiate between linearity and absolute accuracy. This eliminates concerns with absolute standards, permitting certain freedoms in the measurement scheme. In particular, although single-point grounding was used, remote sensing was not. This is a deliberate choice, made to minimize the number of potential error-causing parasitic thermocouples in the signal path.
Results
This KVD-based, high linearity voltage source has been in use in our lab for about a year. During this period, the total linearity uncertainty defined by the source and its monitoring voltmeters has been just 0.3ppm (see Figure 8). This is almost ten times better than the LTC2400’s 2ppm specification, promoting confidence in our measurements.
Figure 8. Linearity Testing Using Repeated Trials with “Voting” Voltmeters.
謝辞
The author is indebted to Lord Kelvin and to Warren Little of the C. S. Draper Laboratory (formerly the M. I. T. Instrumentation Laboratory) standards lab. Warren taught me, with great patience, the wonders of KVDs some thirty years ago and I am still trading on his efforts.