Designed, Built, Tested
Board pictured here has been fully assembled and tested.

Overview

設計リソース

設計/統合ファイル

  • Schematic
  • PCB Layout
  • BOM
  • IODD
Download IODD files 107 KB
設計ファイルのダウンロード 1.53 M

評価用ボード

型番に"Z"が付いているものは、RoHS対応製品です。 本回路の評価には以下の評価用ボードが必要です。

  • MAXREFDES177# ($74.31) EV Kit
在庫確認と購入

説明

MAXREFDES177#为完备的IO-Link®通用模拟输入/输出(IO)参考设计,采用内置保护功能的MAX22515 IO-Link收发器。参考设计用于演示软件可完全配置的模拟IO模块,该模块采用了MAX22000工业级可配置模拟IO器件。MAX14483数字隔离器和隔离电源将模拟(现场)侧与IO-Link侧完全隔离,电源取自于IO-Link主机连接的 L+ (24V)电源。

MAXREFDES177#参考工业规格设计,使用工业标准M12连接器,提供4线IO-Link电缆。模拟(现场)侧使用4向PCB接线端子。完整的参考设计适合61mm x 25mm印刷电路板(PCB)。

可配置模式包括AIO和GND端子之间的模拟电压输入(±10V)、模拟电流输入(±20mA)、模拟电压输出(±10V)和模拟电流输出(±20mA)。MAXREFES177#将线性范围设置为标称范围的105%,满幅范围为125%。在±50°C温度波动范围内,精度保持在0.1%内。其他两个端子可配置为使用PT100或PT1000 RTD等标准器件测量温度。这些端子通过输入AI5和AI6连接到MAX22000的集成可编程增益放大器(PGA)。

Atmel® ATSAM低功耗连接器连接在MAX22000工业级可配置模拟IO器件和MAX22515 IO-Link设备收发器之间。MAX22515集成浪涌保护,支持可靠通信,占用极小的PCB面积,无需TVS二极管等外部保护元件。MAX22515采用微小、20焊球晶圆级封装(WLP),使MAXREFDES177#具有较小的外形尺寸。设计利用MAX22515集成有源极性反接保护电路实现极性反接保护。MAX22515内部包含2个集成LDO稳压器(3.3V和5V),3.3V LDO产生3.3V电源,用于其他电路供电,减少所需的外部元件、节省空间。MAX22515提供低导通电阻的驱动电路(C/Q和DO/DI),以降低功耗,使参考设计功耗最小、发热极低。

该IO-Link器件采用“Technologie Management Gruppe Technologie und Engineering (TMG TE)” IO-Link设备栈与任意IO-Link V1.1兼容主机通信。电路板包括M12头连接器,可通过标准M12电缆连接至IO-Link兼容主机。通过其他软件将MAXREFDES177#连接到USB IO-link主机,例如MAXREFDES165#,便于系统评估。

从设计资源标签页可下载设计文件、固件及软件。提供电路板供用户购买。

機能と利点

  • 符合IEC 61131-9标准
  • TMG TE IO-Link设备协议栈
  • 兼容IO-Link V1.1
  • 通用模拟IO
  • 集成电气隔离

Details Section

Introduction

Advanced factory automation solutions (Industry 4.0) require an increasing number of smart sensors and smart actuators, which are typically controlled using IO-Link point-to-point serial communication between the sensor/actuator and controller (master). Analog Devices, as a leading provider of IO-Link sensor transceivers and master transceiver ICs, also provides complete reference design solutions to help its customers improve their time to market. These proven designs cover all the hardware and software requirements needed for compliance with the IO-Link standard.

IO-Link is the first open, field bus agnostic, low-cost, point-to-point serial communication protocol used for communicating with sensors and actuators that has been adopted as an international standard (IEC 61131-9). IO-Link standardizes the interoperability of industrial equipment worldwide. IO-Link can function directly from the PLC or be integrated into all standard field buses, making it the de-facto standard for universally communicating with smart devices like the MAXREFDES177#.

A true field-configurable, universal IO is realized when the field programmability of the IO-Link is combined with a software-configurable IO. Industrial sensor/actuator OEMs can thus provide end users total flexibility at the factory floor level to simplify equipment installation and commissioning, while reducing their number of SKUs and BOMs, and simplifying and streamlining their purchasing and manufacturing.

Analog Devices and TMG TE collaborated to design the MAXREFDES177# reference design compliant with the IO-Link version 1.1/1.0 standard. The MAXREFDES177# design has an industry-standard MAX22515 IO-Link device transceiver, an Atmel ATSAM low-power microcontroller that uses the TMG TE IO-Link device stack, and a MAX22000 industrial universal analog IO device that is fully software configurable for all common industrial analog input and output, voltage and current ranges. The complete reference design fits on a 61mm x 25mm printed circuit board (PCB).

Detailed Description of Hardware

The MAXREFDES177# IO-Link universal analog IO consumes minimal power, space, and cost, making it a complete solution for the many analog input sensors or analog output actuators found in various industrial control and automation applications.

The MAX22515 IO-Link device transceiver is compliant with the IO-Link version 1.1/1.0 physical-layer specification. It integrates the high-voltage functions commonly found in industrial sensors, including drivers, and two linear regulators, all in a tiny 2.5mm x 2.0mm WLP. The MAX22515 has extensive integrated protection to ensure robust communication in harsh industrial environments. All four I/O pins (V24, C/Q, DO/DI, and GND) are reverse-voltage, short-circuit protected, and have integrated ±1kV/500Ω surge protection. Thus, a very small PCB area is needed with no required external protection components such as TVS diodes. The low on-resistance driver (C/Q) further reduces power dissipation so that this reference design consumes minimal power with very low thermal dissipation. Operation is specified for normal 24V supply voltages up to 36V. Transient protection is simplified due to high voltage tolerance (i.e., 65V absolute maximum rating) in addition to the integrated surge protection.

The two integrated LDO regulators in the MAX22515 generate 3.3V and 5V, reducing the number of additional external components and required space.

The MAX22515 features a flexible control interface through either an SPI or I2C interface. The I2C interface is used in this reference design to reduce the number of pins required by the microcontroller. The I2C interface provides extensive diagnostics for the MAX22515. A 3-wire UART interface is provided for IO-Link communication.

The MAXREFDES177# does not require external protection devices such as varistors or TVS diodes due to the integrated surge protection in the MAX22515 at the IO-Link interface. This reference design meets both the IEC 61000-4-2 for electrostatic discharge (ESD) up to ±4kV and IEC 61000-4-4 for electrical fast transient (EFT) ±4kV standards. It is designed to meet a surge capability (2A at t = 1.2/50μs) up to ±1.0kV. Additional TVS protection circuitry is included as part of the analog IO (field side) circuit.

The MAXREFDES177# uses an industry-standard M12 connector with a 4-wire cable.

The MAX22000 is an industrial-grade configurable analog input/output device configurable on-the-fly in software as a voltage/current input or output. Additional inputs are available to measure other analog signals. The device offers an 18-bit DAC with fast settling time as well as a 24-bit delta-sigma ADC. The ADC and DAC can individually choose between an internal or an external reference. This design uses the internal voltage reference. The MAX22000 can meet an accuracy of 0.1% over a ±50°C temperature variation because of the very stable 5ppm/°C internal reference. The MAX22000 sets the linear range at 105% and full-scale range at 125% of the nominal range. For example, the MAX22000 provides a linear range of ±10.5V and a full-scale range of ±12.5V for a nominal range of ±10V.

The MAX22000 supports the ADC with a low-noise PGA with high-voltage and low-voltage input ranges to support RTD measurements. Additional auxiliary inputs are also present, and in this design, implement on-board diagnostic measurement for the HVDD supply.

The MAX22000 communicates through a high-speed SPI bus for all configuration and management information as well as conversion results. An optional 8-bit CRC enhances the reliability of the SPI interface, protecting against all 8-bit bursts as well as all double-bit errors. The MAX22000 operates from 2.7V to 3.6V analog and digital supplies, and up to ±24V high-voltage supplies. The device is available in a 64-pin LGA package and operates over the -40°C to +125°C industrial temperature range.

Galvanic isolation between the IO-Link side (microcontroller) and the analog IO (field side) is provided by the MAX14483 for data isolation. A switched DC-DC is based around the MAX13256 transformer driver for power isolation.

The MAX14483 is a 6-channel, low-power, 3.75kVRMS SPI digital isolator. The six signal channels are individually optimized for SPI applications, and include very low propagation delay on the SDI, SDO, and SCLK channels. Two extra channels are used in this design for RDY feedback from the MAX22000 and for RST to allow the MCU to provide a software reset to the MAX22000. The MAX14483 is available in a 20-pin SSOP package with 5.5mm creepage and clearance.

The Atmel microcontroller limits the reference design operating temperature range from -40°C to +105°C. However, the MAX22515 IO-Link transceiver, MAX22000, and MAX14483 can all operate over the -40°C to +125°C temperature range.

Refer to the MAX22000 and MAX14483 data sheets for detailed information on the software-configurable analog IO device and digital isolator.


Power Supplies

Power solutions use Analog Devices ICs and modules to generate the various voltage rails on both the IO-Link and field sides of the isolation barrier (Figure 2). Power is supplied from the IO-Link cable on L+ and is nominally 24V on the IO-Link side. The MAX22515 has two internal LDOs, which can step down this 24V rail. However, a more efficient solution is realized by using a tiny MAXM17552 compact step-down power module to create a 5V input to the MAX22515, which then uses an integrated LDO to generate the 3.3V rail. The MAXM17522 is available in a low-profile, compact 10-pin 2.6mm x 3mm x 1.5mm µSLIC package.

The MAX13256 H-bridge transformer driver is a simple solution to make isolated power supplies up to 10W. The device drives a transformer's primary coil with up to 300mA of current from a wide 8V to 36V DC supply. The device is available in a small 10-pin (3mm x 3mm) TDFN package and is specified over the -40°C to +125°C temperature range.

The transformer's secondary-to-primary winding ratio defines the output voltage, allowing the selection of virtually any isolated output voltage. Two supplies, HVDD = +24V and HVSS = -24V, are generated in this design. For this design the same supplies are used for HVDDO and HVSSO respectively. On the analog or field side, a MAXM17522 is used to step down the HVDD rail to 3.3V for the DVDD and AVDD requirements of MAX22000.

The MAXREFDES177# consumes 30mA to 35mA (typ) under normal conditions, and more if the current input or output mode is selected. A red LED indicates a power fault on the transformer driver while an additional green LED indicates the presence of AVDD supply.


Detailed Description of Firmware

The MAXREFDES177# is shipped preprogrammed as a working IO-Link device ready to connect to an IO-Link master. The firmware targets an Atmel ATSAM microcontroller and follows the simple flowchart in Figure 3. The firmware utilizes the TMG TE IO-Link device stack. The MAXREFDES177# waits for a wake-up signal from the IO-Link master after plug-in. The MAXREFDES177# synchronizes to the IO-Link master using the 230.4kbps (COM3) baud rate on receiving the wake-up signal. The communication parameters are exchanged. The IO-Link master then starts a cyclic data exchange by requesting the sensor process data. The IO-Link master detects a missing sensor if the MAXREFDES177# is removed.


Figure 3. MAXREFDES177# firmware flowchart.

Figure 3. MAXREFDES177# firmware flowchart.


The TMG TE IO-Link Device Tool software is Windows®-compatible, features IODD file import capability, connects to a PC through USB, and is available to download from the TMG TE website.

The TMG TE IO-Link Device Tool software is shown in Figure 4. A complete guide is also downloadable from the TMG TE website.


Figure 4. The TMG TE IO-Link device tool.

Figure 4. The TMG TE IO-Link device tool.


The source code for the MAXREFDES177# is not available. The TMG TE IO-Link stack is shipped preprogrammed inside the MAXREFDES177# hardware with a perpetual license.

The TMG TE contact information is:
Technologie Management Gruppe
Technologie und Engineering GmbH
Zur Giesserei 10
76227 Karlsruhe
Germany
Phone: +49 7218 28060
E-Mail: willems@tmgte.de
Internet: www.tmgte.com


Detailed Description of Software

The MAXREFDES177# was verified using the MAXREFDES165# IO-Link Master, featuring the MAX14819 IO-Link master transceiver and IODD interpreter tool IO-Link Device Tool from the TMG TE website.

Download the IODD file (*.xml) located in the Design Resources tab. Follow the step-by-step instructions in the Quick Start Guide section to use the software. Figure 4 is a screenshot of the TMG TE IO-Link Device Tool communicating with the master and sensor.

EMC Testing

The general rules for the test configuration of a device (such as the MAXREFDES177#) are as follows:

  • The SDCI cable shall be unshielded, 20m long, coiled, and placed 10cm (4in) above the ground plane.
  • The devices shall be placed 10cm (4in) above the ground plane.

The MAXREFDES177# was tested in a Analog Devices lab for the common industrial compliance standards, and the test methodology and results are presented in this document. Although the IO-Link Interface and System Specification does not require surge testing, Analog did this test in addition to the ESD and EFT tests.


Equipment Used:

  • MAXREFDES177# IO-Link Sensor
  • MAXREFDES165# 4-Port IO-Link Master
  • 20m M12 Cable
  • Haefely® Technology ECOMPACT4 EFT/Surge Generator
  • Teseq® CDN 117 Signal Line Coupling Network
  • Teseq CDN 3425 EFT Data Line Coupling Clamp
  • Teseg NSG438 ESD Generator

Surge Testing

The MAXREFDES177# module was tested to withstand up to ±1.0kV of 1.2/50µs IEC 61000-4-5 surge with a total source impedance of 500Ω. The surge testing was performed using the MAXREFDES165# IO-Link master. Ten surge pulses were applied for each test (Table 1 and Table 2).

The MAXREFDES177# continued to operate normally (executed code and transferred data) and was not damaged by the tests. The MAX22515 registers were not corrupted while communicating with the master during the tests shown in Table 1. Analog Devices also tested the analog IO (field side) (Table 2) in addition to testing the IO-Link side.


Table 1. Surge test results for the IO-Link interface.
Test Condition Surge Tests
L+ TO GND C/Q TO GND L+ TO CQ
+1kV Pass Pass Pass
-1kV Pass Pass Pass

Table 2. Surge test results for the analog IO interface.
Test Condition Surge Tests
AIO TO AGND AIO TO SNS+ AIO TO SNS-
+1.2kV Pass Pass Pass
-1.2kV Pass Pass Pass

EFT/Burst Testing

The MAXREFDES177# was tested to withstand electrical fast transient (EFT)/bursts up to ±4kV according to IEC 61000-4-4 with a 20m IO-Link cable with standard M12 connectors. The EFT testing was performed using the MAXREFDES165# IO-Link master. The EFT pulses were applied for one minute for each test (Table 3).


Table 3. EFT/Burst test results.
Test Condition 5kHz/15ms 100kHz/0.75ms
+4kV Pass Pass
-4kV Pass Pass

ESD Testing

The MAXREFDES177# was tested to withstand electrostatic discharge (ESD) for Contact and Air-Gap Discharge up to ±4kV according to IEC 61000-4-2. The ESD testing was performed on the MAXREFDES177# M12 connector pins after the test operation was verified using the MAXREFDES165# IO-Link master to transfer data (Table 4). The MAXREFDES177# was not damaged by any ESD tests and continued to operate normally.


Table 4. ESD test results.
Test Condition L+ TO GND C/Q TO GND
+4kV Contact Discharge Pass Pass
-4kV Contact Discharge Pass Pass
+4kV Air-Gap Discharge Pass Pass
-4kV Air-Gap Discharge Pass Pass

The IO-Link interface and system specification version 1.1.2 requires ESD testing with a 20m cable attached, and the ESD strike is applied to the sensor casing. Because this reference design is only a PCB with no metallic casing, the ESD strikes were applied to the male M12 connector pins. Analog Devices expects this design to meet the levels specified in Table 4 when testing with a casing and cable.


Restrictions and Warnings for Analog Devices Reference Design Use

The MAXREFDES177# is designed and tested to meet IO-Link operation and harsh industrial environments covered by the IEC 61000-4-x standards for transient immunity. This board and associated software are designed to be used to evaluate the performance of the MAX22515 and MAX22000 but are not intended to be deployed as-is into an end product in a factory automation system.

The MAXREFDES177# is not for use in functional safety or safety-critical systems.

Quick Start Guide

Connect the MAXREFDES177# universal analog IO to a port of an IO-Link master to test it. The following example uses a MAXREFDES165# IO-Link master and TMG software tool. However, any IO-Link compliant master and associated IO-Link device GUI should work.


Required Equipment

Supplied by Analog

  • MAXREFDES177#

Note: Download the IODD files from the Design Resources tab.

User Supplied

  • IO-Link master (i.e., MAXREFDES165#) with a 24V AC-to-DC power adapter
  • TMG TE IO-Link Device Tool software
  • One IO-Link cable
  • Windows 10 PC with a USB port
  • Digital multimeter (at least 6.5 digit DMM is recommended)
  • Adjustable DC power supply

Master Setup Procedure

  1. Connect the MAXREFDES177# sensor to the IO-Link master with an IO-Link M12 cable.
  2. Connect the IO-Link master to the PC with a USB cable.
  3. Download and install the latest IO-Link Device Tool software from the TMG TE website.
  4. Download the IODD file for the MAXREFDES177# from the Design Resources tab or from the TMG TE website.
  5. The MAXREFDES177# comes preprogrammed with firmware and the IO-Link device stack.

Sensor Testing Procedure

  1. Connect the female end of the IO-Link cable to the MAXREFDES177#.
  2. Connect the male end of the IO-Link cable to one of the ports on the IO-Link master.
  3. Open the IO-Link Device Tool software and click Search Master (Figure 4). Select the 4-port master (MAXREFDES165#) found by the tool.
  4. Import the IODD file for the MAXREFDES177#. This includes a picture of the PCB (Figure 5).
  5. Click Go Online (Figure 4).
  6. The IO-Link Device Tool software shows the IO-Link master connection if communication is established correctly. Select the port number the MAXREFDES177# is connected to and click Check Devices below the Ports section. The software shows the MAXREFDES177# is connected, Click Takeover devices into engineering in Check Devices (Figure 6).
  7. The Go Offline button is green. The software tool shows that the device is MAXREFDES177# and the IODD vendor is TMG TE GmbH (Figure 7).
  8. Double-click port 1 (for this example) to open the window with the MAXREFDES177# sensor details. Select the Process Data tab.
  9. Select the mode (analog output voltage) (Figure 8 and Figure 9). Enter a value between -10 and +10 and read the voltage with a DMM connected to the AIO and AGND terminals. The output voltage is 1V in this example.
  10. Select the mode desired – in this case (analog input voltage). Apply a DC voltage (from an adjustable power supply for example) to terminals AIO and AGND. In this example we set the voltage to approximately 4V. Read the voltage (Figure 10). It reads 4.00414V in this example.
  11. Due to the very high accuracy of the DAC and ADC in MAX22000, it is recommended to use a 6.5 digit or better DMM to measure the external voltages to experience the high precision of the MAX22000 and MAXREFDES177#.
  12. It is recommended to perform a two-point calibration for the voltage/current input and output functions and to store the calibration coefficients in the on-board memory to utilize the full performance of MAXREFDES177#. Refer to the MAX22000 data sheet for the MAX22000 gain and offset calibration details, and the various registers used.

Figure 5. MAXREFDES177# IODD file.

Figure 5. MAXREFDES177# IODD file.


Figure 6. MAXREFDES177# sensor found.

Figure 6. MAXREFDES177# sensor found.


Figure 7. MAXREFDES177# sensor connected to the master.

Figure 7. MAXREFDES177# sensor connected to the master.


Figure 8. MAXREFDES177# analog output modes.

Figure 8. MAXREFDES177# analog output modes.


Figure 9. MAXREFDES177# analog data values.

Figure 9. MAXREFDES177# analog data values.


Figure 10. MAXREFDES177# analog input modes.

Figure 10. MAXREFDES177# analog input modes.


Calibration Procedure for Voltage Input and Output

This calibration procedure takes care of the voltage input/output mode simultaneously. The DAC generates a voltage, which is measured back through the ADC. The voltage is measured with a precision voltmeter. The results are entered in the PDOut field. The MAXREFDES177# then calculates the calibration factors for the analog input/output. It stores these parameters in the non-volatile memory on the board. Follow the steps in the sequence or the calibration fails.

  1. Select Calibrate Voltage High Point in the Parameter tab under Device function (Function 11).
  2. Click a different text box to finish the selection.
  3. Click the yellow arrow to write all changed values to device.

  4. Figure 11. Calibrating the voltage high point.

    Figure 11. Calibrating the voltage high point.


  5. Measure the voltage on the connector X2 between the pins 1 and 4 using a precision voltmeter. The voltage must be approximately +10V.
  6. Select the Process Data tab and enter the measured voltage into Process data output (Figure 12).
  7. Figure 12. Calibrating the voltage output.

    Figure 12. Calibrating the voltage output.

  8. Select Calibrate Voltage Low Point in the Parameter tab under Device function.
  9. Click a different text box to finish the selection.
  10. Click the yellow arrow to write all changed values to device.
  11. Measure the voltage on the connector X2 between pins 1 and 4 using a precision voltmeter. The voltage must be approximately -10V.
  12. Select the Process Data tab and enter the measured voltage into Process data output.
  13. Select High Z in the Parameter tab under Device function.
  14. Click a different text box to finish the selection.
  15. Click the yellow arrow to write all changed values to device.
  16. The MAXREFDES177# calculates the calibration factors for the DAC and ADC voltage modes. It stores them in the non-volatile memory on the board. Each time MAXREFDES177# powers up, the microcontroller copies these calibration factors to the MAX22000 to avoid the need to calibrate the design again.

Calibration Procedure for Current Input and Output

This calibration procedure takes care of the current input/output mode simultaneously. The DAC generates a current, which is measured back through the ADC. The current is measured with a precision ammeter. The results are entered in the PDOut field. The MAXREFDES177# then calculates the calibration factors for the analog input/output. It stores these parameters in the non-volatile memory on the board. Follow the steps in the sequence or the calibration fails.

  1. Select Calibrate Current High Point in the Parameter tab under Device function (Figure 13).
  2. Click a different text box to finish the selection.
  3. Click the yellow arrow to write all changed values to device.

  4. Figure 13. Calibrating the current high point.

    Figure 13. Calibrating the current high point.


  5. Measure the current on the connector X2 between the pins 1 and 4 using a precision ammeter. The current must be approximately +20mA.
  6. Select the Process Data tab and enter the measured current into Process data output (Figure 14).

  7. Figure 14. Calibrating the current output.

    Figure 14. Calibrating the current output.


  8. Select Calibrate Current Low Point in the Parameter tab under Device function.
  9. Click a different text box to finish the selection.
  10. Click the yellow arrow to write all changed values to device.
  11. Measure the current on the connector X2 between the pins 1 and 4 using a precision ammeter. The current must be approximately -20mA.
  12. Select the Process Data tab and enter the measured current into Process data output.
  13. Select High Z in the Parameter tab under Device function.
  14. Click a different text box to finish the selection.
  15. Click the yellow arrow to write all changed values to device.
  16. The MAXREFDES177# calculates the calibration factors for the DAC and ADC (mA) current modes. It stores them in the non-volatile memory on the board.

Trademarks

  • Atmel is a registered trademark and registered service mark of Atmel Corporation.
  • Haefely is a registered trademark of Haefely Test AG.
  • IO-Link is a registered trademark of Profibus User Organization (PNO).
  • Maxim is a registered trademark of Maxim Integrated Products, Inc.
  • µSLIC is a trademark of Maxim Integrated Products, Inc.
  • Teseq is a registered trademark of Ametek CTS.
  • Windows is a registered trademark of Microsoft Corporation.

Support & Training

Search our knowledge base for answers to your technical questions. Our dedicated team of Applications Engineers are also available to answer your technical questions.