Power Supply Subsystems for Photoplethysmography Remote Patient Vital Sign Monitors—Part 1
Power Supply Subsystems for Photoplethysmography Remote Patient Vital Sign Monitors—Part 1
2024-12-18
Read other articles in this series.
摘要
This two-part article presents validated switch-mode power circuit designs for remote patient vital sign monitoring applications, including biosensors with excellent system signal-to-noise performance. “Power Supply Subsystems for Photoplethysmography Remote Patient Vital Sign Monitors—Part 1” shows a discrete solution for best performance and “Power Supply Subsystems for Photoplethysmography Remote Patient Vital Sign Monitors—Part 2” features an integrated solution for space-constrained applications.
➤ Learn how to select a power supply configuration based on photoplethysmogram (PPG) system requirements.
➤ Review the implementation of switch-mode power supply reference circuits for both discrete (Part 1) and integrated designs (Part 2).
➤ See a power supply performance test methodology that validates the system over different device use cases and transient loading conditions.
➤ Get a checklist to validate the implementation.
➤ Gain troubleshooting knowledge to address implementation issues.
Introduction
This two-part article presents prevalidated power supply circuit designs for PPG remote patient vital sign monitoring applications, including biosensors with excellent system signal-to-noise performance. A PPG device can be implemented to measure blood volume changes from which vital sign information such as blood oxygen levels and heart rates are derived. In Part 1, we provide discrete power supply circuit design solutions for best performance using the MAX86171 optical pulse oximeter and heart-rate sensor analog front end (AFE). In Part 2, we will show an integrated solution for space-constrained applications.
Switch-mode power supplies (also referred to as SMPS or DC-to-DC converters) are commonly used in wearable medical and healthcare applications for reasons such as size considerations and power efficiency. Designers can use these power supplies to create battery-operated products that achieve longer lifetimes. Unfortunately, designers are still left to select the appropriate SMPS device followed by creating a suitable circuit board layout that preserves the performance of a biosensing device in their system.
To simplify and speed the process, Analog Devices offers power supply subsystem circuit designs that have been prevalidated (that is, designed, built, and tested) to ensure the signal-to-noise ratio (SNR) performance of each biosensing AFE device. This article provides details for the power supply circuits with each example being complemented with a validation checklist and troubleshooting guide to aid circuit designers if needed. Figure 1 shows a standard power block diagram encountered in many remote-patient monitoring applications. Table 1 reveals the design limits, and Table 2 shows the design considerations for discrete and integrated solutions.
Input | Output (VDIG, VANA, VLED) | Noise, RTO | ||
VIMIN | VIMAX | VOMIN | VOMAX | V p-p(max) |
3.0 V1 | 4.2 V1 | 1.6 V | 2.0 V | 30 mV p-p |
2.0 V2 | 3.4 V2 | 1.6 V | 2.0 V | 30 mV p-p |
4.7 V | 5.3 V | 20 mV p-p |
Note:
1Secondary cell battery (LiPo)
2Primary cell battery (Li coin cell)
Design Configuration | Battery Implementation | Board Area Layout Considerations |
Discrete | Primary (coin cell) Secondary (Li and LiPo) |
Implements separate discrete circuits |
Integrated | Secondary (Li and LiPo) | Uses single integrated circuit for minimal board area requirements Supports secondary batteries only |
Discrete Design Description
This DC-to-DC converter design regulates the three-output power supply rails for use in a remote patient vital sign monitor subsystem. The circuit provides proper line and load regulation while maintaining low output noise levels to preserve biosensing SNR performance, which is powered by a rechargeable lithium polymer (LiPo) battery or a primary Li cell battery. Figure 2 shows the PPG subsystem using discrete power supply devices and Table 3 lists the main components.
Designator | Component | Description |
U1 | DC-to-DC converter | Power converter device (MAX38640A and MAX20343H) |
L1 | 2.2 μH inductor | Low equivalent series resistance (ESR) inductor (energy) storage component1 |
C1 | 22 μF capacitor | Low ESR capacitor (energy) storage component1 |
1L1 and C1 are specially selected passive components that are critical to the performance of the DC-to-DC converter (also known as, switch-mode power supply).
1.8 V SMPS Circuit Using a Nanopower Buck Converter
The following circuit based on the MAX38640A nanopower buck converter (Figure 3) shows the typical input and output power supply level to properly operate the SMPS device in remote patient vital sign monitor applications. As shown in Figure 3, a digital multimeter (DMM) can be used to probe the input and output ports to validate the supply voltage levels. The power supply output levels can vary due to various factors such as:
➤ Discharging battery
➤ Changing loads (that is, device mode changes, devices waking up from sleep mode, etc. )
1.8 V SMPS Circuit Validation Checklist
The circuit validation checklist (Table 4) is intended to help designers with their electrical bench checkout of the 1.8 V SMPS circuit post circuit board assembly (see Figure 4). This checklist can also be used as a template for product testing.
Table 4 can be used as a checklist to validate the operation of the analog or digital 1.8 V SMPS circuit using the MAX38640A device while connected to a biosensing circuit load.
Step | Action | Procedure | Measurement | Need Help? |
1 | Check the input DC power supply | Measure voltage across the battery | Reading range: | For troubleshooting instructions, see below |
LP401230 LiPo batt | 3.0 V to 4.2 V | |||
CR2032 Li coin batt | 2.0 V to 3.4 V | |||
2 | Check the input DC power supply | Measure voltage across CIN | Reading range: | |
LP401230 LiPo batt | 3.0 V to 4.2 V | |||
CR2032 Li coin batt | 2.0 V to 3.4 V | |||
3 | Check VOUT DC level | Measure voltage across COUT | Reading range: 1.71 V to 1.89 V | |
4 | Measure voltage across the load | Reading range: 1.71 V to 1.89 V | ||
5 | Check output noise level | Use pigtail 10× single-ended probe or differential active probe | Ripple noise level should be < 20 mV p-p |
Troubleshooting the MAX38640A (1.8 V Output) SMPS Circuit
The following circuit troubleshooting instructions will help designers if operational issues arise with the operation of the 1.8 V SMPS circuit (see Figure 5). This guide addresses the most common problems that arise in implementing these switch-mode power supplies.
Troubleshooting the MAX38640A SMPS Circuit
Step 1—Check the input voltage: Using a digital multimeter (DMM) with an internal impedance of 1 MΩ or larger (for example, Fluke 87), measure the voltage across at the input to the MAX38640A device. Be sure to connect the negative black lead to the ground and the positive red lead to the input IN pin of the device. If the input pin is not easily accessible, place the leads across the input capacitor, CIN.
Use Table 5 to diagnose and fix associated problems:
Input Voltage Reading | Potential Cause | Action | Notes |
Zero volts/no reading | Battery uncharged or battery defective | Disconnect the battery and check the voltage; if it reads 0 V, recharge the battery | Replace the battery if it doesn’t charge |
No connection from the battery (IN or GND line) | Disconnect the battery and test for conductivity from the battery connector to the device input | PCB may have an open | |
Input capacitor shorted to ground | Disconnect the battery and check for continuity across the capacitor | Bad capacitor; PCB may have short | |
EN pin connected to ground | Disconnect the battery and test for conductivity from the EN pin to ground | EN pin needs to be tied high for normal operation | |
Reading < 3.0 V (LiPo battery) Reading < 2.0 V (Li-Ion battery) |
Low battery charge or battery defective | Disconnect the battery and check the voltage; if it reads below 2.8 V, recharge the battery | Replace the battery if it doesn’t charge |
3.0 V ≥ reading ≤ 4.2 V (LiPo battery) 2.0 V ≥ reading ≤ 3.4 V (Li-Ion battery) |
No action | Input voltage OK, proceed to Step 2 | |
Reading ≥ 4.2 V (LiPo battery) Reading ≥ 3.4 V (Li-Ion battery) |
Defective battery | Replace the battery |
Step 2—Check the inductor signal waveform: Using an oscilloscope or digital storage scope (DSO), probe the LX pin on the MAX38640A device. If the input pin is not easily accessible, place the probe on the inductor end capacitor.
Note: It is recommended that the oscilloscope and probes used have a minimum bandwidth of 200 MHz.
If the circuit is operating with a light load (that is, less than 50 mA), the waveform should appear as shown in Figure 6.
If the circuit is operating with a heavy load, the waveform should be a square wave with minimal ringing on the rise and falling edges as shown in Figure 7.
The square wave amplitude should be approximately equal to the input battery voltage. The square wave floor voltage should be about 200 mV to 300 mV below ground (for example, –250 mV). The duty cycle is proportional to the output voltage. Thus, a 3.6 V input battery voltage will have an approximate 50% duty cycle when producing an output voltage of 1.8 V. Figure 8 shows the relationship between the duty cycle and the output voltage.
Deviations from the ideal square wave can be used to effectively diagnose and fix many problems.
Use Table 6 to diagnose and fix associated problems:
Input Waveform | Potential Cause | Action | Notes |
Amplitude is not correct | Inductor open; IN pin open EN is open or ground | Disconnect the battery and check all connections with DMM | Repair PCB if needed |
The duty cycle is not correct (doesn’t correlate to the output voltage) | RSEL (768 kΩ) is not the correct value; bad external resistor | Disconnect the battery and check RSEL with a DMM (R-measurement) | Replace resistor with correct value resistor |
RSEL pin open (VO = 2.5 V) | Check the output for 2.5 V; disconnect the battery and test for conductivity from the resistor to RSEL pin | PCB may have an open |
|
RSEL pin shorted to ground (VO = 0.8 V) | Check the output for 0.8 V; disconnect the battery and measure the resistance across the capacitor | PCB may have short |
|
Waveform distortion Rounded rising edge | Bad inductor connection | Reconnect the inductor; replace the inductor | Bad connection can cause higher line resistance |
Step 3A—Check the output DC voltage: Using a DMM with an internal impedance of 1 MΩ or larger (for example, Fluke 87), measure the voltage at the output of the MAX38640A device. Be sure to connect the negative black lead to the ground and the positive red lead to the output OUT pin of the device. If the output pin is not easily accessible, place the leads across the output capacitor, COUT.
Use Table 7 to diagnose and fix associated problems:
Output Voltage Reading | Potential Cause | Action | Notes |
Zero volts/no reading | No connection from SMPS to COUT | Disconnect the battery and test for conductivity from output to COUT | PCB may have an open |
Output capacitor shorted to ground | Disconnect the battery and check for continuity across the capacitor | PCB may have short | |
Reading too low (< 1.71 VDC) |
Inductor wrong value; inductor saturated RSEL(768 kΩ) has wrong value | Disconnect the battery and check for the inductor and/or resistor values | |
1.71 V ≥ reading ≤ 1.89 V | No action | Operational | |
Reading too high (> 1.89 VDC) | RSEL(768 kΩ) has wrong value | Disconnect the battery and check RSEL value |
Step 3B—Check the output AC voltage: Using an oscilloscope or DSO, now measure the output ripple (AC) by probing the OUT pin on the MAX38640A device. To properly measure the output and minimize RF pickup, it is recommended that 10× pigtail probes be used. Differential active probes can also be used to reduce ambient noise further.
Note: It is recommended that the oscilloscope and probes used have a minimum bandwidth of 200 MHz.
If the circuit is operating correctly, the waveform should be a 1.8 VDC output with a small ripple waveform superimposed on it. Figure 9 shows the ripple waveform.
Use Table 8 to diagnose and fix associated problems:
Input Waveform | Potential Cause | Action | Notes |
Ripple amplitude is too high (> 20 mV p-p) |
Wrong capacitor value; defective capacitor | Disconnect the battery and check all connections with DMM; measure capacitor value | |
Ripple frequency doesn’t match VLX square wave frequency | Light load | Check load | |
Broadband noise is too high | Load too large; environmental noise | Check load and environmental noise | Use pigtail 10× probe or active differential probing on output to reduce environmental noise |
Transition spikes too high (> 30 mV p-p) |
Load inductance; input current not adequate | Check line inductance; check input current with scope |
5.0 V SMPS Circuit Using a Low Noise Buck-Boost Converter
The following circuit based on the MAX20343H low noise buck-boost converter shows the typical input and output power supply levels for a properly operating SMPS device in remote patient vital sign monitor applications. As shown in Figure 10, a DMM can be used to probe the input and output ports to validate the supply voltage levels. The power supply output levels can vary due to various factors such as:
➤ Discharging battery
➤ Changing loads (that is, device mode changes, devices waking up from sleep mode, etc.)
5.0 V SMPS Circuit Validation Checklist
The following circuit validation checklist (Table 9) is intended to help designers with their electrical bench checkout of the 5.0 V SMPS circuit (see Figure 10) post circuit board assembly. This checklist can also be used as a template for product testing.
Table 9 can be used as a checklist to validate the operation of the analog 5.0 V SMPS circuit using the MAX20343H device while connected to a biosensing circuit load.
Step | Action | Procedure | Measurement | Need help? |
1 | Check the input DC power supply | Measure voltage across the battery | Reading range: | Troubleshooting instructions |
LP401230 LiPo batt | 3.0 V to 4.2 V | |||
CR2032 Li coin batt | 2.0 V to 3.4 V | |||
2 | Check the input DC power supply | Measure voltage across CIN | Reading range: | |
LP401230 LiPo batt | 3.0 V to 4.2 V | |||
CR2032 Li coin batt | 2.0 V to 3.4 V | |||
3 | Check VOUT DC level | Measure voltage across COUT | Reading range: 4.75 V to 5.25 V | |
4 | Check VOUT DC level | Measure voltage across the load | Reading range: 4.75 V to 5.25 V | |
5 | Check output noise level | Use pigtail 10× single-ended probe or differential active probe | Ripple noise level should be < 20 mV p-p |
5.0 V SMPS Circuit Troubleshooting Guide
The following circuit troubleshooting instructions (Figure 11) will help designers if operational issues arise with the operation of the 5.0 V SMPS circuit. This guide addresses the most common problems that arise in implementing these switch-mode power supplies.
Troubleshooting the MAX20343H SMPS Circuit
Step 1—Check the input voltage: Using a DMM with an internal impedance of 1 MΩ or larger (for example, Fluke 87), measure the voltage across at the input to the MAX20343H device. Be sure to connect the negative black lead to the ground and the positive red lead to the input IN pin of the device. If the input pin is not easily accessible, place the leads across the input capacitor, CIN.
Use Table 10 to diagnose and fix associated problems:
Input Voltage Reading | Potential Cause | Action | Notes |
Zero volts/ no reading | Battery uncharged; battery defective | Disconnect the battery and check voltage; if it reads 0 V, recharge the battery | Replace battery if it doesn’t charge |
No connection from the battery (IN or GND line) | Disconnect the battery and test for conductivity from the battery connector to the device input | PCB may have an open | |
Input capacitor shorted to ground | Disconnect the battery and check for continuity across the capacitor | PCB may have short | |
EN pin (SDA/EN) connected to ground | Disconnect the battery and test for conductivity from the battery connector to the device input | EN pin needs to be tied high for normal operation | |
Reading < 2.8 V | Low battery charge; battery defective | Disconnect the battery and check the voltage; if it reads below 2.8 V, recharge the battery | Replace battery if it does not charge |
2.8 V ≥ reading ≤ 4.2 V | No action | Input voltage OK; proceed to Step 2 | |
Reading ≥ 4.2 V | Defective battery | Replace battery |
Step 2—Check the inductor signal waveform: Using an oscilloscope or DSO, probe the HVLX pin on the MAX20343H device. If the input pin is not easily accessible, place the probe on the inductor end cap.
Note: It is recommended that the oscilloscope and probes used have a minimum bandwidth of 200 MHz.
If the circuit is operating correctly, the waveform should be a pulse wave with minimal ringing on the rise and falling edges as shown in Figure 12.
The 500 ns pulse wave amplitude should be approximately equal to the input battery voltage. The pulse wave floor voltage should be within 100 mV of the ground. The output frequency and duty cycle of the pulse wave are proportional to the load current. Figures 13 and 14 show the output wave and signal frequency under different load conditions.
Deviations from the ideal square wave can be used to effectively diagnose and fix many problems.
Use Table 11 to diagnose and fix associated problems:
Input Waveform | Potential Cause | Action | Notes |
Amplitude is not correct | Inductor open; IN pin open; EN is open or ground | Disconnect the battery and check all connections with DMM | Repair PCB if needed |
Duty cycle is not correct (doesn’t correlate to the output voltage) | RSEL (6.65 kΩ) is not the correct value; bad external resistor | Disconnect the battery and check RSEL with a DMM (R-measurement) | Replace the resistor with the correct value resistor |
RSEL pin open (VO = 3.3 V) | Check the output for 3.3 V; disconnect the battery and test for conductivity from the resistor to RSEL pin | PCB may have an open |
|
RSEL pin shorted to ground (VO = 5.5 V) | Check the output for 5.5 V; disconnect the battery and measure resistance across the capacitor | PCB may have short | |
Waveform distortion Rounded rising edge | Bad inductor connection | Reconnect the inductor; replace the inductor | Bad connection can cause higher line resistance |
Step 3A—Check the output DC voltage: Using a DMM with an internal impedance of 1 MΩ or larger (for example, Fluke 87), measure the voltage at the output of the MAX20343H device. Be sure to connect the negative black lead to the ground and the positive red lead to the output OUT pin of the device. If the output pin is not easily accessible, place the leads across the output capacitor, COUT.
Use Table 12 to diagnose and fix associated problems:
Output Voltage Reading | Potential Cause | Action | Notes |
Zero volts/ no reading |
No connection from SMPS to COUT | Disconnect the battery and test for conductivity from the output to COUT | PCB may have an open |
Output capacitor shorted to ground | Disconnect the battery and check for continuity across the capacitor | PCB may have short | |
Reading too low (< 4.75 VDC) |
Inductor wrong value; inductor saturated RSEL(6.65 kΩ) has the wrong value | Disconnect the battery and check for the inductor and/or resistor values | |
4.75 V ≥ reading ≤ 5.25 V |
No action | Operational | |
Reading too high (> 5.25 VDC) |
RSEL (6.65 kΩ) has the wrong value | Disconnect the battery and check RSEL value |
Step 3B—Check the output AC voltage: Using an oscilloscope or DSO, now measure the output ripple (AC) by probing the OUT pin on the MAX20343H device. To properly measure the output and minimize RF pickup, it is recommended that 10× pigtail probes be used. Differential active probes can also be used to reduce ambient noise further.
Note: It is recommended that the oscilloscope and probes used have a minimum bandwidth of 200 MHz.
If the circuit is operating correctly, the waveform should be a 1.8 VDC output with a small ripple waveform superimposed on it. Figure 15 shows the ripple waveform.
Use Table 13 to diagnose and fix associated problems:
Input Waveform | Potential Cause | Action | Notes |
Ripple amplitude is too high | Wrong capacitor value; defective capacitor | Disconnect the battery and check all connections with DMM; measure capacitor value | |
Ripple frequency doesn’t match VHVLX pulse wave frequency | Light load | Check load | |
Broadband noise is too high | Load too large; environmental noise | Check load and environmental noise | Use pigtail 10× probe or active differential probing on output to reduce environmental noise |
Transition spikes too high | Load inductance; input current not adequate | Check line inductance; check input current with scope |
Conclusion
This concludes part one of the two-part article in which prevalidated discrete power supply circuits were presented for use with the MAX86171-based PPG remote patient vital sign monitor. These power supply circuits can be used with MAX86141-based PPG devices as well. In Part 2, we present prevalidated integrated power supply circuits for use with both MAX86171-based and MAX86141-based PPG remote patient vital sign monitors.
References
“Power Supply Subsystems for Vital Sign Monitors.” Analog Devices, Inc., January 2022.
“Designing Accurate, Wearable Optical Heart Rate Monitors.” Analog Devices, Inc., August 2017.
Frenzel, Lou. “Improving Remote Patient Monitoring to Overcome Healthcare Limitations.” Electronic Design, November 2020.
关于作者
关联至此文章
行业解决方案
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}