signals header
A woman with blue sound waves coming from her mouth as she presenting during a meeting and a pair of biam speakers detecting her voice.
A woman with blue sound waves coming from her mouth as she presenting during a meeting and a pair of biam speakers detecting her voice.

SIGNALS+ 在线快讯订阅

持续关注Signals+,了解有关连接、数字健康、电气化和智能工业的最新见解、信息和想法并加以利用。

您可以随时通过单击由ADI公司发送的电子邮件中的退订链接,或者通过ADI隐私设置来更改您的设置。

谢谢您的订阅,请查看您的邮箱确认邮件并完成注册.

您将实时接收突破性技术如何在全球范围内产生深远影响!

关闭

混合办公模式的增强式音频会议体验


Audio conferencing has become a ubiquitous way to connect workplace teams that are spread across locations and time zones worldwide. Even close to home, many employees are seeking flexibility through remote and hybrid roles, and this trend is here to stay.1

Yet conference rooms have been one of the last corners of the workplace to adapt. Installing new AV equipment can require significant time and capital outlays, and office reconfiguration can disrupt employee productivity. To avoid this, many companies continue to depend on outdated equipment, analog cables, or installations they’ve simply outgrown.

Professional audiovisual (pro AV) company Biamp teamed up with longtime partner Analog Devices, Inc. (ADI) to co-create a solution. The Parlé audio conferencing system leverages ADI’s A2B audio bus technology to connect multiple, distributed microphone nodes to a central processor over a single wire. With A2B, the superior quality of digital audio was only one wire away, helping Biamp resolve a connectivity bottleneck and unlock novel audio-conferencing applications.

概览

公司简介

45年来,Biamp一直致力于打造专业视听解决方案,助力高效沟通。从小型会议舱到超大型会场,Biamp的愿景始终如一:在每一个空间里,促进真挚的人际交流。

挑战

会议室技术升级往往耗资巨大、耗时费力,还会中断正常工作。理想的解决方案应该降低企业的升级门槛,助其轻松实现音频会议体验的现代化。

目标

借助出色的数字音频技术,为新一代员工打造更人性化的会议室,改善远程或混合办公模式下的员工体验。

解决方案

ADI帮助Biamp改进了Parlé的A2B音频总线解决方案,为会议桌面带来了简洁的单线缆连接、强大的多通道性能以及实时的配置能力。

选择错误音频设备的隐性成本

视听设备能够连接团队,提高现代工作场所的生产力——前提是设备运行正常。一旦设备出现故障,造成的损失可能非常严重——尤其是在音频方面,因为即使没有画面,会议也能勉强进行,但如果没有清晰的对话,会议就失去了意义。

$40,000
根据全球研究机构IPSOS的调查,员工超过100人的大型公司每年音频会议质量问题造成的损失估计达到4万美元。2

糟糕的音频效果平均每周会浪费员工半小时的时间,并让员工感到烦恼,导致工作效率降低。累计下来,每人每年因此损失的时间相当于3个完整的工作日。对于公司来说,这意味着每年可能要付出数万美元的代价3。不仅如此,劣质的音频还会损害公司声誉,甚至可能在业务关系开始之前就造成负面影响4。因此,配置优质的音频会议设备是一项具有长远价值的投资。

PARLÉ愿景

Biamp明白,全面升级视听系统并非易事。即使更好的视听技术日益普及,相关的安装成本仍可能让许多公司对升级望而却步。

正因如此,Biamp构想了一种兼顾出色、自然的音频体验,又能降低编程、安装和调试难度的音频会议解决方案,而ADI公司的 A2B技术帮助Biamp实现了两全其美的方案。

A woman with blue sound waves coming from her mouth as she's teaching a college course and a of biam speakers detecting her voice.

BIAMP和ADI:齐心协力谋求解决之道

十多年来,Biamp一直采用ADI的数字信号处理器(DSP),尤其是SHARC®DSP。Biamp希望新一代音频系统可以支持多个信号通道和复杂的波束成形算法,然而,连接性能成为了瓶颈。波束成形技术可用于识别发言者,并追踪他们在房间内的走动。

传统的连接,例如USB和AoIP(Audio over IP,即通过IP技术传输音频),都有其局限性。ADI的现场应用工程师(FAE)推荐了 A2B 技术。 Biamp发现,A2B 能够通过可配置的数字互连传输高质量音频,从而有效提升产品的灵活性,使其经得起未来考验。


解决方案和考虑事项

An icon that represents bluetooth.
USB连接
  • 庞大的协议维护软件栈限制了可扩展性。
  • 灵活性有限,每增加一个节点都需要单独布线。
An icon to represent Audio over IP (AoIP).
AoIP (Audio over IP)
  • 每个节点都需要单独的软件,导致部署和维护的成本较高,且更加复杂。
  • 此外还要求使用一套由兼容的网络、扬声器和功放组成的生态系统。
An icon that has the text A2B.
A2B
  • 完全硬件同步
  • 精巧的子节点和精简的软件协议栈支持灵活应用和规模扩展。

ADI的现场应用工程师与Biamp密切合作,提供了评估套件、调试支持、设计见解以及在主节点中运行的软件协议栈。借助ADI成熟的统一通信技术和工具,Biamp避免了自行开发定制电路板所需的漫长开发周期和高昂成本。

A2B的演变:从汽车到会议室

An image of the biamps conferencing hub, Devio SCR 25T.

A2B采用非屏蔽双绞线(UTP)电缆和菊花链架构,大幅减少了冗余电缆走线,从而简化了布线,降低了安装难度和相关成本。此前该技术大大简化了汽车音频系统的布线,并减轻了线束重量,也因此在业内广受认可。

在汽车领域, A2B的主要优势在于通过尽可能减少粗重的线缆,提高设计的灵活性和可扩展性,并优化系统尺寸、重量和功耗。对于Biamp而言,传输距离是重中之重,而 A2B还带来了其他诸多优势。

传统会议室与A2B会议室的比较

音频安装5

An image comparing traditional conferencing hubs with A2B conferencing hub.

减少布线:Parlé使用一个 A2B收发器和三到四个麦克风节点,能够满足最大15米的会议室需求。麦克风线路、命令和控制、电力传输、波束成形算法以及经强化的连接能力,全都整合在一条双向UTP线缆中。

超低确定延迟:音频数据通过 A2B 送达,延迟是已知且一致的。A2B 的超低确定延迟支持出色的语音处理算法性能,有助于实现Biamp的自有音频算法并确保信号完整性。

多个信号通道:Biamp利用 A2B的32个信号通道来实现音频会议领域的新应用。例如,一个通道接收供相关人员理解的信号,而另一个通道接收供机器理解的信号,从而增加对语音转文字功能的支持。

精巧的子节点:Parlé波束追踪麦克风可以智能地识别发言者,并在发言者于会议室中走动时进行跟踪。 A2B将所有这些节点连接到单个中央处理器,无需每个节点使用单独的DSP来实现边缘处理和本地波束成形。

高保真: A2B 支持高保真音频性能,并优化了总线供电,从而减少甚至无需使用专用电缆。相比之下,传统布线不仅限制了系统的灵活性和性能,而且即使在短短10米的距离内,也容易受到噪声干扰。

灵活性: A2B 提供稳健的即插即用协议栈,支持热插拔等功能,可以在系统使用期间连接和重新配置节点,在排除故障时不需要关闭系统,这大大提高了设备的可维护性。

ADI和BIAMP:实现未来会议室

音频会议技术能够以透明、恰当的方式连接分散在各地的团队,其重要性越来越突出。ADI与Biamp合作,通过Parlé系统打造了出色的自然音频体验,降低了企业改善会议环境的准入门槛。A2B技术拥有32个可用信号通道,在音频会议应用领域拥有巨大的发展潜力。

A diverse group of people happily talking in a conferencing room.
参考文献

1 Nicholas Bloom、Jose Maria Barrero、Steven Davis、Brent Meyer和Emil Mihaylov。“Survey: Remote Work Isn’t Going Away—and Executives Know It”。《哈佛商业评论》,2023年8月。
2 “IPSOS Research (Press Release) ”。EPOS Group,2020年4月。
3“IPSOS Research (Press Release) ”。EPOS Group,2020年4月。
4 “Understanding Sound Experiences (Full Report) ”。IPSOS代表EPOS Group撰写,2021年。
5 Carlos Martins,“将A2B用于音频会议系统”。ADI公司,2020年8月。