Input Magic—Differential Signals Allow Input Swing to Exceed Supply Voltage

QUESTION:

My ADC has a 1.8-V power supply. How can it have a 2-V p-p input range?

RAQ: Issue 93

Answer:

The latest generation of low-power, high-speed ADCs—manufactured on fine-line silicon processes—run on low-voltage supplies. ADC designers face a tradeoff between making the input range bigger to get better signal-to-noise ratio (larger signals provide higher SNR), and making the input range smaller to ease the drive requirements. Over the years we’ve seen ADCs with 5‑V supplies and 4-V p-p input ranges, and 3-V supplies with 2-V p-p input ranges, but these didn’t raise any eyebrows. Over the past few years, however, we’ve seen a host of ADCs with 1.8-V supplies and 2‑V p-p input ranges. These raise some seemingly reasonable questions: How can the ADC have a 2-V p-p input voltage range while running on 1.8-V supplies? Doesn’t this require the signal to exceed the supply rails?

The overlooked detail, of course, is that the analog input signal to most high-speed ADCs is differential. Transmitted as complementary single-ended signal pairs on the VIN+ and VIN– pins, the differential input signal VINDIFF = VIN+ – VIN–. The single-ended components, centered within the supply rails, swing only half the amplitude of the differential signal, with a typical common-mode voltage of VSUPPLY/2.

Differential signals are advantageous because they povide good common-mode rejection and inherent cancellation of even-order distortion (This is only true if you have perfect amplitude and phase matching, but that’s another story.). An often overlooked advantage of differential signals, however, is that the amplitude of a differential signal can have twice the amplitude as a single-ended signal within a given supply range. As ADC designs move to even lower supply voltages, the headroom for the input signal will continue to be squeezed, and the differential signal will occupy more of the available supply range. In dc-coupled applications, the common-mode voltage of these low-voltage ADCs presents an interface challenge to the drive amplifiers, but for many applications the signal can be ac-coupled to the ADC, so this will not be an issue.

I invite you to comment on Differential Signals in the Analog Dialogue Community on EngineerZone.

Author

David Buchanan

David Buchanan

David Buchanan received a B.S.E.E. from the University of Virginia in 1987. Employed in marketing and applications engineering roles by Analog Devices, Adaptec, and STMicroelectronics, he has experience with a variety of high performance analog semiconductor products. He is currently a senior applications engineer with ADI’s high speed converters product line in Greensboro, North Carolina.