Positive-to-Negative Converter Powers –48V Telecom Circuits

May 1 1998

If you’re designing a system that interfaces to telecom equipment, chances are you’ll need a −48V supply. The circuit in Figure 1 supplies up to 6W at −48V and scales to more than 12W with higher power components. Based on the Cúk topology, the converter exhibits excellent efficiency over a wide range of loading conditions (see Figure 2).

Figure 1. 12V to −48V features good efficiency over a wide range of loads.

Figure 2. Converter efficiency rises to 80% at only 20mA load.

The LT1171’s error amplifier is designed for positive-boost applications, and hence its gain and reference are of the wrong phase and polarity for sensing an inverted output. In this application, the error amplifier is simply bypassed and feedback is applied at the compensation (VC) pin. Zener diode D2 senses the output, pulling down on Q1 and the VC pin, in response to small increases in output voltage. Pulling down on the VC pin reduces peak switch current, and constitutes negative feedback. If the output is a little low, the Zener’s diminished feedback signal is overcome by an internal 200µA current source at the VC pin, thereby increasing peak switch current and restoring the output voltage.

The combination of the LT1171 and the VP-2 series VERSA-PAC coil (CTX02-13836) are suited for 120mA output current as shown. For lighter loads of up to 60mA, use the LT1172 and a VP-1-series equivalent to the coil shown. For up to 15W, use the LT1171 and a VP-5 equivalent. High voltage versions of the LT1170 family (-HV) allow inputs of up to 20V without exceeding the peak switch-voltage rating.

This converter starts working at 2.7V and will regulate −48V at reduced power. You can add undervoltage lockout by inserting a Zener diode (VZ = VLOCKOUT − 2.7V) between the input supply and the LT1172’s VIN pin.

About the Authors

Mitchell Lee
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project