TEC Controller Applications in Telecommunication Systems

2016年02月01日

Laser diodes are used in fiber optical telecommunication systems as transmitter lasers for sending signals and pump lasers for erbium doped fiber amplifiers (EDFAs) and semiconductor optical amplifiers (SOAs). In these applications, the characteristics of the laser, including wavelength, average optical power, efficiency, and extinction ratio have to be kept stable to ensure the overall performance of the telecom system. These characteristics, however, depend on the laser’s temperature: as long as the temperature drifts, the wavelength will change and the conversion efficiency will degrade. The required temperature stability ranges from ±0.001°C to ±0.5°C, differing between applications.

A loop composed of a thermistor, a thermoelectric cooler (TEC), and a TEC controller is needed for temperature control. Because the thermistor’s resistance changes proportionally with the temperature (either negative or positive proportionality, depending on the type of thermistor), it can be used to convert the temperature into voltage when configured as a voltage divider. The TEC controller will compare this fed-back voltage with the reference voltage, which represents the target temperature, and then adjust the amount of heat the TEC has to transfer by controlling the current flowing through it.

The general diagram of the system described above is shown in Figure 1. The laser diode, TEC, and thermistor sit inside the laser module. The TEC controller ADN8833 or ADN8834 will read the feedback voltage from the thermistor and provide driving voltage to the TEC. A microcontroller is used to monitor and control the thermal loop. Note that the thermal loop can also be constructed in an analog circuit. The ADN8834 has two built-in zero-drift chopper amplifiers that can be utilized as PID compensators.

Figure 1. Temperature control system for laser module.

This article will describe the composition of the thermal control system for a laser diode in a telecom system and introduce the key specifications of the main components. The purpose is to walk through the design consideration from a system-level perspective, providing the designer an overall guideline of how to build a high performance system with good temperature control accuracy, low loss, and small size.

TEC: Thermoelectric Cooling Technology

A thermoelectric cooler consists of two surface ceramic plates and alternately placed P-type and N-type semiconductor arrays in between, as shown in Figure 2.

Figure 2. TEC module with heat sink.

When current flows through these conductors, heat will be absorbed at one end and be released at the other end, and when the current direction is reversed, the heat transfer reverses as well. This process is called the Peltier effect. The carriers in the N-type semiconductor are electrons, therefore, its carrier and heat flows from anode to cathode. The N-type semiconductor on the opposite has hole carriers and the heat also flows in the opposite direction.

Taking a pair of P-N semiconductor pairs and connecting one to the other with metal plates as in Figure 3, the heat will be transferred in one direction as the current flows through.

Figure 3. Peltier effect: heat flow of a P-N semiconductor pair.

The heat transfer direction is reversible by changing the polarity of the dc voltage, and the transferred amount is proportional to the voltage amplitude. With its simplicity and robustness, thermoelectric cooling is applied to a wide variety of applications for thermal conditioning in telecommunication systems.

Selecting a TEC Module

There are many factors in the system to be considered when selecting TEC modules, such as ambient temperature, target object temperature, heat load, supply voltage, and the physical characteristics of the module. The heat load has to be carefully estimated to ensure the selected TEC module has enough capacity to pump the heat from the system to maintain the target temperature. The TEC module manufacturer usually provides two performance curves in the data sheet. One of the performance curves shows the heat transfer capacity at the different temperature difference (ΔT) over supply voltage and the other shows the cooling/heating current required under a different combination of supply voltage and ΔT. The designer can estimate the module’s power capacity and determine whether it’s sufficient for specific application.

TEC Controller Operation and the System Design

To compensate the temperature with a TEC, the TEC controller should be able to generate a reversible differential voltage according to the feed-back error, while providing proper voltage and current limits. A simplified system block diagram of ADN8834 is in Figure 4. The main functional blocks include a temperature sensing circuit, an error amplifier and compensator, TEC voltage/current sense and limit circuits, and a differential voltage driver.

Figure 4. The block diagram of a monolithic TEC controller ADN8834.

Differential Voltage Driver

The TEC controller outputs a differential voltage so that the direction of the current fed through the TEC can pump heat away from the object attached to the TEC, or smoothly transition to the opposite polarity to heat the object. The voltage driver can be a linear mode, a switch mode, or a hybrid bridge. The linear mode driver is simpler and smaller but has poor efficiency. The switch-mode driver, on the other hand, has good efficiency—up to more than 90%—but requires an additional filtering inductor and capacitor at the output. The ADN8833 and ADN8834 use a mixed configuration, with one linear driver and one switch-mode driver, reducing the bulky filtering component count by half while retaining high efficiency performance.

The voltage driver design is critical to the controller since it accounts for most of the power consumption as well as circuit board space. An optimal driver stage can help minimize the power loss, circuit size, the need for a heat sink, and the cost.

Temperature Sensing with an NTC Thermistor

Figure 5 shows the impedance of a negative temperature coefficient (NTC) thermistor over temperature. Because of its temperature dependency, it can be used to transfer temperature into voltage when connected as a voltage divider. A typical connection is shown in Figure 6, the VFB varies as RTH changes with temperature. By adding Rx in series with the thermistor, the temperature-to-voltage transfer function can be linearized in respect of VREF as in Figure 7. It is important that it be placed tightly coupled to the laser inside of the module case, isolated from external temperature disturbances so it can sense the temperature accurately.

Figure 5. Impedance curve of NTC over temperature.

 

Figure 6. NTC thermistor connected as a voltage divider to read the temperature

Figure 7. VFB over temperature.

Error Amplifier and Compensator

The analog thermal feedback loop has two stages composed of two amplifiers, as shown in Figure 8. The first amplifier takes the thermal feedback voltage (VFB) and converts or regulates the input to a linear voltage output. This voltage represents the object temperature and is fed into the compensation amplifier where it is compared with a temperature setpoint voltage, creating an error voltage that is proportional to the difference. The second amplifier is typically used to construct a PID compensator consisting of a very low frequency pole, two separate zeroes at higher frequencies, and two high frequency poles, as shown in Figure 8.

Figure 8. Diagram of the thermal feedback loop using two chopper amplifiers inside of ADN8834.

The PID compensator can be determined either mathematically or empirically. To model the thermal loop mathematically requires the precise thermal time constants of the TEC, the laser diode, the connectors, and the heat sink, which are not easy to get. Tuning the compensator empirically is more common. By asserting a step function to the temperature setpoint terminal and changing the target temperature, the designer can adjust the compensation network to minimize the settling time of the TEC temperature.

An aggressive compensator reacts to thermal disturbance quickly, but also becomes unstable easily, while a conservative compensator settles slowly, but can tolerate the thermal disturbances with less possible overshoot. It is important to reach a balance between system stability and response time.

Key Performances of TEC Controller System

Temperature Regulation Accuracy

Sometimes a steady state error will still exist even when the PID compensator is properly designed. There are a few factors that might contribute to this error. 

  • TEC thermal power budget: TEC and the supply voltage are two of the first things selected when designing the system. However, the selection may not be correct since the heat load is not easy to estimate. In some cases, when the maximum electric power has been applied to the TEC and still can’t meet the target temperature, it might imply that the thermal power budget isn’t enough to handle the heat load. Increasing the supply voltage or picking a TEC with higher power rating can resolve the issue.
  • Voltage reference consistency: The voltage reference will drift with temperature and time, which usually isn’t a problem if the thermal loop is closed. However, especially in digital controlled systems, the voltage reference of the TEC controller and the microcontroller might drift differently, thus causing an error that the compensator won’t see. It is recommended to use the same reference for both circuit, using the voltage with the higher driving capability to overwrite the other one.
  • Temperature sensing: Sensing the load temperature precisely is critical to minimizing temperature error. Any error coming from the feedback will be introduced to the system and again can’t be corrected by the compensator. Use a high precision thermistor and an auto-zero amplifier to avoid errors. The placement of the thermistor is also important. Make sure it is attached to the laser so that it can read the actual temperature we’re controlling.

Efficiency

The driver stage consumes the majority of the power loss in the TEC controller. In ADN8833/ADN8834, the power dissipation of the linear driver is straightforward to derive, given its input-to-output voltage drop and load current. The switch-mode driver loss is more complicated, which can be roughly broken down to the conduction losses, the switching loss, and the transition loss. The conduction loss is proportional to the RDSON of the FETs and the dc resistance of the filtering inductor. It can be reduced by selecting low resistance components. The switching loss and the transition loss depend highly on the switching frequency. With higher frequency, the losses are higher but the passive component size can be reduced. To achieve an optimal design, trade-offs between efficiency and space must be carefully considered.

Noise and Ripple

The switch-mode driver in ADN8833/ADN8834 switches at 2 MHz and the fast PWM switching clock edge contains a broad frequency spectrum, creating voltage ripple at the TEC terminals as well as noise in the whole system. The noise and ripple can be reduced by adding proper decoupling and ripple suppression capacitors.

On the supply voltage rail, the ripple is mainly caused by the discontinuous current chopped by the PWM FETs in the buck topology commonly used for the switch-mode supply. Use multiple SMT ceramic capacitors in parallel to reduce ESR (equivalent serial resistance) and locally decouple the supply voltage. On the switch-mode driver output node, voltage ripple is caused by the current ripple of the filtering inductor. To suppress this ripple, place multiple SMT ceramic capacitors in parallel from the driver’s output to ground. Since the ripple voltage is mostly determined by the product of the capacitor ESR and the inductor ripple current: ΔV_TEC = ESR × ΔI_L. Using multiple capacitors in parallel can effectively reduce the equivalent ESR.

Conclusion

Designing a TEC controller system for laser diodes in telecommunication systems is a complex job. Except for the challenges in thermal accuracy, the package size is typically very small and the power dissipation tolerance is low. In general, a well designed TEC controller should possess merits that include:

  • Accurate temperature regulation
  • High efficiency
  • Small board size
  • Low noise
  • Current and voltage monitoring and protection

著者について

Yajung Tu
Yajung Tu has a master’s degree in electrical engineering, and currently works as an applications engineer in the Power Management Group for Analog Devices. Her area of expertise is thermoelectric cooler controllers.
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成

この記事に関して

製品

最新メディア 21

Subtitle
さらに詳しく
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成